PDK API Guide for J721E
|
This file contains the definition of all the parameter IDs for PM, RM, Security.
Go to the source code of this file.
#define TISCI_PARAM_UNDEF (0xFFFFFFFFU) |
Undefined Param Undefined
#define SCICLIENT_FIRMWARE_ABI_MAJOR (3U) |
#define SCICLIENT_FIRMWARE_ABI_MINOR (1U) |
#define SCICLIENT_CONTEXT_R5_NONSEC_0 (0U) |
R5_0(Non Secure): Cortex R5 context 0 on MCU island
#define SCICLIENT_CONTEXT_R5_SEC_0 (1U) |
R5_1(Secure): Cortex R5 context 1 on MCU island(Boot)
#define SCICLIENT_CONTEXT_R5_NONSEC_1 (2U) |
R5_2(Non Secure): Cortex R5 context 2 on MCU island
#define SCICLIENT_CONTEXT_R5_SEC_1 (3U) |
R5_3(Secure): Cortex R5 context 3 on MCU island
#define SCICLIENT_CONTEXT_A72_SEC_0 (4U) |
A72_0(Secure): Cortex A72 context 0 on Main island
#define SCICLIENT_CONTEXT_A72_SEC_1 (5U) |
A72_1(Secure): Cortex A72 context 1 on Main island
#define SCICLIENT_CONTEXT_A72_NONSEC_0 (6U) |
A72_2(Non Secure): Cortex A72 context 2 on Main island
#define SCICLIENT_CONTEXT_A72_NONSEC_1 (7U) |
A72_3(Non Secure): Cortex A72 context 3 on Main island
#define SCICLIENT_CONTEXT_A72_NONSEC_2 (8U) |
A72_4(Non Secure): Cortex A72 context 4 on Main island
#define SCICLIENT_CONTEXT_C7X_SEC_0 (9U) |
C7X_0(Secure): C7x Context 0 on Main island
#define SCICLIENT_CONTEXT_C7X_NONSEC_0 (10U) |
C7X_1(Non Secure): C7x context 1 on Main island
#define SCICLIENT_CONTEXT_C6X_0_SEC_0 (11U) |
C6X_0_0(Secure): C6x_0 Context 0 on Main island
#define SCICLIENT_CONTEXT_C6X_0_NONSEC_0 (12U) |
C6X_0_1(Non Secure): C6x_0 context 1 on Main island
#define SCICLIENT_CONTEXT_C6X_1_SEC_0 (13U) |
C6X_1_0(Secure): C6x_1 Context 0 on Main island
#define SCICLIENT_CONTEXT_C6X_1_NONSEC_0 (14U) |
C6X_1_1(Non Secure): C6x_1 context 1 on Main island
#define SCICLIENT_CONTEXT_GPU_NONSEC_0 (15U) |
GPU_0(Non Secure): RGX context 0 on Main island
#define SCICLIENT_CONTEXT_MAIN_0_R5_NONSEC_0 (16U) |
MAIN_0_R5_0(Non Secure): Cortex R5_0 context 0 on Main island
#define SCICLIENT_CONTEXT_MAIN_0_R5_SEC_0 (17U) |
MAIN_0_R5_1(Secure): Cortex R5_0 context 1 on Main island
#define SCICLIENT_CONTEXT_MAIN_0_R5_NONSEC_1 (18U) |
MAIN_0_R5_2(Non Secure): Cortex R5_0 context 2 on Main island
#define SCICLIENT_CONTEXT_MAIN_0_R5_SEC_1 (19U) |
MAIN_0_R5_3(Secure): Cortex R5_0 context 3 on MCU island
#define SCICLIENT_CONTEXT_MAX_NUM (20U) |
MAIN_1_R5_0(Non Secure): Cortex R5_1 context 0 on Main island
#define SCICLIENT_PROC_ID_A72SS0_CORE0 (0x20U) |
COMPUTE_CLUSTER_J7ES_TB_VDC_MAIN_0: (Cluster 0 Processor 0)
#define SCICLIENT_PROC_ID_A72SS0_CORE1 (0x21U) |
COMPUTE_CLUSTER_J7ES_TB_VDC_MAIN_0: (Cluster 0 Processor 1)
#define SCICLIENT_PROC_ID_C71SS0 (0x30U) |
COMPUTE_CLUSTER_J7ES_TB_VDC_MAIN_0: (Cluster 4 Processor 0)
#define SCICLIENT_PROC_ID_C66SS0_CORE0 (0x03U) |
J7_MAIN_SEC_MMR_MAIN_0: (Cluster 2 Processor 0)
#define SCICLIENT_PROC_ID_C66SS1_CORE0 (0x04U) |
J7_MAIN_SEC_MMR_MAIN_0: (Cluster 3 Processor 0)
#define SCICLIENT_PROC_ID_R5FSS0_CORE0 (0x06U) |
J7_MAIN_SEC_MMR_MAIN_0: (Cluster 0 Processor 0)
#define SCICLIENT_PROC_ID_R5FSS0_CORE1 (0x07U) |
J7_MAIN_SEC_MMR_MAIN_0: (Cluster 0 Processor 1)
#define SCICLIENT_PROC_ID_R5FSS1_CORE0 (0x08U) |
J7_MAIN_SEC_MMR_MAIN_0: (Cluster 1 Processor 0)
#define SCICLIENT_PROC_ID_R5FSS1_CORE1 (0x09U) |
J7_MAIN_SEC_MMR_MAIN_0: (Cluster 1 Processor 1)
#define SCICLIENT_PROC_ID_MCU_R5FSS0_CORE0 (0x01U) |
J7_MCU_SEC_MMR_MCU_0: (Cluster 0 Processor 0)
#define SCICLIENT_PROC_ID_MCU_R5FSS0_CORE1 (0x02U) |
J7_MCU_SEC_MMR_MCU_0: (Cluster 0 Processor 1)
#define SCICLIENT_SOC_NUM_PROCESSORS (0x0BU) |
Total Number of processors in J721E
#define TISCI_MSG_VALUE_RM_NULL_RING_TYPE (0xFFFFu) |
-----------------— Resource Management Parameters ------------------— Null Ring type
#define TISCI_MSG_VALUE_RM_NULL_RING_INDEX (0xFFFFFFFFu) |
Null Ring Index
#define TISCI_MSG_VALUE_RM_NULL_RING_ADDR (0xFFFFFFFFu) |
The ring base address register fields are not be modified if this value is used for: tisci_msg_rm_ring_cfg_req::addr_lo tisci_msg_rm_ring_cfg_req::addr_hi
#define TISCI_MSG_VALUE_RM_NULL_RING_COUNT (0xFFFFFFFFu) |
The ring size field of the RING_SIZE register is not modified if this value is used for: tisci_msg_rm_ring_cfg_req::count
#define TISCI_MSG_VALUE_RM_NULL_RING_MODE (0xFFu) |
The ring mode field of the RING_SIZE register is not modified if this value is used for: tisci_msg_rm_ring_cfg_req::mode
#define TISCI_MSG_VALUE_RM_NULL_RING_SIZE (0xFFu) |
The ring elsize field of the RING_SIZE register is not modified if this value is used for: tisci_msg_rm_ring_cfg_req::size
#define TISCI_MSG_VALUE_RM_NULL_ORDER_ID (0xFFu) |
Default value for tisci_msg_rm_ring_cfg_req::order_id. No changes to the order ID field of the ring will take place if this value is used.
#define TISCI_MSG_VALUE_RM_UDMAP_NULL_CH_TYPE (0xFFu) |
Value specified for tisci_msg_rm_udmap_tx_ch_cfg_req::tx_chan_type and tisci_msg_rm_udmap_rx_ch_cfg_req::rx_chan_type when an explicit channel index is provided. DMSC RM will return a NACK if a non-NULL channel type is passed along with an explicit channel index.
#define TISCI_MSG_VALUE_RM_UDMAP_NULL_CH_INDEX (0xFFFFFFFFu) |
Value specified for tisci_msg_rm_udmap_tx_ch_cfg_req::index and tisci_msg_rm_udmap_rx_ch_cfg_req::index when the user wants to request DMSC RM allocate an unused UDMAP channel. When specified for the channel index a valid channel type must be provided.
#define TISCI_ISC_CC_ID (160U) |
Special ISC ID to refer to compute cluster privid registers.
#define TISCI_RINGACC0_OES_IRQ_SRC_IDX_START (0U) |
#define TISCI_RINGACC0_MON_IRQ_SRC_IDX_START (1024U) |
#define TISCI_RINGACC0_EOES_IRQ_SRC_IDX_START (2048U) |
#define TISCI_UDMAP0_TX_OES_IRQ_SRC_IDX_START (0U) |
#define TISCI_UDMAP0_TX_EOES_IRQ_SRC_IDX_START (512U) |
#define TISCI_UDMAP0_RX_OES_IRQ_SRC_IDX_START (1024U) |
#define TISCI_UDMAP0_RX_EOES_IRQ_SRC_IDX_START (1280U) |
#define TISCI_UDMAP0_RX_FLOW_EOES_IRQ_SRC_IDX_START (1536U) |
#define SCICLIENT_C7X_NON_SECURE_INTERRUPT_NUM (9U) |
#define SCICLIENT_C7X_SECURE_INTERRUPT_NUM (10U) |
#define SCICLIENT_DEV_MCU_R5FSS0_CORE0 (TISCI_DEV_MCU_R5FSS0_CORE0) |
#define SCICLIENT_DEV_MCU_R5FSS0_CORE1 (TISCI_DEV_MCU_R5FSS0_CORE1) |
#define SCICLIENT_DEV_MCU_R5FSS0_CORE0_PROCID (SCICLIENT_PROC_ID_MCU_R5FSS0_CORE0) |
#define SCICLIENT_DEV_MCU_R5FSS0_CORE1_PROCID (SCICLIENT_PROC_ID_MCU_R5FSS0_CORE1) |
#define SCICLIENT_ALLOWED_BOARDCFG_BASE_START (CSL_MCU_MSRAM_1MB0_RAM_BASE) |
Board config Base start address
#define SCICLIENT_ALLOWED_BOARDCFG_BASE_END (CSL_MCU_MSRAM_1MB0_RAM_BASE + CSL_MCU_MSRAM_1MB0_RAM_SIZE) |
Board config Base end address