This is LDC Configuration file
|
file | ldc_cfg.h |
| Defines the structures / control operations that could be used to configure / control LDC module.
|
|
|
typedef void(* | Ldc_ErrEventCbFxn) (Fvid2_Handle handle, uint32_t errEvents, void *appData) |
| Prototype for the Error Event for LDC. The callback for the LDC error events can be registered using Ldc_ErrEventParams. One of the parameter in this is call back. Driver calls this callback when error occurs. More...
|
|
◆ IOCTL_LDC_SET_LUMA_TONEMAP_LUT_CFG
#define IOCTL_LDC_SET_LUMA_TONEMAP_LUT_CFG |
Value: 0x0U)
#define VHWA_IOCTL_LDC_IOCTL_BASE
Definition: vhwa_common.h:122
IOCTL for setting Luma Lut. struct Ldc_RemapLutCfg is as argument.
- Returns
- FVID2_SOK on success, else error code.
◆ IOCTL_LDC_SET_CHROMA_TONEMAP_LUT_CFG
#define IOCTL_LDC_SET_CHROMA_TONEMAP_LUT_CFG |
Value: 0x1U)
#define VHWA_IOCTL_LDC_IOCTL_BASE
Definition: vhwa_common.h:122
IOCTL for setting Chroma Lut. struct Ldc_RemapLutCfg is as argument.
- Returns
- FVID2_SOK on success, else error code.
◆ LDC_MAX_OUTPUT
#define LDC_MAX_OUTPUT (2u) |
◆ LDC_MESH_BUF_ADDR_ALIGN
#define LDC_MESH_BUF_ADDR_ALIGN (0x10u) |
Alignment requirement for LDC Mesh Table.
◆ LDC_MAX_HORZ_REGIONS
#define LDC_MAX_HORZ_REGIONS (3U) |
Maximum number of horizontal regions supported by LDC.
◆ LDC_MAX_VERT_REGIONS
#define LDC_MAX_VERT_REGIONS (3U) |
Maximum number of horizontal regions supported by LDC.
◆ LDC_MAX_REGIONS
Value: LDC_MAX_VERT_REGIONS)
#define LDC_MAX_HORZ_REGIONS
Maximum number of horizontal regions supported by LDC.
Definition: ldc_cfg.h:107
Maximum number of regions supported by LDC.
◆ LDC_REMAP_LUT_SIZE
#define LDC_REMAP_LUT_SIZE (513u) |
◆ VHWA_LDC_LUMA_INTRP_BICUBIC
#define VHWA_LDC_LUMA_INTRP_BICUBIC (0U) |
Bicubic interpolation is used for Luma.
<Bilinear interpolation is used for Luma
◆ VHWA_LDC_LUMA_INTRP_BILINEAR
#define VHWA_LDC_LUMA_INTRP_BILINEAR (1U) |
Interpolation Max, used for error checking.
◆ VHWA_LDC_LUMA_INTRP_MAX
#define VHWA_LDC_LUMA_INTRP_MAX (2U) |
◆ VHWA_LDC_LUT_DS_FACTOR_1
#define VHWA_LDC_LUT_DS_FACTOR_1 (0U) |
no downsampling
<Down sampling by 2
◆ VHWA_LDC_LUT_DS_FACTOR_2
#define VHWA_LDC_LUT_DS_FACTOR_2 (1U) |
◆ VHWA_LDC_LUT_DS_FACTOR_4
#define VHWA_LDC_LUT_DS_FACTOR_4 (2U) |
◆ VHWA_LDC_LUT_DS_FACTOR_8
#define VHWA_LDC_LUT_DS_FACTOR_8 (3U) |
◆ VHWA_LDC_LUT_DS_FACTOR_16
#define VHWA_LDC_LUT_DS_FACTOR_16 (4U) |
◆ VHWA_LDC_LUT_DS_FACTOR_32
#define VHWA_LDC_LUT_DS_FACTOR_32 (5U) |
◆ VHWA_LDC_LUT_DS_FACTOR_64
#define VHWA_LDC_LUT_DS_FACTOR_64 (6U) |
◆ VHWA_LDC_LUT_DS_FACTOR_128
#define VHWA_LDC_LUT_DS_FACTOR_128 (7U) |
Downscaling factor MAX, used for error checking.
◆ VHWA_LDC_LUT_DS_FACTOR_MAX
#define VHWA_LDC_LUT_DS_FACTOR_MAX (8U) |
◆ VHWA_LDC_MAX_BURST_LENGTH_16
#define VHWA_LDC_MAX_BURST_LENGTH_16 (0U) |
Max Burst length of 16.
<Max Burst length of 8
◆ VHWA_LDC_MAX_BURST_LENGTH_8
#define VHWA_LDC_MAX_BURST_LENGTH_8 (1U) |
◆ VHWA_LDC_MAX_BURST_LENGTH_4
#define VHWA_LDC_MAX_BURST_LENGTH_4 (2U) |
◆ VHWA_LDC_MAX_BURST_LENGTH_2
#define VHWA_LDC_MAX_BURST_LENGTH_2 (3U) |
LDC Burst Length max, used for error checking.
◆ VHWA_LDC_MAX_BURST_LENGTH_MAX
#define VHWA_LDC_MAX_BURST_LENGTH_MAX (4U) |
◆ VHWA_LDC_PIX_IBLK_OUTOFBOUND_ERR
#define VHWA_LDC_PIX_IBLK_OUTOFBOUND_ERR (0x1U) |
Back mapped pixel co-ordinate goes out of the pre-computed input pixel bounding box.
<Block mesh co-ordinate goes out of the pre-computed mesh bounding box
◆ VHWA_LDC_MESH_IBLK_OUTOFBOUND
#define VHWA_LDC_MESH_IBLK_OUTOFBOUND (0x2U) |
Input Pixel block memory overflow.
◆ VHWA_LDC_PIX_IBLK_MEMOVF
#define VHWA_LDC_PIX_IBLK_MEMOVF (0x4U) |
Mesh block memory overflow.
◆ VHWA_LDC_MESH_IBLK_MEMOVF
#define VHWA_LDC_MESH_IBLK_MEMOVF (0x8U) |
Back mapped input co-ordinate goes out of input frame range.
◆ VHWA_LDC_IFR_OUTOFBOUND
#define VHWA_LDC_IFR_OUTOFBOUND (0x10U) |
Affine and perspective transform precision overflow error.
◆ VHWA_LDC_INT_SZOVF
#define VHWA_LDC_INT_SZOVF (0x20U) |
Error on SL2 VBSUM Write interface.
◆ VHWA_LDC_SL2_WR_ERR
#define VHWA_LDC_SL2_WR_ERR (0x80U) |
Error on Input VBUSM Read interface.
◆ VHWA_LDC_VBUSM_RD_ERR
#define VHWA_LDC_VBUSM_RD_ERR (0x100U) |
◆ Ldc_ErrEventCbFxn
typedef void(* Ldc_ErrEventCbFxn) (Fvid2_Handle handle, uint32_t errEvents, void *appData) |
Prototype for the Error Event for LDC. The callback for the LDC error events can be registered using Ldc_ErrEventParams. One of the parameter in this is call back. Driver calls this callback when error occurs.
- Parameters
-
handle | FVID2 driver handle, for which error has occurred. |
errEvents | Error Events occured, Refer to Ldc_ErrorEvents for valid values. |
- Returns
- None.
◆ Ldc_ConfigInit()
This function should be used to initialize variable of type Ldc_Config.
Ldc_ConfigInit
- Parameters
-
- Returns
- None