![]() |
TIOVX User Guide
|
The configuration data structure used by the TIVX_KERNEL_CAPTURE kernel. More...
#include <j7_capture.h>
Data Fields | |
tivx_capture_inst_params_t | instCfg [TIVX_CAPTURE_MAX_INST] |
uint32_t | instId [TIVX_CAPTURE_MAX_INST] |
uint32_t | numInst |
uint32_t | numCh |
uint32_t | chVcNum [TIVX_CAPTURE_MAX_CH] |
uint32_t | chInstMap [TIVX_CAPTURE_MAX_CH] |
uint32_t | timeout |
uint32_t | timeoutInitial |
The configuration data structure used by the TIVX_KERNEL_CAPTURE kernel.
Definition at line 336 of file j7_capture.h.
tivx_capture_inst_params_t tivx_capture_params_t::instCfg[TIVX_CAPTURE_MAX_INST] |
CSI2Rx Instance configuration
Definition at line 338 of file j7_capture.h.
uint32_t tivx_capture_params_t::instId[TIVX_CAPTURE_MAX_INST] |
CSI2Rx Instance Id, 0:CSIRx0 1:CSIRx0
Definition at line 339 of file j7_capture.h.
uint32_t tivx_capture_params_t::numInst |
Number of instances in current capture node
Definition at line 340 of file j7_capture.h.
uint32_t tivx_capture_params_t::numCh |
Number of channels to be processed on current instance of Node
Definition at line 341 of file j7_capture.h.
uint32_t tivx_capture_params_t::chVcNum[TIVX_CAPTURE_MAX_CH] |
Virtual Channel Number for each channel
Definition at line 342 of file j7_capture.h.
uint32_t tivx_capture_params_t::chInstMap[TIVX_CAPTURE_MAX_CH] |
Instance ID for each channel
Definition at line 343 of file j7_capture.h.
uint32_t tivx_capture_params_t::timeout |
Total timeout (in ms) for all cameras. If this timeout is exceeded, cameras that have not been received are dead. The timeout value will only be considered if calling the tivxCaptureRegisterErrorFrame API to enable error detection
Definition at line 344 of file j7_capture.h.
uint32_t tivx_capture_params_t::timeoutInitial |
Initial failure timeout (in ms) for first time the capture node fails. Once this timeout has been exceeded, the "timeout" parameter will then be used. The timeout value will only be considered if calling the tivxCaptureRegisterErrorFrame API to enable error detection
Definition at line 346 of file j7_capture.h.