![]() |
TIOVX User Guide
|
Capture (Source Node) Kernels.
Data Structures | |
struct | tivx_capture_inst_params_t |
The CSIRX DRV instance configuration data structure used by the TIVX_KERNEL_CAPTURE kernel. More... | |
struct | tivx_capture_params_t |
The configuration data structure used by the TIVX_KERNEL_CAPTURE kernel. More... | |
struct | tivx_capture_statistics_t |
Capture status structure used to get the current status. More... | |
Defines | |
#define | TIVX_KERNEL_CAPTURE_NAME "com.ti.capture" |
capture kernel name | |
#define | TIVX_CAPTURE_PRINT_STATISTICS (0x40000000u) |
Control Command to print capture statistics No argument is needed to query statistics. | |
#define | TIVX_CAPTURE_GET_STATISTICS (0x40000001u) |
Control Command to return capture statistics to application. More... | |
#define | TIVX_CAPTURE_REGISTER_ERROR_FRAME (0x40000002u) |
Control Command to create additional frame object descriptors from a provided frame reference. The data buffers for each new descriptor will point to the same data buffer as the provided frame reference. | |
#define | TIVX_CAPTURE_MAX_CH (16U) |
Maximum number of channels supported in the capture node. | |
#define | TIVX_CAPTURE_MAX_INST (2U) |
Maximum number of instances supported in the capture node. | |
#define | TIVX_CAPTURE_MAX_STRM (4U) |
Maximum number of streams supported in a capture module. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_80_TO_100_MBPS ((uint32_t) 0x00U) |
Lane Band Speed: 80 Mbps to 100 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_100_TO_120_MBPS ((uint32_t) 0x01U) |
Lane Band Speed: 100 Mbps to 120 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_120_TO_160_MBPS ((uint32_t) 0x02U) |
Lane Band Speed: 120 Mbps to 160 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_160_TO_200_MBPS ((uint32_t) 0x03U) |
Lane Band Speed: 160 Mbps to 200 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_200_TO_240_MBPS ((uint32_t) 0x04U) |
Lane Band Speed: 200 Mbps to 240 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_240_TO_280_MBPS ((uint32_t) 0x05U) |
Lane Band Speed: 240 Mbps to 280 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_280_TO_320_MBPS ((uint32_t) 0x06U) |
Lane Band Speed: 280 Mbps to 320 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_320_TO_360_MBPS ((uint32_t) 0x07U) |
Lane Band Speed: 320 Mbps to 360 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_360_TO_400_MBPS ((uint32_t) 0x08U) |
Lane Band Speed: 360 Mbps to 400 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_400_TO_480_MBPS ((uint32_t) 0x09U) |
Lane Band Speed: 400 Mbps to 480 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_480_TO_560_MBPS ((uint32_t) 0x0AU) |
Lane Band Speed: 480 Mbps to 560 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_560_TO_640_MBPS ((uint32_t) 0x0BU) |
Lane Band Speed: 560 Mbps to 640 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_640_TO_720_MBPS ((uint32_t) 0x0CU) |
Lane Band Speed: 640 Mbps to 720 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_720_TO_800_MBPS ((uint32_t) 0x0DU) |
Lane Band Speed: 720 Mbps to 800 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_800_TO_880_MBPS ((uint32_t) 0x0EU) |
Lane Band Speed: 800 Mbps to 880 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_880_TO_1040_MBPS ((uint32_t) 0x0FU) |
Lane Band Speed: 880 Mbps to 1040 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_1040_TO_1200_MBPS ((uint32_t) 0x10U) |
Lane Band Speed: 1040 Mbps to 1200 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_1200_TO_1350_MBPS ((uint32_t) 0x11U) |
Lane Band Speed: 1200 Mbps to 1350 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_1350_TO_1500_MBPS ((uint32_t) 0x12U) |
Lane Band Speed: 1350 Mbps to 1500 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_1500_TO_1750_MBPS ((uint32_t) 0x13U) |
Lane Band Speed: 1500 Mbps to 1750 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_1750_TO_2000_MBPS ((uint32_t) 0x14U) |
Lane Band Speed: 1750 Mbps to 2000 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_2000_TO_2250_MBPS ((uint32_t) 0x15U) |
Lane Band Speed: 2000 Mbps to 2250 Mbps. | |
#define | TIVX_CAPTURE_LANE_BAND_SPEED_2250_TO_2500_MBPS ((uint32_t) 0x16U) |
Lane Band Speed: 2250 Mbps to 2500 Mbps. | |
Functions | |
void | tivxRegisterHwaTargetCaptureKernels (void) |
Function to register HWA Kernels on the capture Target. | |
void | tivxUnRegisterHwaTargetCaptureKernels (void) |
Function to un-register HWA Kernels on the capture Target. | |
VX_API_ENTRY vx_node VX_API_CALL | tivxCaptureNode (vx_graph graph, vx_user_data_object input, vx_object_array output) |
[Graph] Creates a camera capture node. More... | |
void | tivx_capture_params_init (tivx_capture_params_t *prms) |
Function to initialize Capture Parameters. More... | |
vx_status | tivxCaptureRegisterErrorFrame (vx_node node, vx_reference ref) |
Function to send error frame to capture node. More... | |
#define TIVX_CAPTURE_GET_STATISTICS (0x40000001u) |
Control Command to return capture statistics to application.
This control command returns the status of the capture node. Please refer to tivx_capture_statistics_t structure.
Definition at line 134 of file j7_capture.h.
VX_API_ENTRY vx_node VX_API_CALL tivxCaptureNode | ( | vx_graph | graph, |
vx_user_data_object | input, | ||
vx_object_array | output | ||
) |
[Graph] Creates a camera capture node.
The capture node takes in a user data object of type tivx_capture_params_t
to configure one or more capture channels. The output is of type vx_object_array, which contain an array of either vx_image or tivx_raw_image data types. vx_image is used if the sensor outputs processed image formats, while tivx_raw_image is used for raw sensor outputs.
If using tivx_raw_image as the output, the raw image type MUST be one of the following formats:
If using vx_image, the image type MUST be one of the following formats:
The number of items in the output object array corresponds to the number of syncronized, homogeneous camera sensors assigned to the capture node. Each item in an object array must have the same dimensions and formats. If multiple sensors are needed tot be configured at different rates, formats, or resolutions, then separate capture nodes should be used and syncronized by the application code.
[in] | graph | The reference to the graph. |
[in] | input | The input user data object of a single capture params structure of type tivx_capture_params_t . |
[out] | output | Object array output which has been created from an exemplar of either vx_image or tivx_raw_image. |
TIVX_KERNEL_CAPTURE_NAME
vx_node
. vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
void tivx_capture_params_init | ( | tivx_capture_params_t * | prms | ) |
Function to initialize Capture Parameters.
prms | [in] Pointer to capture params configuration structure |
vx_status tivxCaptureRegisterErrorFrame | ( | vx_node | node, |
vx_reference | ref | ||
) |
Function to send error frame to capture node.
Provided ref must be of the same type and have same properties as an element of the capture node output object array This API must be called after the vxVerifyGraph call and before the processing of the OpenVX graph
node | [in] Capture node reference |
ref | [in] Error frame to be replicated |