PDK API Guide for J721E
|
PMIC TPS6594x Leo PMIC GPIO API/interface file.
Go to the source code of this file.
Macros | |
PMIC GPIO supported pins for TPS6594x Leo Device | |
#define | PMIC_TPS6594X_GPIO1_PIN (1U) |
#define | PMIC_TPS6594X_GPIO2_PIN (2U) |
#define | PMIC_TPS6594X_GPIO3_PIN (3U) |
#define | PMIC_TPS6594X_GPIO4_PIN (4U) |
#define | PMIC_TPS6594X_GPIO5_PIN (5U) |
#define | PMIC_TPS6594X_GPIO6_PIN (6U) |
#define | PMIC_TPS6594X_GPIO7_PIN (7U) |
#define | PMIC_TPS6594X_GPIO8_PIN (8U) |
#define | PMIC_TPS6594X_GPIO9_PIN (9U) |
#define | PMIC_TPS6594X_GPIO10_PIN (10U) |
#define | PMIC_TPS6594X_GPIO11_PIN (11U) |
PMIC GPIO pin functions supported for TPS6594x Leo Device | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO (0U) |
Used to configure GPIO Pin Function. Valid for all GPIO Pins. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO1_SCL_I2C2_CS_SPI (1U) |
Used to configure SCL_I2C2/CS_SPI Pin Function. Valid only for GPIO1 pin. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO2_GPIO11_TRIG_WDOG (1U) |
Used to configure TRIG_WDOG Pin Function. Valid only for GPIO2 and GPIO11 pins. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO3_GPIO4_GPIO8_CLK32KOUT (1U) |
Used to configure CLK32KOUT Pin Function. Valid only for GPIO3, GPIO4 and GPIO8 pins. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO5_SCLK_SPMI (1U) |
Used to configure SCLK_SPMI Pin Function. Valid only for GPIO5 pin. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO6_SDATA_SPMI (1U) |
Used to configure SDATA_SPMI Pin Function. Valid only for GPIO6 pin. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO7_NERR_MCU (1U) |
Used to configure NERR_MCU Pin Function. Valid only for GPIO7 pin. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO9_PGOOD (1U) |
Used to configure PGOOD Pin Function. Valid only for GPIO9 pin. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO10_SYNCCLKIN (1U) |
Used to configure SYNCCLKIN Pin Function. Valid only for GPIO10 pin. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO1_GPIO11_NRSTOUT_SOC (2U) |
Used to configure NRSTOUT_SOC Pin Function. Valid only for GPIO1 and GPIO11 pin. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO2_SDA_I2C2_SDO_SPI (2U) |
Used to configure SDA_I2C2/SDO_SPI Pin Function. Valid only for GPIO2 pin. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO3_NERR_SOC (2U) |
Used to configure NERR_SOC Pin Function. Valid only for GPIO3 pin. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO8_GPIO10_SYNCCLKOUT (2U) |
Used to configure SYNCCLKOUT Pin Function. Valid only for GPIO8 and GPIO10 pin. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO9_DISABLE_WDOG (2U) |
Used to configure DISABLE_WDOG Pin Function. Valid only for GPIO9 pin. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO8_DISABLE_WDOG (3U) |
Used to configure DISABLE_WDOG Pin Function. Valid only for GPIO8 pin. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO9_SYNCCLKOUT (3U) |
Used to configure SYNCCLKOUT Pin Function. Valid only for GPIO9 pin. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO10_CLK32KOUT (3U) |
Used to configure CLK32KOUT Pin Function. Valid only for GPIO10 pin. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_NSLEEP1 (4U) |
Used to configure NSLEEP1 Pin Function. Valid for all GPIO Pins. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_NSLEEP2 (5U) |
Used to configure NSLEEP2 Pin Function. Valid for all GPIO Pins. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_WKUP1 (6U) |
Used to configure WKUP1 Pin Function. Valid for all GPIO Pins except GPIO3 and GPIO4 pins. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO3_GPIO4_LP_WKUP1 (6U) |
Used to configure LP_WKUP1 Pin Function. Valid only for GPIO3 and GPIO4 pins. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_WKUP2 (7U) |
Used to configure WKUP2 Pin Function. Valid for all GPIO Pins except GPIO3 and GPIO4 pins. More... | |
#define | PMIC_TPS6594X_GPIO_PINFUNC_GPIO3_GPIO4_LP_WKUP2 (7U) |
Used to configure LP_WKUP2 Pin Function. Valid only for GPIO3 and GPIO4 pins. More... | |
PMIC GPIO NPWRON pin functions supported for TPS6594x Leo Device | |
#define | PMIC_TPS6594X_NPWRON_PINFUNC_ENABLE (0U) |
Enable Signal Function for NPWRON/ENABLE pin. More... | |
#define | PMIC_TPS6594X_NPWRON_PINFUNC_NPWRON (1U) |
NPWRON Signal Function for NPWRON/ENABLE pin. More... | |
#define | PMIC_TPS6594X_NPWRON_PINFUNC_NONE (2U) |
None Function for NPWRON/ENABLE pin. More... | |
Functions | |
int32_t | Pmic_gpioTps6594xNPwronPinGetValue (Pmic_CoreHandle_t *pPmicCoreHandle, uint8_t *pPinValue) |
API to get PMIC GPIO NPWRON/Enable pin value. More... | |