46 #ifndef PMIC_GPIO_TPS6594X_H_ 47 #define PMIC_GPIO_TPS6594X_H_ 68 #define PMIC_TPS6594X_GPIO1_PIN (1U) 69 #define PMIC_TPS6594X_GPIO2_PIN (2U) 70 #define PMIC_TPS6594X_GPIO3_PIN (3U) 71 #define PMIC_TPS6594X_GPIO4_PIN (4U) 72 #define PMIC_TPS6594X_GPIO5_PIN (5U) 73 #define PMIC_TPS6594X_GPIO6_PIN (6U) 74 #define PMIC_TPS6594X_GPIO7_PIN (7U) 75 #define PMIC_TPS6594X_GPIO8_PIN (8U) 76 #define PMIC_TPS6594X_GPIO9_PIN (9U) 77 #define PMIC_TPS6594X_GPIO10_PIN (10U) 78 #define PMIC_TPS6594X_GPIO11_PIN (11U) 89 #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO (0U) 92 #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO1_SCL_I2C2_CS_SPI (1U) 95 #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO2_GPIO11_TRIG_WDOG (1U) 98 #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO3_GPIO4_GPIO8_CLK32KOUT (1U) 101 #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO5_SCLK_SPMI (1U) 104 #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO6_SDATA_SPMI (1U) 107 #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO7_NERR_MCU (1U) 110 #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO9_PGOOD (1U) 113 #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO10_SYNCCLKIN (1U) 116 #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO1_GPIO11_NRSTOUT_SOC (2U) 119 #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO2_SDA_I2C2_SDO_SPI (2U) 122 #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO3_NERR_SOC (2U) 125 #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO8_GPIO10_SYNCCLKOUT (2U) 128 #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO9_DISABLE_WDOG (2U) 131 #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO8_DISABLE_WDOG (3U) 134 #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO9_SYNCCLKOUT (3U) 137 #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO10_CLK32KOUT (3U) 140 #define PMIC_TPS6594X_GPIO_PINFUNC_NSLEEP1 (4U) 143 #define PMIC_TPS6594X_GPIO_PINFUNC_NSLEEP2 (5U) 146 #define PMIC_TPS6594X_GPIO_PINFUNC_WKUP1 (6U) 149 #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO3_GPIO4_LP_WKUP1 (6U) 152 #define PMIC_TPS6594X_GPIO_PINFUNC_WKUP2 (7U) 155 #define PMIC_TPS6594X_GPIO_PINFUNC_GPIO3_GPIO4_LP_WKUP2 (7U) 165 #define PMIC_TPS6594X_NPWRON_PINFUNC_ENABLE (0U) 167 #define PMIC_TPS6594X_NPWRON_PINFUNC_NPWRON (1U) 169 #define PMIC_TPS6594X_NPWRON_PINFUNC_NONE (2U) PMIC Interface Handle. Contains various PMIC driver instance specific information....
Definition: pmic_types.h:148
PMIC Driver Common API/interface file.
int32_t Pmic_gpioTps6594xNPwronPinGetValue(Pmic_CoreHandle_t *pPmicCoreHandle, uint8_t *pPinValue)
API to get PMIC GPIO NPWRON/Enable pin value.