![]() |
PDK API Guide for J721E
|
PMIC common Driver contains Miscellaneous APIs supported by all supported PMIC Devices. Like, PMIC recovery count APIs, Read/Write Scratchpad registers APIs and PMIC nSLEEP Setup APIs.
Files | |
file | pmic_core.h |
PMIC Driver Common API/interface file. | |
file | pmic_types.h |
PMIC Driver Common data types file. | |
Data Structures | |
struct | Pmic_RecovCntCfg_t |
PMIC Recovery Counter Configuration Note: validParams is input param for all Set and Get APIs. other params except validParams is input param for Set APIS and output param for Get APIs. More... | |
struct | Pmic_CommonCtrlCfg_t |
PMIC common control param configuration Note: validParams is input param for all Set and Get APIs. other params except validParams is input param for Set APIs and output param for Get APIs. More... | |
struct | Pmic_MiscCtrlCfg_t |
PMIC Miscellaneous control param Configuration Note: validParams is input param for all Set and Get APIs. other params except validParams is input param for Set APIs and output param for Get APIs. More... | |
struct | Pmic_BatteryCtrlCfg_t |
PMIC Backup Battery control param Configuration Note: validParams is input param for all Set and Get APIs. other params except validParams is input param for Set APIs and output param for Get APIs. More... | |
struct | Pmic_CommonCtrlStat_t |
PMIC common control param status Note: validParams is input param for all Get APIs. other params except validParams is output param for Get APIs. More... | |
struct | Pmic_DeviceInfo_t |
PMIC Device Information. More... | |
struct | Pmic_DevSubSysInfo_t |
PMIC Subsystems. More... | |
struct | Pmic_CoreHandle_t |
PMIC Interface Handle. Contains various PMIC driver instance specific information. like, the PMIC device type, PMIC interface mode, Slave addresses, various application defined API function pointers for LLD and Critical sections. More... | |
Functions | |
int32_t | Pmic_setRecoveryCntCfg (Pmic_CoreHandle_t *pPmicCoreHandle, const Pmic_RecovCntCfg_t recovCntCfg) |
API to Set Recovery Counter Configuration. More... | |
int32_t | Pmic_getRecoveryCntCfg (Pmic_CoreHandle_t *pPmicCoreHandle, Pmic_RecovCntCfg_t *pRecovCntCfg) |
API to Get Recovery Counter Configuration. More... | |
int32_t | Pmic_getRecoveryCnt (Pmic_CoreHandle_t *pPmicCoreHandle, uint8_t *pRecovCntVal) |
API to Read Recovery Count Value. More... | |
int32_t | Pmic_setScratchPadValue (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t scratchPadRegNum, const uint8_t data) |
API to set/write value in/to scratchpad register. More... | |
int32_t | Pmic_getScratchPadValue (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t scratchPadRegNum, uint8_t *pData) |
API to get/read data from scratchpad register. More... | |
int32_t | Pmic_setUserSpareValue (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t userSpareRegNum, const uint8_t data) |
API to set/write value in/to User Spare register. More... | |
int32_t | Pmic_getUserSpareValue (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t userSpareRegNum, uint8_t *pData) |
API to get/read data from User Spare register. More... | |
int32_t | Pmic_setCommonCtrlConfig (Pmic_CoreHandle_t *pPmicCoreHandle, const Pmic_CommonCtrlCfg_t commonCtrlCfg) |
API to set PMIC common control parameter configuration. More... | |
int32_t | Pmic_getCommonCtrlConfig (Pmic_CoreHandle_t *pPmicCoreHandle, Pmic_CommonCtrlCfg_t *pCommonCtrlCfg) |
API to get PMIC common control parameter configuration. More... | |
int32_t | Pmic_setMiscCtrlConfig (Pmic_CoreHandle_t *pPmicCoreHandle, const Pmic_MiscCtrlCfg_t miscCtrlCfg) |
API to set PMIC Miscellaneous control parameter configuration. More... | |
int32_t | Pmic_getMiscCtrlConfig (Pmic_CoreHandle_t *pPmicCoreHandle, Pmic_MiscCtrlCfg_t *pMiscCtrlCfg) |
API to get PMIC Miscellaneous control parameter configuration. More... | |
int32_t | Pmic_setBatteryCtrlConfig (Pmic_CoreHandle_t *pPmicCoreHandle, const Pmic_BatteryCtrlCfg_t batteryCtrlCfg) |
API to set PMIC Battery Backup control parameter configuration. More... | |
int32_t | Pmic_getBatteryCtrlConfig (Pmic_CoreHandle_t *pPmicCoreHandle, Pmic_BatteryCtrlCfg_t *pBatteryCtrlCfg) |
API to get PMIC Battery Backup control parameter configuration. Note: validParams is input param for all Set and Get APIs. other params except validParams is input param for Set APIs and output param for Get APIs. More... | |
int32_t | Pmic_getPinValue (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t pinType, uint8_t *pPinValue) |
API to get PMIC GPIO NRSTOUT_SOC/ NRSTOUT/ EN_DRV Pin. More... | |
int32_t | Pmic_getCommonCtrlStat (Pmic_CoreHandle_t *pPmicCoreHandle, Pmic_CommonCtrlStat_t *pCommonCtrlStat) |
API to get PMIC common control parameter status. More... | |
int32_t | Pmic_getI2CSpeed (Pmic_CoreHandle_t *pPmicCoreHandle, uint8_t *pI2C1Speed, uint8_t *pI2C2Speed) |
API to get configured value for I2C1 or I2C2 Speed based on commMode. More... | |
int32_t | Pmic_enableCRC (Pmic_CoreHandle_t *pPmicCoreHandle) |
API to Enable CRC. More... | |
int32_t | Pmic_getCrcStatus (Pmic_CoreHandle_t *pPmicCoreHandle, uint8_t *pI2c1SpiCrcStatus, uint8_t *pI2c2CrcStatus) |
API to get CRC Status. More... | |
int32_t | Pmic_getDeviceInfo (Pmic_CoreHandle_t *pPmicCoreHandle, Pmic_DeviceInfo_t *pDeviceInfo) |
API to get PMIC Device Information. More... | |
int32_t | Pmic_setI2CSpeedCfg (Pmic_CoreHandle_t *pPmicCoreHandle) |
API to set I2C1 or I2C2 Speed based on commMode. More... | |
Macros | |
#define | DRV_INIT_SUCCESS (0xABCD0000U) |
PMIC driver Core Handle INIT status Magic Number. Used to validate Handle to avoid corrupted PmicHandle usage. on Success: (DRV_INIT_SUCCESS | Pmic_InstType_t) More... | |
#define | PMIC_SILICON_REV_ID_PG_2_0 (0x08U) |
Silicon Revision Id - PG 2.0 for TPS6594x Leo and LP8764x Hera. More... | |
#define | PMIC_SILICON_REV_ID_PG_1_0 (0x0U) |
Silicon Revision Id - PG 1.0 for TPS6594x Leo and LP8764x Hera. More... | |
PMIC Recovery Counter Configuration Type | |
#define | PMIC_CFG_RECOV_CNT_THR_VAL_VALID (0U) |
validParams value used to set/get Recovery Counter Threshold Value More... | |
#define | PMIC_CFG_RECOV_CNT_CLR_CNT_VALID (1U) |
validParams value used to Clear/get Recovery Counter Value More... | |
PMIC Recovery Count Configuration Structure Param Bit shift values | |
Application can use below shifted values to set the validParams struct members defined in Pmic_RecovCntCfg_t structure | |
#define | PMIC_CFG_RECOV_CNT_THR_VAL_VALID_SHIFT (1U << PMIC_CFG_RECOV_CNT_THR_VAL_VALID) |
#define | PMIC_CFG_RECOV_CNT_CLR_CNT_VALID_SHIFT (1U << PMIC_CFG_RECOV_CNT_CLR_CNT_VALID) |
PMIC Scratchpad register selection | |
#define | PMIC_SCRATCH_PAD_REG_1 (0x0U) |
#define | PMIC_SCRATCH_PAD_REG_2 (0x1U) |
#define | PMIC_SCRATCH_PAD_REG_3 (0x2U) |
#define | PMIC_SCRATCH_PAD_REG_4 (0x3U) |
PMIC User Spare register selection | |
#define | PMIC_USER_SPARE_REG_1 (0x0U) |
#define | PMIC_USER_SPARE_REG_2 (0x1U) |
#define | PMIC_USER_SPARE_REG_3 (0x2U) |
#define | PMIC_USER_SPARE_REG_4 (0x3U) |
PMIC User Spare register Value | |
#define | PMIC_USER_SPARE_REG_VAL_0 (0x0U) |
#define | PMIC_USER_SPARE_REG_VAL_1 (0x1U) |
PMIC Common control param status Structure Param Bits | |
PMIC valid params configuration type for the structure member validParams of Pmic_CommonCtrlStat_t structure | |
#define | PMIC_CFG_BB_EOC_INDICATION_STAT_VALID (0U) |
validParams value used to get Backup Battery End of charge Indication Status More... | |
#define | PMIC_CFG_REGISTER_LOCK_STAT_VALID (1U) |
validParams value used to get Register lock status More... | |
#define | PMIC_CFG_EXT_CLK_VALIDITY_STAT_VALID (2U) |
validParams value used to get External clock validity status More... | |
#define | PMIC_CFG_STARTUP_PIN_STAT_VALID (3U) |
validParams value used to get Startup(nPWRON/Enable) pin status More... | |
#define | PMIC_CFG_EN_DRV_PIN_STAT_VALID (4U) |
validParams value used to get EN_DRV Pin status More... | |
#define | PMIC_CFG_NRSTOUTSOC_PIN_STAT_VALID (5U) |
validParams value used to get nRSTOUT_SOC Pin status More... | |
#define | PMIC_CFG_NRSTOUT_PIN_STAT_VALID (6U) |
validParams value used to get nRSTOUT Pin status More... | |
#define | PMIC_CFG_NINT_PIN_STAT_VALID (7U) |
validParams value used to get nINT Pin status More... | |
#define | PMIC_CFG_SPMI_LPM_STAT_VALID (8U) |
validParams value used to get SPMI Low Power Mode status More... | |
#define | PMIC_CFG_FORCE_ENABLE_DRV_LOW_STAT_VALID (9U) |
validParams value used to get status of ENABLE_DRV Configuration by I2C/SPI More... | |
PMIC Common Control param status valid param bit shift values | |
Application can use below shifted values to set the validParam member defined in Pmic_CommonCtrlStat_t structure | |
#define | PMIC_CFG_BB_EOC_INDICATION_STAT_VALID_SHIFT (1U << PMIC_CFG_BB_EOC_INDICATION_STAT_VALID) |
#define | PMIC_CFG_REGISTER_LOCK_STAT_VALID_SHIFT (1U << PMIC_CFG_REGISTER_LOCK_STAT_VALID) |
#define | PMIC_CFG_EXT_CLK_VALIDITY_STAT_VALID_SHIFT (1U << PMIC_CFG_EXT_CLK_VALIDITY_STAT_VALID) |
#define | PMIC_CFG_STARTUP_PIN_STAT_VALID_SHIFT (1U << PMIC_CFG_STARTUP_PIN_STAT_VALID) |
#define | PMIC_CFG_EN_DRV_PIN_STAT_VALID_SHIFT (1U << PMIC_CFG_EN_DRV_PIN_STAT_VALID) |
#define | PMIC_CFG_NRSTOUTSOC_PIN_STAT_VALID_SHIFT (1U << PMIC_CFG_NRSTOUTSOC_PIN_STAT_VALID) |
#define | PMIC_CFG_NRSTOUT_PIN_STAT_VALID_SHIFT (1U << PMIC_CFG_NRSTOUT_PIN_STAT_VALID) |
#define | PMIC_CFG_NINT_PIN_STAT_VALID_SHIFT (1U << PMIC_CFG_NINT_PIN_STAT_VALID) |
#define | PMIC_CFG_SPMI_LPM_STAT_VALID_SHIFT (1U << PMIC_CFG_SPMI_LPM_STAT_VALID) |
#define | PMIC_CFG_FORCE_ENABLE_DRV_LOW_STAT_VALID_SHIFT (1U << PMIC_CFG_FORCE_ENABLE_DRV_LOW_STAT_VALID) |
PMIC signal level of the STARTUP(NPWRON/ENABLE)/ NINT / NRSTOUT_SOC/ | |
#define | PMIC_PIN_SIGNAL_LEVEL_LOW (0U) |
#define | PMIC_PIN_SIGNAL_LEVEL_HIGH (1U) |
PMIC Pin Type Selection as NRSTOUT_SOC/ NRSTOUT/ EN_DRV | |
#define | PMIC_PIN_TYPE_EN_DRV (0U) |
#define | PMIC_PIN_TYPE_NRSTOUT_SOC (1U) |
#define | PMIC_PIN_TYPE_NRSTOUT (2U) |
PMIC ENABLE_DRV I2C/SPI configuration status | |
#define | PMIC_ENABLE_DRV_I2C_SPI_CONFIG_ENABLE (0U) |
#define | PMIC_ENABLE_DRV_I2C_SPI_CONFIG_DISABLE (1U) |
PMIC Register Lock Configuration | |
#define | PMIC_REGISTER_UNLOCK (0x9BU) |
Unlock PMIC Registers. More... | |
#define | PMIC_REGISTER_LOCK (0x10U) |
Lock PMIC Registers - Write any value other than 0x9B. Here 0x10 is used. More... | |
PMIC Register Lock Status | |
#define | PMIC_REGISTER_STATUS_UNLOCK (0x0U) |
#define | PMIC_REGISTER_STATUS_LOCK (0x1U) |
PMIC Spread Spectrum Configuration | |
#define | PMIC_SPREAD_SPECTRUM_CFG_DISABLE (0U) |
Disable Spread Spectrum Configuration. More... | |
#define | PMIC_SPREAD_SPECTRUM_CFG_ENABLE (1U) |
Enable Spread Spectrum Configuration. More... | |
PMIC Spread Spectrum Modulation Depth Sel | |
#define | PMIC_SPREAD_SPECTRUM_MODULATION_DEPTH_NONE (0U) |
No Modulation. More... | |
#define | PMIC_SPREAD_SPECTRUM_MODULATION_DEPTH_6_3_PERCENT (1U) |
Modulation Depth as +/- 6.3%. More... | |
#define | PMIC_SPREAD_SPECTRUM_MODULATION_DEPTH_8_4_PERCENT (2U) |
Modulation Depth as +/- 8.4%. More... | |
PMIC SPMI LPM Mode Control Status | |
#define | PMIC_SPMI_LPM_MODE_CTRL_CFG_DISABLED (0U) |
SPMI LPM Mode Control Configuration is Disabled. More... | |
#define | PMIC_SPMI_LPM_MODE_CTRL_CFG_ENABLED (1U) |
SPMI LPM Mode Control Configuration is Enabled. More... | |
PMIC Internal Clock Monitoring Configuration | |
#define | PMIC_INTERNAL_CLK_MONITORING_CFG_DISABLE (0U) |
Disable Internal Clock Monitoring. More... | |
#define | PMIC_INTERNAL_CLK_MONITORING_CFG_ENABLE (1U) |
Enable Internal Clock Monitoring. More... | |
PMIC SYNCCLKOUT Frequency selection | |
#define | PMIC_SYNCCLKOUT_DISABLE (0U) |
DISABLE SYNCCLKOUT. More... | |
#define | PMIC_SYNCCLKOUT_1_1_MHZ (1U) |
SYNCCLKOUT Frequency as 1.1 MHz. More... | |
#define | PMIC_SYNCCLKOUT_2_2_MHZ (2U) |
SYNCCLKOUT Frequency as 2.2 MHz. More... | |
#define | PMIC_SYNCCLKOUT_4_4_MHZ (3U) |
SYNCCLKOUT Frequency as 4.4 MHz. More... | |
PMIC External Clock selection | |
#define | PMIC_INTERNAL_RC_OSC (0U) |
Forced to Internal RC Oscillator. More... | |
#define | PMIC_AUTOMATIC_EXT_CLK (1U) |
Selects External clock when Available. More... | |
PMIC External Clock Validity Status | |
#define | PMIC_EXT_CLK_STATUS_VALID (0U) |
#define | PMIC_EXT_CLK_STATUS_INVALID (1U) |
PMIC CRC Status for I2C1/I2C2/SPI | |
#define | PMIC_CRC_STATUS_DISABLED (0U) |
CRC is disabled. More... | |
#define | PMIC_CRC_STATUS_ENABLED (1U) |
CRC is enabled. More... | |
PMIC Common Control Configuration Structure Param Bits | |
PMIC valid params configuration type for the structure member validParams of Pmic_CommonCtrlCfg_t structure | |
#define | PMIC_CFG_SPREAD_SPECTRUM_EN_VALID (0U) |
validParams value used to set/get Spread Spectrum Enable/Disable More... | |
#define | PMIC_CFG_ENABLE_DRV_VALID (1U) |
validParams value used to set/get ENABLE_DRV pin configuration More... | |
#define | PMIC_CFG_REG_LOCK_VALID (2U) |
validParams value used to set/get Register Lock configuration More... | |
#define | PMIC_CFG_SPREAD_SPECTRUM_DEPTH_VALID (3U) |
validParams value used to set/get Spread Spectrum modulation Depth Value More... | |
#define | PMIC_CFG_EEPROM_DEFAULT_VALID (4U) |
validParams value used to set/get to Enable/Disable load from EEPROM defaults on RTC Domain(TPS6594X Leo)/ conf(LP8764x Hera) registers More... | |
#define | PMIC_CFG_SKIP_EEPROM_LOAD_VALID (5U) |
validParams value used to set/get to Enable/Disable to skip EEPROM defaults load on conf and Other registers Valid only for LP8764x Hera More... | |
PMIC Common Control Configuration valid param bit shift values | |
Application can use below shifted values to set the validParam member defined in Pmic_CommonCtrlCfg_t structure | |
#define | PMIC_CFG_SPREAD_SPECTRUM_EN_VALID_SHIFT (1U << PMIC_CFG_SPREAD_SPECTRUM_EN_VALID) |
#define | PMIC_CFG_ENABLE_DRV_VALID_SHIFT (1U << PMIC_CFG_ENABLE_DRV_VALID) |
#define | PMIC_CFG_REG_LOCK_VALID_SHIFT (1U << PMIC_CFG_REG_LOCK_VALID) |
#define | PMIC_CFG_SPREAD_SPECTRUM_DEPTH_VALID_SHIFT (1U << PMIC_CFG_SPREAD_SPECTRUM_DEPTH_VALID) |
#define | PMIC_CFG_EEPROM_DEFAULT_VALID_SHIFT (1U << PMIC_CFG_EEPROM_DEFAULT_VALID) |
#define | PMIC_CFG_SKIP_EEPROM_LOAD_VALID_SHIFT (1U << PMIC_CFG_SKIP_EEPROM_LOAD_VALID) |
PMIC Miscellaneous Control Configuration Structure Param Bits | |
PMIC valid params configuration type for the structure member validParams of Pmic_MiscCtrlCfg_t structure | |
#define | PMIC_CFG_AMUX_OUT_REF_OUT_EN_VALID (0U) |
validParams value used to set/get to Enable/Disable Band gap Voltage to AMUX OUT/REF OUT Pin More... | |
#define | PMIC_CFG_CLK_MON_EN_VALID (1U) |
validParams value used to set/get to Enable or Disable internal Clock Monitoring More... | |
#define | PMIC_CFG_SYNC_CLK_OUT_FREQ_SEL_VALID (2U) |
validParams value used to set/get to Select SYNCCLKOUT Frequency More... | |
#define | PMIC_CFG_EXT_CLK_SEL_VALID (3U) |
validParams value used to set/get External clock Selection More... | |
#define | PMIC_CFG_SYNC_CLK_IN_FREQ_VALID (4U) |
validParams value used to set/get to Select External clock Frequency More... | |
#define | PMIC_CFG_NRSTOUT_SOC_VALID (5U) |
validParams value used to set/get to NRSTOUT_SOC Signal More... | |
#define | PMIC_CFG_NRSTOUT_VALID (6U) |
validParams value used to set/get NRSTOUT Signal More... | |
PMIC Miscellaneous Control Configuration valid param bit shift | |
Application can use below shifted values to set the validParam member defined in Pmic_MiscCtrlCfg_t structure | |
#define | PMIC_CFG_AMUX_OUT_REF_OUT_EN_VALID_SHIFT (1U << PMIC_CFG_AMUX_OUT_REF_OUT_EN_VALID) |
#define | PMIC_CFG_CLK_MON_EN_VALID_SHIFT (1U << PMIC_CFG_CLK_MON_EN_VALID) |
#define | PMIC_CFG_SYNC_CLK_OUT_FREQ_SEL_VALID_SHIFT (1U << PMIC_CFG_SYNC_CLK_OUT_FREQ_SEL_VALID) |
#define | PMIC_CFG_EXT_CLK_SEL_VALID_SHIFT (1U << PMIC_CFG_EXT_CLK_SEL_VALID) |
#define | PMIC_CFG_SYNC_CLK_IN_FREQ_VALID_SHIFT (1U << PMIC_CFG_SYNC_CLK_IN_FREQ_VALID) |
#define | PMIC_CFG_NRSTOUT_SOC_VALID_SHIFT (1U << PMIC_CFG_NRSTOUT_SOC_VALID) |
#define | PMIC_CFG_NRSTOUT_VALID_SHIFT (1U << PMIC_CFG_NRSTOUT_VALID) |
PMIC Backup Battery Control Configuration Structure Param Bits | |
PMIC valid params configuration type for the structure member validParams of Pmic_BatteryCtrlCfg_t structure | |
#define | PMIC_CFG_CHARGING_EN_VALID (0U) |
validParams value used to set/get to Enable/Disable Backup Battery Charging More... | |
#define | PMIC_CFG_END_OF_CHARGE_VOLTAGE_VALID (1U) |
validParams value used to set/get to Backup Battery configuration for End of charge Voltage More... | |
#define | PMIC_CFG_CHARGE_CURRENT_VALID (2U) |
validParams value used to set/get to Backup Battery charging current value More... | |
PMIC Backup Battery Control Configuration valid param bit shift | |
Application can use below shifted values to set the validParam member defined in Pmic_BatteryCtrlCfg_t structure | |
#define | PMIC_CFG_CHARGING_EN_VALID_SHIFT (1U << PMIC_CFG_CHARGING_EN_VALID) |
#define | PMIC_CFG_END_OF_CHARGE_VOLTAGE_VALID_SHIFT (1U << PMIC_CFG_END_OF_CHARGE_VOLTAGE_VALID) |
#define | PMIC_CFG_CHARGE_CURRENT_VALID_SHIFT (1U << PMIC_CFG_CHARGE_CURRENT_VALID) |
PMIC CRC Enable/Disable Configuration | |
#define | PMIC_CRC_DISABLE (0U) |
#define | PMIC_CRC_ENABLE (1U) |
#define DRV_INIT_SUCCESS (0xABCD0000U) |
PMIC driver Core Handle INIT status Magic Number. Used to validate Handle to avoid corrupted PmicHandle usage. on Success: (DRV_INIT_SUCCESS | Pmic_InstType_t)
#define PMIC_SILICON_REV_ID_PG_2_0 (0x08U) |
Silicon Revision Id - PG 2.0 for TPS6594x Leo and LP8764x Hera.
#define PMIC_SILICON_REV_ID_PG_1_0 (0x0U) |
Silicon Revision Id - PG 1.0 for TPS6594x Leo and LP8764x Hera.
#define PMIC_CFG_RECOV_CNT_THR_VAL_VALID (0U) |
validParams value used to set/get Recovery Counter Threshold Value
#define PMIC_CFG_RECOV_CNT_CLR_CNT_VALID (1U) |
validParams value used to Clear/get Recovery Counter Value
#define PMIC_CFG_RECOV_CNT_THR_VAL_VALID_SHIFT (1U << PMIC_CFG_RECOV_CNT_THR_VAL_VALID) |
#define PMIC_CFG_RECOV_CNT_CLR_CNT_VALID_SHIFT (1U << PMIC_CFG_RECOV_CNT_CLR_CNT_VALID) |
#define PMIC_SCRATCH_PAD_REG_1 (0x0U) |
#define PMIC_SCRATCH_PAD_REG_2 (0x1U) |
#define PMIC_SCRATCH_PAD_REG_3 (0x2U) |
#define PMIC_SCRATCH_PAD_REG_4 (0x3U) |
#define PMIC_USER_SPARE_REG_1 (0x0U) |
#define PMIC_USER_SPARE_REG_2 (0x1U) |
#define PMIC_USER_SPARE_REG_3 (0x2U) |
#define PMIC_USER_SPARE_REG_4 (0x3U) |
#define PMIC_USER_SPARE_REG_VAL_0 (0x0U) |
#define PMIC_USER_SPARE_REG_VAL_1 (0x1U) |
#define PMIC_CFG_BB_EOC_INDICATION_STAT_VALID (0U) |
validParams value used to get Backup Battery End of charge Indication Status
#define PMIC_CFG_REGISTER_LOCK_STAT_VALID (1U) |
validParams value used to get Register lock status
#define PMIC_CFG_EXT_CLK_VALIDITY_STAT_VALID (2U) |
validParams value used to get External clock validity status
#define PMIC_CFG_STARTUP_PIN_STAT_VALID (3U) |
validParams value used to get Startup(nPWRON/Enable) pin status
#define PMIC_CFG_EN_DRV_PIN_STAT_VALID (4U) |
validParams value used to get EN_DRV Pin status
#define PMIC_CFG_NRSTOUTSOC_PIN_STAT_VALID (5U) |
validParams value used to get nRSTOUT_SOC Pin status
#define PMIC_CFG_NRSTOUT_PIN_STAT_VALID (6U) |
validParams value used to get nRSTOUT Pin status
#define PMIC_CFG_NINT_PIN_STAT_VALID (7U) |
validParams value used to get nINT Pin status
#define PMIC_CFG_SPMI_LPM_STAT_VALID (8U) |
validParams value used to get SPMI Low Power Mode status
#define PMIC_CFG_FORCE_ENABLE_DRV_LOW_STAT_VALID (9U) |
validParams value used to get status of ENABLE_DRV Configuration by I2C/SPI
#define PMIC_CFG_BB_EOC_INDICATION_STAT_VALID_SHIFT (1U << PMIC_CFG_BB_EOC_INDICATION_STAT_VALID) |
#define PMIC_CFG_REGISTER_LOCK_STAT_VALID_SHIFT (1U << PMIC_CFG_REGISTER_LOCK_STAT_VALID) |
#define PMIC_CFG_EXT_CLK_VALIDITY_STAT_VALID_SHIFT (1U << PMIC_CFG_EXT_CLK_VALIDITY_STAT_VALID) |
#define PMIC_CFG_STARTUP_PIN_STAT_VALID_SHIFT (1U << PMIC_CFG_STARTUP_PIN_STAT_VALID) |
#define PMIC_CFG_EN_DRV_PIN_STAT_VALID_SHIFT (1U << PMIC_CFG_EN_DRV_PIN_STAT_VALID) |
#define PMIC_CFG_NRSTOUTSOC_PIN_STAT_VALID_SHIFT (1U << PMIC_CFG_NRSTOUTSOC_PIN_STAT_VALID) |
#define PMIC_CFG_NRSTOUT_PIN_STAT_VALID_SHIFT (1U << PMIC_CFG_NRSTOUT_PIN_STAT_VALID) |
#define PMIC_CFG_NINT_PIN_STAT_VALID_SHIFT (1U << PMIC_CFG_NINT_PIN_STAT_VALID) |
#define PMIC_CFG_SPMI_LPM_STAT_VALID_SHIFT (1U << PMIC_CFG_SPMI_LPM_STAT_VALID) |
#define PMIC_CFG_FORCE_ENABLE_DRV_LOW_STAT_VALID_SHIFT (1U << PMIC_CFG_FORCE_ENABLE_DRV_LOW_STAT_VALID) |
#define PMIC_PIN_SIGNAL_LEVEL_LOW (0U) |
#define PMIC_PIN_SIGNAL_LEVEL_HIGH (1U) |
#define PMIC_PIN_TYPE_EN_DRV (0U) |
#define PMIC_PIN_TYPE_NRSTOUT_SOC (1U) |
#define PMIC_PIN_TYPE_NRSTOUT (2U) |
#define PMIC_ENABLE_DRV_I2C_SPI_CONFIG_ENABLE (0U) |
#define PMIC_ENABLE_DRV_I2C_SPI_CONFIG_DISABLE (1U) |
#define PMIC_REGISTER_UNLOCK (0x9BU) |
Unlock PMIC Registers.
#define PMIC_REGISTER_LOCK (0x10U) |
Lock PMIC Registers - Write any value other than 0x9B. Here 0x10 is used.
#define PMIC_REGISTER_STATUS_UNLOCK (0x0U) |
#define PMIC_REGISTER_STATUS_LOCK (0x1U) |
#define PMIC_SPREAD_SPECTRUM_CFG_DISABLE (0U) |
Disable Spread Spectrum Configuration.
#define PMIC_SPREAD_SPECTRUM_CFG_ENABLE (1U) |
Enable Spread Spectrum Configuration.
#define PMIC_SPREAD_SPECTRUM_MODULATION_DEPTH_NONE (0U) |
No Modulation.
#define PMIC_SPREAD_SPECTRUM_MODULATION_DEPTH_6_3_PERCENT (1U) |
Modulation Depth as +/- 6.3%.
#define PMIC_SPREAD_SPECTRUM_MODULATION_DEPTH_8_4_PERCENT (2U) |
Modulation Depth as +/- 8.4%.
#define PMIC_SPMI_LPM_MODE_CTRL_CFG_DISABLED (0U) |
SPMI LPM Mode Control Configuration is Disabled.
#define PMIC_SPMI_LPM_MODE_CTRL_CFG_ENABLED (1U) |
SPMI LPM Mode Control Configuration is Enabled.
#define PMIC_INTERNAL_CLK_MONITORING_CFG_DISABLE (0U) |
Disable Internal Clock Monitoring.
#define PMIC_INTERNAL_CLK_MONITORING_CFG_ENABLE (1U) |
Enable Internal Clock Monitoring.
#define PMIC_SYNCCLKOUT_DISABLE (0U) |
DISABLE SYNCCLKOUT.
#define PMIC_SYNCCLKOUT_1_1_MHZ (1U) |
SYNCCLKOUT Frequency as 1.1 MHz.
#define PMIC_SYNCCLKOUT_2_2_MHZ (2U) |
SYNCCLKOUT Frequency as 2.2 MHz.
#define PMIC_SYNCCLKOUT_4_4_MHZ (3U) |
SYNCCLKOUT Frequency as 4.4 MHz.
#define PMIC_INTERNAL_RC_OSC (0U) |
Forced to Internal RC Oscillator.
#define PMIC_AUTOMATIC_EXT_CLK (1U) |
Selects External clock when Available.
#define PMIC_EXT_CLK_STATUS_VALID (0U) |
#define PMIC_EXT_CLK_STATUS_INVALID (1U) |
#define PMIC_CRC_STATUS_DISABLED (0U) |
CRC is disabled.
#define PMIC_CRC_STATUS_ENABLED (1U) |
CRC is enabled.
#define PMIC_CFG_SPREAD_SPECTRUM_EN_VALID (0U) |
validParams value used to set/get Spread Spectrum Enable/Disable
#define PMIC_CFG_ENABLE_DRV_VALID (1U) |
validParams value used to set/get ENABLE_DRV pin configuration
#define PMIC_CFG_REG_LOCK_VALID (2U) |
validParams value used to set/get Register Lock configuration
#define PMIC_CFG_SPREAD_SPECTRUM_DEPTH_VALID (3U) |
validParams value used to set/get Spread Spectrum modulation Depth Value
#define PMIC_CFG_EEPROM_DEFAULT_VALID (4U) |
validParams value used to set/get to Enable/Disable load from EEPROM defaults on RTC Domain(TPS6594X Leo)/ conf(LP8764x Hera) registers
#define PMIC_CFG_SKIP_EEPROM_LOAD_VALID (5U) |
validParams value used to set/get to Enable/Disable to skip EEPROM defaults load on conf and Other registers Valid only for LP8764x Hera
#define PMIC_CFG_SPREAD_SPECTRUM_EN_VALID_SHIFT (1U << PMIC_CFG_SPREAD_SPECTRUM_EN_VALID) |
#define PMIC_CFG_ENABLE_DRV_VALID_SHIFT (1U << PMIC_CFG_ENABLE_DRV_VALID) |
#define PMIC_CFG_REG_LOCK_VALID_SHIFT (1U << PMIC_CFG_REG_LOCK_VALID) |
#define PMIC_CFG_SPREAD_SPECTRUM_DEPTH_VALID_SHIFT (1U << PMIC_CFG_SPREAD_SPECTRUM_DEPTH_VALID) |
#define PMIC_CFG_EEPROM_DEFAULT_VALID_SHIFT (1U << PMIC_CFG_EEPROM_DEFAULT_VALID) |
#define PMIC_CFG_SKIP_EEPROM_LOAD_VALID_SHIFT (1U << PMIC_CFG_SKIP_EEPROM_LOAD_VALID) |
#define PMIC_CFG_AMUX_OUT_REF_OUT_EN_VALID (0U) |
validParams value used to set/get to Enable/Disable Band gap Voltage to AMUX OUT/REF OUT Pin
#define PMIC_CFG_CLK_MON_EN_VALID (1U) |
validParams value used to set/get to Enable or Disable internal Clock Monitoring
#define PMIC_CFG_SYNC_CLK_OUT_FREQ_SEL_VALID (2U) |
validParams value used to set/get to Select SYNCCLKOUT Frequency
#define PMIC_CFG_EXT_CLK_SEL_VALID (3U) |
validParams value used to set/get External clock Selection
#define PMIC_CFG_SYNC_CLK_IN_FREQ_VALID (4U) |
validParams value used to set/get to Select External clock Frequency
#define PMIC_CFG_NRSTOUT_SOC_VALID (5U) |
validParams value used to set/get to NRSTOUT_SOC Signal
#define PMIC_CFG_NRSTOUT_VALID (6U) |
validParams value used to set/get NRSTOUT Signal
#define PMIC_CFG_AMUX_OUT_REF_OUT_EN_VALID_SHIFT (1U << PMIC_CFG_AMUX_OUT_REF_OUT_EN_VALID) |
#define PMIC_CFG_CLK_MON_EN_VALID_SHIFT (1U << PMIC_CFG_CLK_MON_EN_VALID) |
#define PMIC_CFG_SYNC_CLK_OUT_FREQ_SEL_VALID_SHIFT (1U << PMIC_CFG_SYNC_CLK_OUT_FREQ_SEL_VALID) |
#define PMIC_CFG_EXT_CLK_SEL_VALID_SHIFT (1U << PMIC_CFG_EXT_CLK_SEL_VALID) |
#define PMIC_CFG_SYNC_CLK_IN_FREQ_VALID_SHIFT (1U << PMIC_CFG_SYNC_CLK_IN_FREQ_VALID) |
#define PMIC_CFG_NRSTOUT_SOC_VALID_SHIFT (1U << PMIC_CFG_NRSTOUT_SOC_VALID) |
#define PMIC_CFG_NRSTOUT_VALID_SHIFT (1U << PMIC_CFG_NRSTOUT_VALID) |
#define PMIC_CFG_CHARGING_EN_VALID (0U) |
validParams value used to set/get to Enable/Disable Backup Battery Charging
#define PMIC_CFG_END_OF_CHARGE_VOLTAGE_VALID (1U) |
validParams value used to set/get to Backup Battery configuration for End of charge Voltage
#define PMIC_CFG_CHARGE_CURRENT_VALID (2U) |
validParams value used to set/get to Backup Battery charging current value
#define PMIC_CFG_CHARGING_EN_VALID_SHIFT (1U << PMIC_CFG_CHARGING_EN_VALID) |
#define PMIC_CFG_END_OF_CHARGE_VOLTAGE_VALID_SHIFT (1U << PMIC_CFG_END_OF_CHARGE_VOLTAGE_VALID) |
#define PMIC_CFG_CHARGE_CURRENT_VALID_SHIFT (1U << PMIC_CFG_CHARGE_CURRENT_VALID) |
#define PMIC_CRC_DISABLE (0U) |
#define PMIC_CRC_ENABLE (1U) |
int32_t Pmic_setRecoveryCntCfg | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
const Pmic_RecovCntCfg_t | recovCntCfg | ||
) |
API to Set Recovery Counter Configuration.
Requirement: REQ_TAG(PDK-5809) Design: did_pmic_err_recov_cnt_cfg_readback
This function configures PMIC Recovery Counter register, controlling recovery count Threshold and Clear, when corresponding validParam bit field is set in the Pmic_RecovCntCfg_t structure. For more information \ref Pmic_RecovCntCfg_t
pPmicCoreHandle | [IN] PMIC Interface Handle. |
recovCntCfg | [IN] Set configuration value for Recovery counter |
PMIC_ST_SUCCESS | in case of success or appropriate error code For valid values Pmic_ErrorCodes |
int32_t Pmic_getRecoveryCntCfg | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
Pmic_RecovCntCfg_t * | pRecovCntCfg | ||
) |
API to Get Recovery Counter Configuration.
Requirement: REQ_TAG(PDK-5809) Design: did_pmic_err_recov_cnt_cfg_readback
This function gets PMIC Recovery Counter configuration values. Like, recovery count Threshold and Clear, when corresponding validParam bit field is set in the Pmic_RecovCntCfg_t structure. For more information \ref Pmic_RecovCntCfg_t
pPmicCoreHandle | [IN] PMIC Interface Handle. |
pRecovCntCfg | [IN/OUT] Pointer to store recovery counter configuration value |
PMIC_ST_SUCCESS | in case of success or appropriate error code For valid values Pmic_ErrorCodes |
int32_t Pmic_getRecoveryCnt | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
uint8_t * | pRecovCntVal | ||
) |
API to Read Recovery Count Value.
Requirement: REQ_TAG(PDK-5809) Design: did_pmic_err_recov_cnt_cfg_readback
This function reads out the recovery count value.
pPmicCoreHandle | [IN] PMIC Interface Handle. |
pRecovCntVal | [OUT] Pointer to store recovery count value |
PMIC_ST_SUCCESS | in case of success or appropriate error code For valid values Pmic_ErrorCodes |
int32_t Pmic_setScratchPadValue | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
const uint8_t | scratchPadRegNum, | ||
const uint8_t | data | ||
) |
API to set/write value in/to scratchpad register.
Requirement: REQ_TAG(PDK-5810), REQ_TAG(PDK-5843) Design: did_pmic_comm_single_i2c_cfg, did_pmic_comm_spi_cfg
This function is used write data to scratchpad register of PMIC
pPmicCoreHandle | [IN] PMIC Interface Handle. |
scratchPadRegNum | [IN] ScratchPad register number Valid values Pmic_ScratchPad_Sel |
data | [IN] Data/Value to be written to scratchpad. |
int32_t Pmic_getScratchPadValue | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
const uint8_t | scratchPadRegNum, | ||
uint8_t * | pData | ||
) |
API to get/read data from scratchpad register.
Requirement: REQ_TAG(PDK-5810), REQ_TAG(PDK-5843) Design: did_pmic_comm_single_i2c_cfg, did_pmic_comm_spi_cfg
This function is used read data from scratchpad register of PMIC
pPmicCoreHandle | [IN] PMIC Interface Handle. |
scratchPadRegNum | [IN] ScratchPad register number Valid valuesPmic_ScratchPad_Sel |
pData | [OUT] Parameter to hold the Data/Value read from scratchpad. |
int32_t Pmic_setUserSpareValue | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
const uint8_t | userSpareRegNum, | ||
const uint8_t | data | ||
) |
API to set/write value in/to User Spare register.
Requirement: REQ_TAG(PDK-9133) Design: did_pmic_user_spare_cfg_readback
This function is used write data to User Spare register of PMIC
pPmicCoreHandle | [IN] PMIC Interface Handle. |
userSpareRegNum | [IN] UserSpare register number Valid values Pmic_UserSpareReg_Sel |
data | [IN] Data/Value to be written to UserSpare register Valid values Pmic_UserSpareReg_Val |
int32_t Pmic_getUserSpareValue | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
const uint8_t | userSpareRegNum, | ||
uint8_t * | pData | ||
) |
API to get/read data from User Spare register.
Requirement: REQ_TAG(PDK-9133) Design: did_pmic_user_spare_cfg_readback
This function is used read data from User Spare register of PMIC
pPmicCoreHandle | [IN] PMIC Interface Handle. |
userSpareRegNum | [IN] User Spare register number Valid values Pmic_UserSpareReg_Sel |
pData | [OUT] Parameter to hold the Data/Value read from User Spare register. |
int32_t Pmic_setCommonCtrlConfig | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
const Pmic_CommonCtrlCfg_t | commonCtrlCfg | ||
) |
API to set PMIC common control parameter configuration.
Requirement: REQ_TAG(PDK-9112), REQ_TAG(PDK-9114), REQ_TAG(PDK-9131), REQ_TAG(PDK-9143), REQ_TAG(PDK-9111) Design: did_pmic_common_ctrl_cfg_readback
This function is used to set the required common control parameter configuration when corresponding validParam bit field is set in the Pmic_CommonCtrlCfg_t For more information \ref Pmic_CommonCtrlCfg_t
pPmicCoreHandle | [IN] PMIC Interface Handle. |
commonCtrlCfg | [IN] Set PMIC required common control parameter configuration. |
int32_t Pmic_getCommonCtrlConfig | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
Pmic_CommonCtrlCfg_t * | pCommonCtrlCfg | ||
) |
API to get PMIC common control parameter configuration.
Requirement: REQ_TAG(PDK-9112), REQ_TAG(PDK-9114), REQ_TAG(PDK-9131), REQ_TAG(PDK-9143) Design: did_pmic_common_ctrl_cfg_readback
This function is used to get the required common control parameter configuration when corresponding validParam bit field is set in the Pmic_CommonCtrlCfg_t For more information \ref Pmic_CommonCtrlCfg_t
pPmicCoreHandle | [IN] PMIC Interface Handle. |
pCommonCtrlCfg | [IN/OUT] Pointer to store PMIC required common control parameter configuration. |
int32_t Pmic_setMiscCtrlConfig | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
const Pmic_MiscCtrlCfg_t | miscCtrlCfg | ||
) |
API to set PMIC Miscellaneous control parameter configuration.
Requirement: REQ_TAG(PDK-9132), REQ_TAG(PDK-9127), REQ_TAG(PDK-9111) Design: did_pmic_misc_ctrl_cfg_readback
This function is used to set the required miscellaneous control parameter configuration when corresponding validParam bit field is set in the Pmic_MiscCtrlCfg_t For more information \ref Pmic_MiscCtrlCfg_t
pPmicCoreHandle | [IN] PMIC Interface Handle. |
miscCtrlCfg | [IN] Set PMIC required miscellaneous control parameter configuration. |
int32_t Pmic_getMiscCtrlConfig | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
Pmic_MiscCtrlCfg_t * | pMiscCtrlCfg | ||
) |
API to get PMIC Miscellaneous control parameter configuration.
Requirement: REQ_TAG(PDK-9132), REQ_TAG(PDK-9127) Design: did_pmic_misc_ctrl_cfg_readback
This function is used to get the required miscellaneous control parameter configuration when corresponding validParam bit field is set in the Pmic_MiscCtrlCfg_t For more information \ref Pmic_MiscCtrlCfg_t
pPmicCoreHandle | [IN] PMIC Interface Handle. |
pMiscCtrlCfg | [IN/OUT] Pointer to store PMIC required miscellaneous control parameter configuration. |
int32_t Pmic_setBatteryCtrlConfig | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
const Pmic_BatteryCtrlCfg_t | batteryCtrlCfg | ||
) |
API to set PMIC Battery Backup control parameter configuration.
Requirement: REQ_TAG(PDK-9130), REQ_TAG(PDK-9111) Design: did_pmic_battery_ctrl_cfg_readback
This function is used to set the required Battery Backup control parameter configuration when corresponding validParam bit field is set in the Pmic_BatteryCtrlCfg_t For more information \ref Pmic_BatteryCtrlCfg_t
pPmicCoreHandle | [IN] PMIC Interface Handle. |
batteryCtrlCfg | [IN] Set PMIC required Battery Backup control parameter configuration. |
int32_t Pmic_getBatteryCtrlConfig | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
Pmic_BatteryCtrlCfg_t * | pBatteryCtrlCfg | ||
) |
API to get PMIC Battery Backup control parameter configuration. Note: validParams is input param for all Set and Get APIs. other params except validParams is input param for Set APIs and output param for Get APIs.
Requirement: REQ_TAG(PDK-9130) Design: did_pmic_battery_ctrl_cfg_readback
This function is used to get the required Battery Backup control parameter configuration when corresponding validParam bit field is set in the Pmic_BatteryCtrlCfg_t For more information \ref Pmic_BatteryCtrlCfg_t
pPmicCoreHandle | [IN] PMIC Interface Handle. |
pBatteryCtrlCfg | [IN/OUT] Pointer to store PMIC required Battery Backup control parameter configuration |
int32_t Pmic_getPinValue | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
const uint8_t | pinType, | ||
uint8_t * | pPinValue | ||
) |
API to get PMIC GPIO NRSTOUT_SOC/ NRSTOUT/ EN_DRV Pin.
Requirement: REQ_TAG(PDK-9137), REQ_TAG(PDK-9131) Design: did_pmic_pin_readback
This function is used to read the signal level of the NRSTOUT_SOC/ NRSTOUT/ EN_DRV Pin
pPmicCoreHandle | [IN] PMIC Interface Handle |
pinType | [IN] PMIC pin type. Valid values of pin type Pmic_PinType_Sel |
pPinValue | [OUT] Pointer to store the status of pin type Valid values Pmic_SignalLvl |
int32_t Pmic_getCommonCtrlStat | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
Pmic_CommonCtrlStat_t * | pCommonCtrlStat | ||
) |
API to get PMIC common control parameter status.
Requirement: REQ_TAG(PDK-9126), REQ_TAG(PDK-9124), REQ_TAG(PDK-9130), REQ_TAG(PDK-9125), REQ_TAG(PDK-9139), REQ_TAG(PDK-9138), REQ_TAG(PDK-9112) Design: did_pmic_common_ctrl_status_readback
This function is used to get the required common control parameter status when corresponding validParam bit field is set in the Pmic_CommonCtrlStat_t For more information \ref Pmic_CommonCtrlStat_t
pPmicCoreHandle | [IN] PMIC Interface Handle. |
pCommonCtrlStat | [IN/OUT] Pointer to store PMIC required common control parameter status. |
int32_t Pmic_getI2CSpeed | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
uint8_t * | pI2C1Speed, | ||
uint8_t * | pI2C2Speed | ||
) |
API to get configured value for I2C1 or I2C2 Speed based on commMode.
Requirement: REQ_TAG(PDK-9129) Design: did_pmic_i2c_speed_readback
This function is used to get the configured value for I2C1 or I2C2 Speed based on commMode
pPmicCoreHandle | [IN] PMIC Interface Handle. |
pI2C1Speed | [OUT] Pointer to store I2C1 Speed for both PMIC_INTF_SINGLE_I2C and PMIC_INTF_DUAL_I2C interface Valid Vaues Pmic_I2CSpeedSel |
pI2C2Speed | [OUT] Pointer to store I2C2 Speed for both PMIC_INTF_DUAL_I2C interface only Valid Vaues Pmic_I2CSpeedSel |
int32_t Pmic_enableCRC | ( | Pmic_CoreHandle_t * | pPmicCoreHandle | ) |
API to Enable CRC.
Requirement: REQ_TAG(PDK-9119) Design: did_pmic_crc_enable
This function is used to enable CRC on Primary PMIC which enables CRC for I2C1, I2C2, SPI interface of both Primary and Secondary PMIC Note: Application shall not do reads and writes of the any PMIC registers for at least 2ms to allow the recalculation of the register CRC value due to the change Valid only for TPS6594x Leo PMIC PG2.0 and LP8764x Hera PMIC PG2.0
pPmicCoreHandle | [IN] PMIC Interface Handle. |
int32_t Pmic_getCrcStatus | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
uint8_t * | pI2c1SpiCrcStatus, | ||
uint8_t * | pI2c2CrcStatus | ||
) |
API to get CRC Status.
Requirement: REQ_TAG(PDK-9329) Design: did_pmic_crc_status
This function is used to get the CRC Status based on commMode
pPmicCoreHandle | [IN] PMIC Interface Handle. |
pI2c1SpiCrcStatus | [OUT] Pointer to store CRC Status for I2C1/ SPI interface Valid Vaues Pmic_CrcStatus |
pI2c2CrcStatus | [OUT] Pointer to store CRC Status for I2C2 interface Valid Vaues Pmic_CrcStatus |
int32_t Pmic_getDeviceInfo | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
Pmic_DeviceInfo_t * | pDeviceInfo | ||
) |
API to get PMIC Device Information.
Requirement: REQ_TAG(PDK-9109), REQ_TAG(PDK-9110), REQ_TAG(PDK-9149), REQ_TAG(PDK-9159), REQ_TAG(PDK-9329) Design: did_pmic_dev_info_readback
This function is used to get PMIC Device Information such as TI DeviceID, TI NVM ID, TI NVM Revision, TI Silicon Revision, Custom NVM ID Note: customNvmID is valid only for TPS6594x Leo PMIC PG2.0 and LP8764x Hera PMIC PG2.0
pPmicCoreHandle | [IN] PMIC Interface Handle. |
pDeviceInfo | [OUT] PMIC Device Information value |
int32_t Pmic_setI2CSpeedCfg | ( | Pmic_CoreHandle_t * | pPmicCoreHandle | ) |
API to set I2C1 or I2C2 Speed based on commMode.
Requirement: REQ_TAG(PDK-9129) Design: did_pmic_i2c_speed_readback
This function is used to configure I2C1 speed for Single or Dual I2C Interface and I2C2 Speed for Dual I2C Interface based on commMode. Note: I2C Master before switching the I2C speed to HS/Standard Mode, I2C Master has to configure I2C1/I2C2 speed accordingly then only I2C Master can communicate with PMIC in HS/Standard Mode
pPmicCoreHandle | [IN] PMIC Interface Handle. |