PDK API Guide for J721E
|
TimeSync protocol configuration structure.
Data Fields | |
TimeSync_NetworkProtType | protocol |
TimeSync_DeviceConfig | deviceCfg |
uint8_t | domainNumber [TIMESYNC_NUM_DOMAINS] |
uint8_t | clockIdentity [8] |
TimeSync_StepMode | stepMode |
TimeSync_VlanConfig | vlanCfg |
TimeSync_PpsConfig | ppsConfig |
uint8_t | portMask |
TimeSync_NetworkProtType TimeSync_ProtocolConfig::protocol |
Packet type in which PTP is encapsulated
TimeSync_DeviceConfig TimeSync_ProtocolConfig::deviceCfg |
Device's PTP mode of operation
uint8_t TimeSync_ProtocolConfig::domainNumber[TIMESYNC_NUM_DOMAINS] |
List of 802.1AS-rev domainNumbers
uint8_t TimeSync_ProtocolConfig::clockIdentity[8] |
Clock Identity = MAC ID + Protocol Identifier
TimeSync_StepMode TimeSync_ProtocolConfig::stepMode |
PTP step mode
TimeSync_VlanConfig TimeSync_ProtocolConfig::vlanCfg |
VLAN comfiguration
TimeSync_PpsConfig TimeSync_ProtocolConfig::ppsConfig |
PTP PPS comfiguration
uint8_t TimeSync_ProtocolConfig::portMask |
Port mask indicating ports to be used for PTP