PDK API Guide for J721E
|
Enet UDMA channel ring parameters.
Ring configuration structure for RX flow and TX channel FQ & CQ rings.
Data Fields | |
uint8_t | orderId |
uint8_t | mode |
bool | useRingMon |
EnetUdma_RingMonCfg | ringMonCfg |
uint8_t EnetUdma_UdmaRingPrms::orderId |
Ring bus order ID value to be programmed into the orderid field of the ring's RING_ORDERID register.
uint8_t EnetUdma_UdmaRingPrms::mode |
Ring mode. Refer tisci_msg_rm_ring_cfg_req::mode
bool EnetUdma_UdmaRingPrms::useRingMon |
Flag to indicate if ring monitor should be allocated for this ring. This should be enabled only for those flows that require very high throughput as there are limited ring monitors available in the system
EnetUdma_RingMonCfg EnetUdma_UdmaRingPrms::ringMonCfg |
Ring monitor config (used only if useRingMon is true)