![]() |
PDK API Guide for J721E
|
Param struct for the RX channel open.
The parameter structure for the RX channel open, containing a channel config structure.
Data Fields | |
uint8_t | dmaPriority |
uint8_t EnetUdma_RxChInitPrms::dmaPriority |
This field selects which scheduling bin the channel will be placed in for bandwidth allocation of the TX DMA units. Refer tisci_msg_rm_udmap_tx_ch_cfg_req::tx_sched_priority