![]() |
PDK API Guide for J721E
|
Param struct for the get default flowId open parameters.
The param struct for the RX flow open function The returned channel handle is an opaque variable used to access the RX Flow in other function commands.
Data Fields | |
Udma_DrvHandle | hUdmaDrv |
uint32_t | startIdx |
uint32_t | flowIdx |
EnetUdma_UdmaChPrms | udmaChPrms |
bool | useGlobalEvt |
EnetDma_PktNotifyCb | notifyCb |
EnetUdma_UdmaFlowPrms | flowPrms |
uint32_t | numRxPkts |
bool | disableCacheOpsFlag |
uint32_t | rxFlowMtu |
EnetUdma_AllocRingMemFxn | ringMemAllocFxn |
EnetUdma_FreeRingMemFxn | ringMemFreeFxn |
EnetUdma_AllocDmaDescFxn | dmaDescAllocFxn |
EnetUdma_FreeDmaDescFxn | dmaDescFreeFxn |
void * | cbArg |
bool | useProxy |
EnetUdma_AutoReclaimPrms | autoReclaimPrms |
Udma_DrvHandle EnetUdma_OpenRxFlowPrms::hUdmaDrv |
UDMA driver handle
uint32_t EnetUdma_OpenRxFlowPrms::startIdx |
Flow start index
uint32_t EnetUdma_OpenRxFlowPrms::flowIdx |
Flow index to be opened
EnetUdma_UdmaChPrms EnetUdma_OpenRxFlowPrms::udmaChPrms |
UDMA specific channel params
bool EnetUdma_OpenRxFlowPrms::useGlobalEvt |
Whether to use the shared global event or not. If set to false, a dedicated event will be used for this channel.
EnetDma_PktNotifyCb EnetUdma_OpenRxFlowPrms::notifyCb |
Enet UDMA event callback function - this function will be called when the registered packets are received on RX Flow
EnetUdma_UdmaFlowPrms EnetUdma_OpenRxFlowPrms::flowPrms |
UDMA Flow params
uint32_t EnetUdma_OpenRxFlowPrms::numRxPkts |
Number of receive packets, used for allocating number of DMA descriptors Note - The HW ring element count field is 19-bit
bool EnetUdma_OpenRxFlowPrms::disableCacheOpsFlag |
Flag to disable cache operations on the ring memory
uint32_t EnetUdma_OpenRxFlowPrms::rxFlowMtu |
Maximum receive packet length for this flow. Make sure packets of at least this length are submitted in EnetDma_submitRxPktQ()
EnetUdma_AllocRingMemFxn EnetUdma_OpenRxFlowPrms::ringMemAllocFxn |
Callback functions. Callback function typedefs so that the EnetUdma layer can call into the app layer and let it translate between the hardware buffer descriptors and packets and the stack/translation layer's buffers and packets
Ring memory allocation callback, this cannot be NULL
EnetUdma_FreeRingMemFxn EnetUdma_OpenRxFlowPrms::ringMemFreeFxn |
Ring memory free function callback, used in close flow
EnetUdma_AllocDmaDescFxn EnetUdma_OpenRxFlowPrms::dmaDescAllocFxn |
DMA HPD (host packet descriptor) memory allocation callback
EnetUdma_FreeDmaDescFxn EnetUdma_OpenRxFlowPrms::dmaDescFreeFxn |
Transmit HPD (host packet descriptor) memory free callback
void* EnetUdma_OpenRxFlowPrms::cbArg |
Argument to be used for the callback routines (it should mean something to layer into which the callback calls)
bool EnetUdma_OpenRxFlowPrms::useProxy |
Flag to indicate if a dedicated proxy should be allocated for the "FQ" for this flow. This should be enabled only for those flows that require very high throughput as there are limited proxy available in the system
EnetUdma_AutoReclaimPrms EnetUdma_OpenRxFlowPrms::autoReclaimPrms |
Buffer auto-reclaim params