![]() |
PDK API Guide for J721E
|
Structure containing DSS sync operations configuration. This structure is used as a part of Dss_DctrlVpParams.
Data Fields | |
uint32_t | enabled |
uint32_t | isPrimary |
uint32_t | syncVpIds [CSL_DSS_VP_ID_MAX] |
uint32_t | numSyncVpIds |
uint32_t Dss_DctrlSyncOpCfg::enabled |
Enable sync operations configuration
uint32_t Dss_DctrlSyncOpCfg::isPrimary |
Whether this VP is the primary output. Only operations on the primary VP results in H/W register operations. For secondary VPs, the enable / setGo operations pend on the corresponding operation on the primary VP
uint32_t Dss_DctrlSyncOpCfg::syncVpIds[CSL_DSS_VP_ID_MAX] |
Array of VP Ids for Sync operations
uint32_t Dss_DctrlSyncOpCfg::numSyncVpIds |
Number of valid VP Ids in syncVpIds