![]() |
PDK API Guide for J721E
|
Structure containing csitx module initialization arguments.
Data Fields | |
uint32_t | rxCompEnable |
uint32_t | rxv1p3MapEnable |
uint32_t | numDataLanes |
uint32_t | lanePolarityCtrl [(CSITX_TX_DATA_LANES_MAX+CSITX_TX_CLK_LANES_MAX)] |
uint32_t | enableFrameRepeat |
Csitx_DPhyCfg | dphyCfg |
uint32_t | eventGrpNum |
Csitx_EventPrms | eventParams [CSITX_EVENT_GROUP_MAX] |
uint32_t Csitx_InstCfg::rxCompEnable |
Enable RX compatibility mode 0: Disable RX compatibility mode. 1: Enable RX compatibility mode.
uint32_t Csitx_InstCfg::rxv1p3MapEnable |
Enable TX controller to use pixel mappings for 8-bit data types which match that of the CSI-2 RX v1.3 Controller 0: Disable RX v1p3 mapping. 1: Enable RX v1p3 mapping.
uint32_t Csitx_InstCfg::numDataLanes |
Number of data to be used for receiving data
uint32_t Csitx_InstCfg::lanePolarityCtrl[(CSITX_TX_DATA_LANES_MAX+CSITX_TX_CLK_LANES_MAX)] |
Invert control for differential pair of DPHY 0: Default mapping. 1: Invert P and N pair of the differential signals. dlMap[0U]: Invert control for clock lane dlMap[1U]: Invert control for data lane 1 dlMap[2U]: Invert control for data lane 2 dlMap[3U]: Invert control for data lane 3 dlMap[4U]: Invert control for data lane 4 Note: This feature is currently not supported.
uint32_t Csitx_InstCfg::enableFrameRepeat |
Enable frame repeat control. 0: Disable Frame Repeat 1: Enable Frame Repeat Last frame is repeated (and will not be returned to the application) until new frame is queued for transmission. Enable this feature for remote device which expects frames at regular intervals like display.
Csitx_DPhyCfg Csitx_InstCfg::dphyCfg |
CSITX D-PHY configurations.
uint32_t Csitx_InstCfg::eventGrpNum |
CSITX number of event groups to register
Csitx_EventPrms Csitx_InstCfg::eventParams[CSITX_EVENT_GROUP_MAX] |
CSITX event configurations parameter.