![]() |
PDK API Guide for J721E
|
D-PHY configuration structure.
Data Fields | |
uint32_t | inst |
uint32_t | psmClkFreqDiv |
uint32_t | pllByteClkDiv |
uint32_t | pwmCtrlDivLow |
uint32_t | pwmCtrlDivHigh |
uint32_t | pllLockThreshold |
uint32_t | pllLockStart |
uint32_t | pllIpDiv |
uint32_t | pllOpDiv |
uint32_t | pllFbDiv |
uint32_t | pllPd |
uint32_t | laneBandSpeed |
uint32_t | waitBurstTime |
uint32_t | txClkExitTime |
uint32_t | dlWkupTime |
uint32_t | clWkupTime |
uint32_t | clkMode |
uint32_t | dphyMode |
uint32_t | clSlewRateCtrl |
uint32_t | dlSlewRateCtrl |
uint32_t | laneSpeedMbps |
uint32_t Csitx_DPhyCfg::inst |
CSITX istance. See CSITX_InstanceId for details
uint32_t Csitx_DPhyCfg::psmClkFreqDiv |
PMA state machine clock frequency divider control. Valid values: 1 to 255
uint32_t Csitx_DPhyCfg::pllByteClkDiv |
Selects the byte clock divider value, by driving the cmnda_pll_byteclk_div signal to the analog. Valid values: 0x01: Div 1 0x02: Div 2 0x04: Div 4 0x08: Div 8 0x10: Div 16 0x20: Div 32
uint32_t Csitx_DPhyCfg::pwmCtrlDivLow |
Low division value setting for the gm PWM control divider. Valid values: 1 to 1023
uint32_t Csitx_DPhyCfg::pwmCtrlDivHigh |
High division value setting for the gm PWM control divider. Valid values: 1 to 1023
uint32_t Csitx_DPhyCfg::pllLockThreshold |
pllcnt lock threshold value for PLL lock detect module. Valid values: 1 to 65535
uint32_t Csitx_DPhyCfg::pllLockStart |
pllcnt start value for PLL lock detect module. Valid values: 1 to 65535
uint32_t Csitx_DPhyCfg::pllIpDiv |
PLL IP Divider value. This value is calculated in the driver.
uint32_t Csitx_DPhyCfg::pllOpDiv |
PLL OP Divider value. This value is calculated in the driver
uint32_t Csitx_DPhyCfg::pllFbDiv |
PLL IP Divider value. This value is calculated in the driver
uint32_t Csitx_DPhyCfg::pllPd |
PLL PD value. 0: Disable and 1: Enable
uint32_t Csitx_DPhyCfg::laneBandSpeed |
Data rates for lane band control. This parameter is optional if valid value for 'laneSpeedMbps' is provided by the application i.e. 'laneSpeedMbps' is updated by the application after init to a valid value. See Csitx_LaneBandSpeed for details
uint32_t Csitx_DPhyCfg::waitBurstTime |
Tx clock exit time - Number of tx_byte_clk cycles corresponding to the HS clock exit time. Valid values: 1 to 255
uint32_t Csitx_DPhyCfg::txClkExitTime |
Wait Burst Time - Number of tx_byte_clk cycles corresponding to the inter HS burst gap. Valid values: 1 to 255
uint32_t Csitx_DPhyCfg::dlWkupTime |
D-PHY data lane wakeup time in ppi_tx_esc_clk cycles. Valid values: 1 to 65535
uint32_t Csitx_DPhyCfg::clWkupTime |
D-PHY clock lane wakeup time in ppi_tx_esc_clk cycles. Valid values: 1 to 65535
uint32_t Csitx_DPhyCfg::clkMode |
DPHY Clock Mode. See Csitx_ClkMode for details
uint32_t Csitx_DPhyCfg::dphyMode |
DPHY Mode. See Csitx_DphyMode for details This parameter is only valid when 'clkMode' is 'CSITX_CLK_MODE_NON_CONTINUOUS'.
uint32_t Csitx_DPhyCfg::clSlewRateCtrl |
Slew Rate: Slew rate control for clock lane. Range [0-31] Slew Rate Control Values: value 0 is for minimum slew cap i.e faster slew rate value 31 is for maximum slew cap i.e slowest slew rate Default Slew Rate Control Values: For 80M to 1Gbps : 27 For 1Gbps to 1.5Gbps : 7 For 1.5Gbps to 2.5Gbps : 1
uint32_t Csitx_DPhyCfg::dlSlewRateCtrl |
Slew Rate: Slew rate control for data lane. Range [0-31] Slew Rate Control Values: value 0 is for minimum slew cap i.e faster slew rate value 31 is for maximum slew cap i.e slowest slew rate Default Slew Rate Control Values: For 80M to 1Gbps : 27 For 1Gbps to 1.5Gbps : 7 For 1.5Gbps to 2.5Gbps : 1
uint32_t Csitx_DPhyCfg::laneSpeedMbps |
Exact DPHY lane speed from the selected speed band in Megabits per sec. This parameter is set to default value during init time. If updated in the application after init, newly set value will be used for DPHY clock configurations. If this parameter is set by the application, then application need not to set 'laneBandSpeed' parameter as it will be auto-calculated in the driver during create time.