PDK API Guide for J721E
|
UDMAP configuration structure.
This structure contains configuration information for the UDMAP.
Data Fields | |
CSL_udmap_gcfgRegs * | pGenCfgRegs |
CSL_udmap_rxfcfgRegs * | pRxFlowCfgRegs |
CSL_udmap_txccfgRegs * | pTxChanCfgRegs |
CSL_udmap_rxccfgRegs * | pRxChanCfgRegs |
CSL_udmap_txcrtRegs * | pTxChanRtRegs |
CSL_udmap_rxcrtRegs * | pRxChanRtRegs |
uint32_t | cap0 |
uint32_t | cap1 |
uint32_t | txChanCnt |
uint32_t | rxChanCnt |
uint32_t | rxFlowCnt |
uint32_t | txExtUtcChanCnt |
uint32_t | txHighCapacityChanCnt |
uint32_t | txUltraHighCapacityChanCnt |
CSL_udmap_gcfgRegs* CSL_UdmapCfg::pGenCfgRegs |
[IN] Pointer to the general configuration registers
CSL_udmap_rxfcfgRegs* CSL_UdmapCfg::pRxFlowCfgRegs |
[IN] Pointer to the rx flow configuration registers
CSL_udmap_txccfgRegs* CSL_UdmapCfg::pTxChanCfgRegs |
[IN] Pointer to the tx channel configuration registers
CSL_udmap_rxccfgRegs* CSL_UdmapCfg::pRxChanCfgRegs |
[IN] Pointer to the rx channel configuration registers
CSL_udmap_txcrtRegs* CSL_UdmapCfg::pTxChanRtRegs |
[IN] Pointer to the tx channel real-time registers
CSL_udmap_rxcrtRegs* CSL_UdmapCfg::pRxChanRtRegs |
[IN] Pointer to the rx channel real-time registers
uint32_t CSL_UdmapCfg::cap0 |
[OUT] Contains the contents of the Capabilities Register 0 (populated by the CSL_udmapGetCfg function)
uint32_t CSL_UdmapCfg::cap1 |
[OUT] Contains the contents of the Capabilities Register 1 (populated by the CSL_udmapGetCfg function)
uint32_t CSL_UdmapCfg::txChanCnt |
[OUT] Tx channel count (populated by the CSL_udmapGetCfg function)
uint32_t CSL_UdmapCfg::rxChanCnt |
[OUT] Rx channel count (populated by the CSL_udmapGetCfg function)
uint32_t CSL_UdmapCfg::rxFlowCnt |
[OUT] Rx flow count (populated by the CSL_udmapGetCfg function)
uint32_t CSL_UdmapCfg::txExtUtcChanCnt |
[OUT] Tx external UTC channel count (populated by the CSL_udmapGetCfg function)
uint32_t CSL_UdmapCfg::txHighCapacityChanCnt |
[OUT] Tx external UTC channel count (populated by the CSL_udmapGetCfg function)
uint32_t CSL_UdmapCfg::txUltraHighCapacityChanCnt |
[OUT] Tx external UTC channel count (populated by the CSL_udmapGetCfg function)