![]() |
PDK API Guide for J721E
|
Functions | |
uint32_t | CSL_udmapGetRevision (const CSL_UdmapCfg *pCfg) |
Return revision of the UDMAP module. More... | |
int32_t | CSL_udmapGetRevisionInfo (const CSL_UdmapCfg *pCfg, CSL_UdmapRevision *pRev) |
Return revision information of the UDMAP module. More... | |
void | CSL_udmapGetCfg (CSL_UdmapCfg *pCfg) |
Return UDMAP configuration information. More... | |
void | CSL_udmapInitTxChanCfg (CSL_UdmapTxChanCfg *pTxChanCfg) |
Initialize a CSL_UdmapTxChanCfg structure. More... | |
void | CSL_udmapInitRxChanCfg (CSL_UdmapRxChanCfg *pRxChanCfg) |
Initialize a CSL_UdmapRxChanCfg structure. More... | |
void | CSL_udmapInitRxFlowCfg (CSL_UdmapRxFlowCfg *pFlow) |
Initialize a CSL_UdmapRxFlowCfg structure. More... | |
void | CSL_udmapSetPerfCtrl (CSL_UdmapCfg *pCfg, uint32_t rxRetryTimeoutCnt) |
Set performance control parmeters. More... | |
void | CSL_udmapSetUtcCtrl (CSL_UdmapCfg *pCfg, uint32_t startingThreadNum) |
Set UTC control parmeters. More... | |
int32_t | CSL_udmapRxFlowCfg (CSL_UdmapCfg *pCfg, uint32_t flow, const CSL_UdmapRxFlowCfg *pFlow) |
Configure an RX flow. More... | |
int32_t | CSL_udmapRxChanCfg (CSL_UdmapCfg *pCfg, uint32_t chanIdx, const CSL_UdmapRxChanCfg *pRxChanCfg) |
Configure an RX channel. More... | |
int32_t | CSL_udmapTxChanCfg (CSL_UdmapCfg *pCfg, uint32_t chanIdx, const CSL_UdmapTxChanCfg *pTxChanCfg) |
Configure a TX channel. More... | |
int32_t | CSL_udmapRxChanSetTrEvent (CSL_UdmapCfg *pCfg, uint32_t chanIdx, uint32_t trEventNum) |
Configure an RX channel TR event. More... | |
int32_t | CSL_udmapTxChanSetTrEvent (CSL_UdmapCfg *pCfg, uint32_t chanIdx, uint32_t trEventNum) |
Configure an TX channel TR event. More... | |
int32_t | CSL_udmapRxChanSetBurstSize (CSL_UdmapCfg *pCfg, uint32_t chanIdx, CSL_UdmapChanBurstSize burstSize) |
Configure RX channel burst size. More... | |
int32_t | CSL_udmapTxChanSetBurstSize (CSL_UdmapCfg *pCfg, uint32_t chanIdx, CSL_UdmapChanBurstSize burstSize) |
Configure TX channel burst size. More... | |
int32_t | CSL_udmapGetRxRT (const CSL_UdmapCfg *pCfg, uint32_t chanIdx, CSL_UdmapRT *pRT) |
Get an RX channel's real-time register values. More... | |
int32_t | CSL_udmapGetTxRT (const CSL_UdmapCfg *pCfg, uint32_t chanIdx, CSL_UdmapRT *pRT) |
Get a TX channel's real-time register values. More... | |
int32_t | CSL_udmapSetRxRT (CSL_UdmapCfg *pCfg, uint32_t chanIdx, const CSL_UdmapRT *pRT) |
Set an RX channel's real-time register values. More... | |
int32_t | CSL_udmapSetTxRT (CSL_UdmapCfg *pCfg, uint32_t chanIdx, const CSL_UdmapRT *pRT) |
Set a TX channel's real-time register values. More... | |
int32_t | CSL_udmapEnableTxChan (CSL_UdmapCfg *pCfg, uint32_t chanIdx) |
Enable a transmit channel. More... | |
int32_t | CSL_udmapDisableTxChan (CSL_UdmapCfg *pCfg, uint32_t chanIdx) |
Disable a transmit channel. More... | |
int32_t | CSL_udmapTeardownTxChan (CSL_UdmapCfg *pCfg, uint32_t chanIdx, bool bForce, bool bWait) |
Teardown a transmit channel. More... | |
int32_t | CSL_udmapPauseTxChan (CSL_UdmapCfg *pCfg, uint32_t chanIdx) |
Pause a transmit channel. More... | |
int32_t | CSL_udmapUnpauseTxChan (CSL_UdmapCfg *pCfg, uint32_t chanIdx) |
Un-pause a transmit channel. More... | |
int32_t | CSL_udmapTriggerTxChan (CSL_UdmapCfg *pCfg, uint32_t chanIdx) |
Send a trigger event to a TX channel. More... | |
void | CSL_udmapClearTxChanError (CSL_UdmapCfg *pCfg, uint32_t chanIdx) |
Clear error indication in a transmit channel. More... | |
int32_t | CSL_udmapEnableRxChan (CSL_UdmapCfg *pCfg, uint32_t chanIdx) |
Enable a receive channel. More... | |
int32_t | CSL_udmapDisableRxChan (CSL_UdmapCfg *pCfg, uint32_t chanIdx) |
Disable a receive channel. More... | |
int32_t | CSL_udmapTeardownRxChan (CSL_UdmapCfg *pCfg, uint32_t chanIdx, bool bForce, bool bWait) |
Teardown a receive channel. More... | |
int32_t | CSL_udmapPauseRxChan (CSL_UdmapCfg *pCfg, uint32_t chanIdx) |
Pause a receive channel. More... | |
int32_t | CSL_udmapUnpauseRxChan (CSL_UdmapCfg *pCfg, uint32_t chanIdx) |
Un-pause a receive channel. More... | |
int32_t | CSL_udmapTriggerRxChan (CSL_UdmapCfg *pCfg, uint32_t chanIdx) |
Send a trigger event to an RX channel. More... | |
void | CSL_udmapClearRxChanError (CSL_UdmapCfg *pCfg, uint32_t chanIdx) |
Clear error indication in a receive channel. More... | |
void | CSL_udmapCfgRxFlowIdFirewall (CSL_UdmapCfg *pCfg, uint32_t outEvtNum) |
Configure the receive flow ID range firewall. More... | |
bool | CSL_udmapGetRxFlowIdFirewallStatus (CSL_UdmapCfg *pCfg, CSL_UdmapRxFlowIdFirewallStatus *pRxFlowIdFwStatus) |
Get receive flow ID range firewall status information. More... | |
void | CSL_udmapGetChanStats (const CSL_UdmapCfg *pCfg, uint32_t chanIdx, CSL_UdmapChanDir chanDir, CSL_UdmapChanStats *pChanStats) |
Get channel statistics. More... | |
void | CSL_udmapDecChanStats (CSL_UdmapCfg *pCfg, uint32_t chanIdx, CSL_UdmapChanDir chanDir, const CSL_UdmapChanStats *pChanStats) |
Decrement channel statistics. More... | |
int32_t | CSL_udmapGetChanPeerReg (const CSL_UdmapCfg *pCfg, uint32_t chanIdx, CSL_UdmapChanDir chanDir, uint32_t regIdx, uint32_t *pVal) |
Read a channel peer register. More... | |
int32_t | CSL_udmapSetChanPeerReg (const CSL_UdmapCfg *pCfg, uint32_t chanIdx, CSL_UdmapChanDir chanDir, uint32_t regIdx, uint32_t *pVal) |
Write a TX channel peer register. More... | |
int32_t | CSL_udmapEnableLink (CSL_UdmapCfg *pCfg, uint32_t chanIdx, CSL_UdmapChanDir chanDir) |
Enable a directional data flow for a paired link. More... | |
int32_t | CSL_udmapSetAutoClockGatingEnable (CSL_UdmapCfg *pCfg, CSL_UdmapAutoClkgateBlock blockIds, bool bEnable) |
Enable or disable automatic dynamic clock gating for one or more blocks. More... | |
int32_t | CSL_udmapSetCommandThrottleThreshold (CSL_UdmapCfg *pCfg, CSL_UdmapMasterInterface interfaceId, uint32_t readCountThresh, uint32_t writeCountThresh) |
Set the command throttle threshold for a UDMAP VBUSM master interface. More... | |
uint32_t CSL_udmapGetRevision | ( | const CSL_UdmapCfg * | pCfg | ) |
Return revision of the UDMAP module.
This function returns the contents of the UDMAP revision register. Consult the UDMAP module documentation for a description of the contents of the revision register.
pCfg | [IN] Pointer to the UDMAP configuration structure |
int32_t CSL_udmapGetRevisionInfo | ( | const CSL_UdmapCfg * | pCfg, |
CSL_UdmapRevision * | pRev | ||
) |
Return revision information of the UDMAP module.
This function returns revision information for the UDMAP module.
pCfg | [IN] Pointer to the UDMAP configuration structure |
pRev | [OUT] Pointer to a CSL_UdmapRevision structure where the revision information is returned |
void CSL_udmapGetCfg | ( | CSL_UdmapCfg * | pCfg | ) |
Return UDMAP configuration information.
This function returns configuration and capability information for the UDMAP module. See the CSL_UdmapCfg structure for details on the information that is returned.
pCfg | [IN/OUT] Pointer to the UDMAP configuration structure |
void CSL_udmapInitTxChanCfg | ( | CSL_UdmapTxChanCfg * | pTxChanCfg | ) |
Initialize a CSL_UdmapTxChanCfg structure.
This function initializes the specified CSL_UdmapTxChanCfg structure to known, safe values. Software then only needs to configure elements that are different than their initialized values prior to calling the CSL_udmapTxChanCfg function.
All elements of the CSL_UdmapTxChanCfg structure are initialized to zero except for the following:
chanType = CSL_UDMAP_CHAN_TYPE_REF_PKT_RING; fetchWordSize = CSL_UDMAP_FETCH_WORD_SIZE_16; trEventNum = CSL_UDMAP_NO_EVENT; errEventNum = CSL_UDMAP_NO_EVENT;
pTxChanCfg | [OUT] Pointer to a CSL_UdmapTxChanCfg structure |
void CSL_udmapInitRxChanCfg | ( | CSL_UdmapRxChanCfg * | pRxChanCfg | ) |
Initialize a CSL_UdmapRxChanCfg structure.
This function initializes the specified CSL_UdmapRxChanCfg structure to known, safe values. Software then only needs to configure elements that are different than their initialized values prior to calling the CSL_udmapRxChanCfg function.
All elements of the CSL_UdmapRxChanCfg structure are initialized to zero except for the following:
chanType = CSL_UDMAP_CHAN_TYPE_REF_PKT_RING; fetchWordSize = CSL_UDMAP_FETCH_WORD_SIZE_16; trEventNum = CSL_UDMAP_NO_EVENT; errEventNum = CSL_UDMAP_NO_EVENT; flowIdFwRangeCnt = CSL_UDMAP_RXCCFG_CHAN_RFLOW_RNG_FLOWID_CNT_RESETVAL;
pRxChanCfg | [OUT] Pointer to a CSL_UdmapRxChanCfg structure |
void CSL_udmapInitRxFlowCfg | ( | CSL_UdmapRxFlowCfg * | pFlow | ) |
Initialize a CSL_UdmapRxFlowCfg structure.
This function initializes the specified CSL_UdmapRxFlowCfg structure to known, safe values. Software then only needs to configure elements that are different than their initialized values prior to calling the CSL_udmapRxFlowCfg function.
All elements of the CSL_UdmapRxFlowCfg structure are initialized to zero.
pFlow | [OUT] Pointer to a CSL_UdmapRxFlowCfg structure |
void CSL_udmapSetPerfCtrl | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | rxRetryTimeoutCnt | ||
) |
Set performance control parmeters.
This function is used to set performance control paramaters available in the UDMAP module.
pCfg | [IN] Pointer to the UDMAP configuration structure |
rxRetryTimeoutCnt | [IN] This parameter specifies the minimum amount of time (in clock cycles) that an Rx channel will be required to wait when it encounters a buffer starvation condition and the Rx error handling bit is set to 1 |
void CSL_udmapSetUtcCtrl | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | startingThreadNum | ||
) |
Set UTC control parmeters.
This function is used to set UTC control paramaters available in the UDMAP module.
pCfg | [IN] Pointer to the UDMAP configuration structure |
startingThreadNum | [IN] This parameter specifies the starting PSI-L thread number for the external UTC |
int32_t CSL_udmapRxFlowCfg | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | flow, | ||
const CSL_UdmapRxFlowCfg * | pFlow | ||
) |
Configure an RX flow.
This function initializes a receive flow with values specified in the CSL_UdmapRxFlowCfg structure.
pCfg | [IN] Pointer to the UDMAP configuration structure |
flow | [IN] Index of the receive flow to initialize |
pFlow | [IN] Pointer to a CSL_UdmapRxFlowCfg structure containing initialization values |
int32_t CSL_udmapRxChanCfg | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx, | ||
const CSL_UdmapRxChanCfg * | pRxChanCfg | ||
) |
Configure an RX channel.
This function initializes a receive channel with values specified in the CSL_UdmapRxChanCfg structure.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] Index of the receive channel to initialize |
pRxChanCfg | [IN] Pointer to a CSL_UdmapRxChanCfg structure containing initialization values |
int32_t CSL_udmapTxChanCfg | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx, | ||
const CSL_UdmapTxChanCfg * | pTxChanCfg | ||
) |
Configure a TX channel.
This function initializes a transmit channel with values specified in the CSL_UdmapTxChanCfg structure.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] Index of the transmit channel to initialize |
pTxChanCfg | [IN] Pointer to a CSL_UdmapTxChanCfg structure containing initialization values |
int32_t CSL_udmapRxChanSetTrEvent | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx, | ||
uint32_t | trEventNum | ||
) |
Configure an RX channel TR event.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] Index of the receive channel to initialize |
trEventNum | [IN] Specifies a global event number to generate anytime the required event generation criteria specified in a TR are met Set to CSL_UDMAP_NO_EVENT for no event generation. |
int32_t CSL_udmapTxChanSetTrEvent | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx, | ||
uint32_t | trEventNum | ||
) |
Configure an TX channel TR event.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] Index of the transmit channel to initialize |
trEventNum | [IN] Specifies a global event number to generate anytime the required event generation criteria specified in a TR are met Set to CSL_UDMAP_NO_EVENT for no event generation. |
int32_t CSL_udmapRxChanSetBurstSize | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx, | ||
CSL_UdmapChanBurstSize | burstSize | ||
) |
Configure RX channel burst size.
This function enables configuration of the nominal burst size and alignment for data transfers on the specified RX channel. The default burst size is 64 bytes (a value of CSL_UDMAP_CHAN_BURST_SIZE_64_BYTES).
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] Index of the receive channel to initialize |
burstSize | [IN] Burst size value. See CSL_UdmapChanBurstSize for a list of valid burst size values. |
int32_t CSL_udmapTxChanSetBurstSize | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx, | ||
CSL_UdmapChanBurstSize | burstSize | ||
) |
Configure TX channel burst size.
This function enables configuration of the nominal burst size and alignment for data transfers on the specified TX channel. The default burst size is 64 bytes (a value of CSL_UDMAP_CHAN_BURST_SIZE_64_BYTES).
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] Index of the transmit channel to initialize |
burstSize | [IN] Burst size value. See CSL_UdmapChanBurstSize for a list of valid burst size values. |
int32_t CSL_udmapGetRxRT | ( | const CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx, | ||
CSL_UdmapRT * | pRT | ||
) |
Get an RX channel's real-time register values.
This function returns the real-time register values for the specified receive channel.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] Index of the receive channel |
pRT | [OUT] Pointer to a CSL_UdmapRT structure where values are returned |
int32_t CSL_udmapGetTxRT | ( | const CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx, | ||
CSL_UdmapRT * | pRT | ||
) |
Get a TX channel's real-time register values.
This function returns the real-time register values for the specified transmit channel.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] Index of the transmit channel |
pRT | [OUT] Pointer to a CSL_UdmapRT structure where values are returned |
int32_t CSL_udmapSetRxRT | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx, | ||
const CSL_UdmapRT * | pRT | ||
) |
Set an RX channel's real-time register values.
This function sets the real-time register values for the specified receive channel.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] Index of the receive channel |
pRT | [IN] Pointer to a CSL_UdmapRT structure containing initialization values |
int32_t CSL_udmapSetTxRT | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx, | ||
const CSL_UdmapRT * | pRT | ||
) |
Set a TX channel's real-time register values.
This function sets the real-time register values for the specified transmit channel.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] Index of the transmit channel |
pRT | [IN] Pointer to a CSL_UdmapRT structure containing initialization values |
int32_t CSL_udmapEnableTxChan | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx | ||
) |
Enable a transmit channel.
This function enables the transmit channel specified by 'chanIdx'.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] The index of the transmit channel |
int32_t CSL_udmapDisableTxChan | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx | ||
) |
Disable a transmit channel.
This function disables the transmit channel specified by 'chanIdx'.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] The index of the transmit channel |
int32_t CSL_udmapTeardownTxChan | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx, | ||
bool | bForce, | ||
bool | bWait | ||
) |
Teardown a transmit channel.
This function tears down the transmit channel specified by 'chanIdx' at the next packet boundary.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] The index of the transmit channel |
bForce | [IN] If true, the channel is torn down without attempting to preserve data or wait for events (flushes the channel). If false, any packets in flight are completed prior to the channel being torn down. |
bWait | [IN] If true, wait for the teardown operation to complete. Otherwise, return immediately. |
int32_t CSL_udmapPauseTxChan | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx | ||
) |
Pause a transmit channel.
This function pauses the transmit channel specified by 'chanIdx' at the next packet boundary. This is a more graceful method of halting processing than disabling the channel as it will not allow any current packets to underflow.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] The index of the transmit channel |
int32_t CSL_udmapUnpauseTxChan | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx | ||
) |
Un-pause a transmit channel.
This function un-pauses the transmit channel specified by 'chanIdx'.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] The index of the transmit channel |
int32_t CSL_udmapTriggerTxChan | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx | ||
) |
Send a trigger event to a TX channel.
This function causes a trigger event to be sent to the specified transmit channel.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] Index of the transmit channel |
void CSL_udmapClearTxChanError | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx | ||
) |
Clear error indication in a transmit channel.
This function clears the error indication in the specified transmit channel.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] The index of the transmit channel |
int32_t CSL_udmapEnableRxChan | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx | ||
) |
Enable a receive channel.
This function enables the receive channel specified by 'chanIdx'.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] The index of the receive channel |
int32_t CSL_udmapDisableRxChan | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx | ||
) |
Disable a receive channel.
This function disables the receive channel specified by 'chanIdx'.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] The index of the receive channel |
int32_t CSL_udmapTeardownRxChan | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx, | ||
bool | bForce, | ||
bool | bWait | ||
) |
Teardown a receive channel.
This function tears down the receive channel specified by 'chanIdx' at the next packet boundary.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] The index of the receive channel |
bForce | [IN] If true, the channel is torn down without attempting to preserve data or wait for events (flushes the channel). If false, any packets in flight are completed prior to the channel being torn down. |
bWait | [IN] If true, wait for the teardown operation to complete. Otherwise, return immediately. |
int32_t CSL_udmapPauseRxChan | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx | ||
) |
Pause a receive channel.
This function pauses the receive channel specified by 'chanIdx' at the next packet boundary. This is a more graceful method of halting processing than disabling the channel as it will not allow any current packets to underflow.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] The index of the receive channel |
int32_t CSL_udmapUnpauseRxChan | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx | ||
) |
Un-pause a receive channel.
This function un-pauses the receive channel specified by 'chanIdx'.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] The index of the transmit channel |
int32_t CSL_udmapTriggerRxChan | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx | ||
) |
Send a trigger event to an RX channel.
This function causes a trigger event to be sent to the specified receive channel.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] Index of the receive channel |
void CSL_udmapClearRxChanError | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx | ||
) |
Clear error indication in a receive channel.
This function clears the error indication in the specified receive channel.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] The index of the receive channel |
void CSL_udmapCfgRxFlowIdFirewall | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | outEvtNum | ||
) |
Configure the receive flow ID range firewall.
This function is used to configure the receive flow ID range firewall.
pCfg | [IN] Pointer to the UDMAP configuration structure |
outEvtNum | [IN] Output event number to use when the receive flow ID range firewall detects an error |
bool CSL_udmapGetRxFlowIdFirewallStatus | ( | CSL_UdmapCfg * | pCfg, |
CSL_UdmapRxFlowIdFirewallStatus * | pRxFlowIdFwStatus | ||
) |
Get receive flow ID range firewall status information.
This function returns information from the receive flow ID range firewall.
If the receive flow ID firewall has detected an out of range flow ID, the function returns true and the fields within the CSL_UdmapRxFlowIdFirewallStatus structure contain error details. The function will automatically reset the receive flow ID firewall to capture the next error.
If the receive flow ID firewall has not detected an out of range flow ID, the function returns false and the fields within the CSL_UdmapRxFlowIdFirewallStatus structure are not updated.
pCfg | [IN] Pointer to the UDMAP configuration structure |
pRxFlowIdFwStatus | [IN] Pointer to a CSL_UdmapRxFlowIdFirewallStatus structure containing error details (valid only when true is returned) |
void CSL_udmapGetChanStats | ( | const CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx, | ||
CSL_UdmapChanDir | chanDir, | ||
CSL_UdmapChanStats * | pChanStats | ||
) |
Get channel statistics.
This function is used to read statistics for a transmit or receive channel.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] Index of the channel |
chanDir | [IN] Channel direction (see CSL_UdmapChanDir) |
pChanStats | [OUT] Pointer to a CSL_UdmapChanStats structure where the statistics are returned |
void CSL_udmapDecChanStats | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx, | ||
CSL_UdmapChanDir | chanDir, | ||
const CSL_UdmapChanStats * | pChanStats | ||
) |
Decrement channel statistics.
This function is used to decrement statistics for a transmit or receive channel by the counts contained in the specified CSL_UdmapChanStats structure.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] Index of the channel |
chanDir | [IN] Channel direction (see CSL_UdmapChanDir) |
pChanStats | [IN] Pointer to a CSL_UdmapChanStats structure containing the counts to decrement each statistic by |
int32_t CSL_udmapGetChanPeerReg | ( | const CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx, | ||
CSL_UdmapChanDir | chanDir, | ||
uint32_t | regIdx, | ||
uint32_t * | pVal | ||
) |
Read a channel peer register.
This function is used to read the value from a peer register for the specified channel.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] Index of the channel |
chanDir | [IN] Channel direction (see CSL_UdmapChanDir) |
regIdx | [IN] Peer register index (0..15) |
pVal | [OUT] Pointer where the register value is returned |
int32_t CSL_udmapSetChanPeerReg | ( | const CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx, | ||
CSL_UdmapChanDir | chanDir, | ||
uint32_t | regIdx, | ||
uint32_t * | pVal | ||
) |
Write a TX channel peer register.
This function is used to write a value to a peer register for the specified transmit channel.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] Index of the transmit channel |
chanDir | [IN] Channel direction (see CSL_UdmapChanDir) |
regIdx | [IN] Peer register index (0..15) |
pVal | [IN] Pointer to the register value to be written |
int32_t CSL_udmapEnableLink | ( | CSL_UdmapCfg * | pCfg, |
uint32_t | chanIdx, | ||
CSL_UdmapChanDir | chanDir | ||
) |
Enable a directional data flow for a paired link.
This function is used to enable a directional data flow for a given UDMAP channel between UDMAP and a paired PSIL peer.
pCfg | [IN] Pointer to the UDMAP configuration structure |
chanIdx | [IN] Index of the UDMAP channel (TX or RX) |
chanDir | [IN] Channel direction (TX or RX, see CSL_UdmapChanDir) |
int32_t CSL_udmapSetAutoClockGatingEnable | ( | CSL_UdmapCfg * | pCfg, |
CSL_UdmapAutoClkgateBlock | blockIds, | ||
bool | bEnable | ||
) |
Enable or disable automatic dynamic clock gating for one or more blocks.
This function is used to enable or disable automatic dynamic clock gating for one or more internal sub-blocks within the UDMAP.
UDMAP revision 2.2.0.0 and later provides automatic dynamic clock gating support for internal sub-blocks based on real-time monitoring of activity.
pCfg | [IN] Pointer to the UDMAP configuration structure |
blockIds | [IN] One or more block ID's created by logically or'ing one or more ID's defined in CSL_UdmapAutoClkgateBlock |
bEnable | [IN] If true, automatic dynamic clock gating for the specified blocks is enabled. Otherwise, it is disabled. |
int32_t CSL_udmapSetCommandThrottleThreshold | ( | CSL_UdmapCfg * | pCfg, |
CSL_UdmapMasterInterface | interfaceId, | ||
uint32_t | readCountThresh, | ||
uint32_t | writeCountThresh | ||
) |
Set the command throttle threshold for a UDMAP VBUSM master interface.
This function is used to set the read and/or write command throttle threshold for a UDMAP VBUSM master interface. Command dispatching will be disabled for virtualized channels whenver the current virtualized read or write count from this interface meets or exceeds the programmed value.
Note that this feature is only available in UDMAP revision 2.1.32.0 and later.
The following table shows if read and/or write thresholds can be set for each available interface:
Read Write ---- -----
CSL_UDMAP_MASTER_INTERFACE_PKTDMA_0 X X CSL_UDMAP_MASTER_INTERFACE_PKTDMA_1 X X CSL_UDMAP_MASTER_INTERFACE_UTC_READ X CSL_UDMAP_MASTER_INTERFACE_UTC_WRITE X
pCfg | [IN] Pointer to the UDMAP configuration structure |
interfaceId | [IN] Interface ID. See CSL_UdmapMasterInterface |
readCountThresh | [IN] Read command threshold value. Must be > 0. |
writeCountThresh | [IN] Write command threshold value. Must be > 0. |