![]() |
PDK API Guide for J721E
|
PMIC Driver initialization API/interface file.
Go to the source code of this file.
Data Structures | |
struct | Pmic_CoreCfg_t |
PMIC configuration structure. Contains various parameters which are needed to prepare PMIC driver handle using Valid params. like, PMIC device type, PMIC interface mode, Slave address, various application defined API function pointers for LLD and Critical sections. Application has to set the corresponding bit in validParams structure member to update the driver with Pmic_CoreCfg_t structure fields. For Example, If the Application needs to configure the PMIC driver pmicDeviceType member of the structure then application has to set PMIC_CFG_DEVICE_TYPE_VALID bit of validParams struct and then call pmic_init(). More... | |
Macros | |
PMIC Error Codes | |
#define | PMIC_ST_SUCCESS (0) |
Error Code for SUCCESS. More... | |
#define | PMIC_ST_ERR_INV_HANDLE (-((int32_t)1)) |
Error Code for Invalid input Handle. More... | |
#define | PMIC_ST_ERR_NULL_PARAM (-((int32_t)2)) |
Error Code when input Param is NULL. More... | |
#define | PMIC_ST_ERR_INV_PARAM (-((int32_t)3)) |
Error Code for Invalid input Param. More... | |
#define | PMIC_ST_ERR_INV_DEVICE (-((int32_t)4)) |
Error Code for Invalid PMIC Device. More... | |
#define | PMIC_ST_ERR_NULL_FPTR (-((int32_t)5)) |
Error Code when input Function pointer is NULL. More... | |
#define | PMIC_ST_ERR_INV_SUBSYSTEM (-((int32_t)6)) |
Error Code for Invalid PMIC Subsystem. More... | |
#define | PMIC_ST_ERR_INSUFFICIENT_CFG (-((int32_t)7)) |
Error Code for Insufficient input configuration params for PMIC Device Initialization. More... | |
#define | PMIC_ST_ERR_I2C_COMM_FAIL (-((int32_t)8)) |
Error Code for I2C Communication Fail. More... | |
#define | PMIC_ST_ERR_SPI_COMM_FAIL (-((int32_t)9)) |
Error Code for SPI Communication Fail. More... | |
#define | PMIC_ST_ERR_DATA_IO_CRC (-((int32_t)10)) |
Error Code for IO data failure when CRC is enabled. More... | |
#define | PMIC_ST_ERR_INTF_SETUP_FAILED (-((int32_t)11)) |
Error Code for Interface Selected is not working properly. More... | |
#define | PMIC_ST_ERR_COMM_INTF_INIT_FAIL (-((int32_t)12)) |
Error Code for Interface Init Fail. More... | |
#define | PMIC_ST_ERR_UNINIT (-((int32_t)13)) |
Error Code if Pmic_init() function called before PMIC driver is initialized. More... | |
#define | PMIC_ST_ERR_INV_VOLTAGE (-((int32_t)14)) |
Error Code for Invalid Voltage Value. More... | |
#define | PMIC_ST_ERR_INV_REGULATOR (-((int32_t)15)) |
Error Code for Invalid Power resource Value. More... | |
#define | PMIC_ST_ERR_INV_PGOOD_LEVEL (-((int32_t)16)) |
Error Code for Invalid Power Good Threshold Value. More... | |
#define | PMIC_ST_ERR_INV_TEMP_THRESHOLD (-((int32_t)17)) |
Error Code for Invalid Temperature Threshold value. More... | |
#define | PMIC_ST_ERR_INV_GPIO (-((int32_t)18)) |
Error Code for Invalid input GPIO PIN. More... | |
#define | PMIC_ST_ERR_INV_GPIO_FUNC (-((int32_t)19)) |
Error Code for Invalid GPIO Functionality. More... | |
#define | PMIC_ST_ERR_INV_GPIO_LINE_PARAMS (-((int32_t)20)) |
Error Code for input GPIO handle is invalid. More... | |
#define | PMIC_ST_ERR_PIN_NOT_GPIO (-((int32_t)21)) |
Error Code for Invalid Pin for GPIO Configuration. More... | |
#define | PMIC_ST_ERR_INV_WDG_WINDOW (-((int32_t)22)) |
Error Code for Invalid Watchdog longwindow or Window-1 or Window-2 duration. More... | |
#define | PMIC_ST_ERR_INV_WDG_ANSWER (-((int32_t)23)) |
Error Code for Invalid Watchdog Answer. More... | |
#define | PMIC_ST_ERR_WDG_EARLY_ANSWER (-((int32_t)24)) |
Error Code for Watchdog early Answer. More... | |
#define | PMIC_ST_ERR_INV_ESM_TARGET (-((int32_t)25)) |
Error Code for input ESM TargetID is invalid. More... | |
#define | PMIC_ST_ERR_INV_ESM_MODE (-((int32_t)26)) |
Error Code for ESM Operation Mode is invalid. More... | |
#define | PMIC_ST_ERR_INV_INT (-((int32_t)27)) |
Error Code for Invalid Interrupt. More... | |
#define | PMIC_ST_ERR_CLEAR_INT_FAILED (-((int32_t)28)) |
Error Code when Interrupts Clear is failed. More... | |
#define | PMIC_ST_ERR_INV_TIME (-((int32_t)29)) |
Error Code for Invalid Time. More... | |
#define | PMIC_ST_ERR_INV_DATE (-((int32_t)30)) |
Error Code for Invalid Date. More... | |
#define | PMIC_ST_ERR_RTC_STOP_FAIL (-((int32_t)31)) |
Error Code for RTC Stop command failure. More... | |
#define | PMIC_ST_ERR_FAIL (-((int32_t)32)) |
Error Code for any other failures. More... | |
#define | PMIC_ST_ERR_ESM_STARTED (-((int32_t)33)) |
Error Code for ESM in Start State. More... | |
#define | PMIC_ST_ERR_INV_ESM_VAL (-((int32_t)34)) |
Error Code for Invalid ESM delay1, delay2, HMAX, HMIN, LMAX and LMIN values. More... | |
#define | PMIC_ST_WARN_INV_DEVICE_ID (-((int32_t)35)) |
warning Code for Device ID mismatch warning More... | |
#define | PMIC_ST_ERR_INV_EN_DRV_PIN_CFG (-((int32_t)36)) |
Error Code for EN_DRV Pin configuration when FORCE_EN_DRV_LOW is set to '1'. More... | |
#define | PMIC_ST_ERR_INV_COMM_MODE (-((int32_t)37)) |
Error Code for I2C Speed configuration when commMode is set to PMIC_INTF_SPI. More... | |
#define | PMIC_ST_ERR_CRC_STATUS_FAIL (-((int32_t)38)) |
Error Code for CRC Status Failure. More... | |
#define | PMIC_ST_ERR_REG_LOCKED_WR_FAIL (-((int32_t)39)) |
Error Code for Register Write Failure when register is locked. More... | |
#define | PMIC_ST_ERR_NOT_SUPPORTED (-((int32_t)40)) |
Error Code for when a feature is not supported on PMIC device type or PMIC silicon revision. More... | |
PMIC Device type | |
#define | PMIC_DEV_LEO_TPS6594X (0U) |
#define | PMIC_DEV_HERA_LP8764X (1U) |
PMIC Communication Mode | |
#define | PMIC_INTF_SINGLE_I2C (0U) |
#define | PMIC_INTF_DUAL_I2C (1U) |
#define | PMIC_INTF_SPI (2U) |
PMIC Select I2C Speed | |
#define | PMIC_I2C_STANDARD_MODE (0U) |
Standard or Fast or Fast+ Mode. More... | |
#define | PMIC_I2C_FORCED_HS_MODE (1U) |
High-Speed Mode. More... | |
PMIC Instance Type | |
#define | PMIC_MAIN_INST (1U << 0U) |
#define | PMIC_QA_INST (1U << 1U) |
#define | PMIC_NVM_INST (1U << 2U) |
Valid only to read CRC status from Page-1 using NVM Slave Address Valid only while calling the pFnPmicCommIoRead API. More... | |
PMIC Config Structure Param Bits | |
#define | PMIC_CFG_DEVICE_TYPE_VALID (0U) |
validParams value used to set PMIC device type of PMIC Driver Handle More... | |
#define | PMIC_CFG_COMM_MODE_VALID (1U) |
validParams value used to set Interface mode of PMIC Driver Handle More... | |
#define | PMIC_CFG_SLAVEADDR_VALID (2U) |
validParams value used to set Main Interface Slave Address of PMIC Driver Handle More... | |
#define | PMIC_CFG_QASLAVEADDR_VALID (3U) |
validParams value used to set WDOG QA Interface Slave Address of PMIC Driver Handle More... | |
#define | PMIC_CFG_NVMSLAVEADDR_VALID (4U) |
validParams value used to set NVM Slave Address of PMIC Driver Handle More... | |
#define | PMIC_CFG_COMM_HANDLE_VALID (5U) |
validParams value used to set Pointer to Handle for I2C1/SPI Main Interface of PMIC Driver Handle More... | |
#define | PMIC_CFG_QACOMM_HANDLE_VALID (6U) |
validParams value used to set Pointer to Handle for I2C2-QA Interface of PMIC Driver Handle More... | |
#define | PMIC_CFG_COMM_IO_RD_VALID (7U) |
validParams value used to set Pointer to I2C/SPI Comm LLD Read Function of PMIC Driver Handle More... | |
#define | PMIC_CFG_COMM_IO_WR_VALID (8U) |
validParams value used to set Pointer to I2C/SPI Comm LLD Write Function of PMIC Driver Handle More... | |
#define | PMIC_CFG_CRITSEC_START_VALID (9U) |
validParams value used to set Pointer to Pmic Critical-Section Start Function of PMIC Driver Handle More... | |
#define | PMIC_CFG_CRITSEC_STOP_VALID (10U) |
validParams value used to set Pointer to Pmic Critical-Section Stop Function of PMIC Driver Handle More... | |
#define | PMIC_CFG_I2C1_SPEED_VALID (11U) |
validParams value used to set I2C1 Speed of PMIC Driver Handle More... | |
#define | PMIC_CFG_I2C2_SPEED_VALID (12U) |
validParams value used to set I2C2 Speed of PMIC Driver Handle More... | |
PMIC Config Structure Param Bit shift values | |
Application can use below shifted values to set the validParam struct member defined in Pmic_CoreCfg_t structure | |
#define | PMIC_CFG_DEVICE_TYPE_VALID_SHIFT (1U << PMIC_CFG_DEVICE_TYPE_VALID) |
#define | PMIC_CFG_COMM_MODE_VALID_SHIFT (1U << PMIC_CFG_COMM_MODE_VALID) |
#define | PMIC_CFG_SLAVEADDR_VALID_SHIFT (1U << PMIC_CFG_SLAVEADDR_VALID) |
#define | PMIC_CFG_QASLAVEADDR_VALID_SHIFT (1U << PMIC_CFG_QASLAVEADDR_VALID) |
#define | PMIC_CFG_NVMSLAVEADDR_VALID_SHIFT (1U << PMIC_CFG_NVMSLAVEADDR_VALID) |
#define | PMIC_CFG_COMM_HANDLE_VALID_SHIFT (1U << PMIC_CFG_COMM_HANDLE_VALID) |
#define | PMIC_CFG_QACOMM_HANDLE_VALID_SHIFT (1U << PMIC_CFG_QACOMM_HANDLE_VALID) |
#define | PMIC_CFG_COMM_IO_RD_VALID_SHIFT (1U << PMIC_CFG_COMM_IO_RD_VALID) |
#define | PMIC_CFG_COMM_IO_WR_VALID_SHIFT (1U << PMIC_CFG_COMM_IO_WR_VALID) |
#define | PMIC_CFG_CRITSEC_START_VALID_SHIFT (1U << PMIC_CFG_CRITSEC_START_VALID) |
#define | PMIC_CFG_CRITSEC_STOP_VALID_SHIFT (1U << PMIC_CFG_CRITSEC_STOP_VALID) |
#define | PMIC_CFG_I2C1_SPEED_VALID_SHIFT (1U << PMIC_CFG_I2C1_SPEED_VALID) |
#define | PMIC_CFG_I2C2_SPEED_VALID_SHIFT (1U << PMIC_CFG_I2C2_SPEED_VALID) |
Functions | |
int32_t | Pmic_init (const Pmic_CoreCfg_t *pPmicConfigData, Pmic_CoreHandle_t *pPmicCoreHandle) |
API to Initialize pmic core handle for PMIC LLD. More... | |
int32_t | Pmic_deinit (Pmic_CoreHandle_t *pPmicCoreHandle) |
API to DeInitilizes an existing PMIC Instance. More... | |