83 #define CPSW_ALE_PUBLIC_IOCTL(x) (ENET_IOCTL_TYPE_PUBLIC | \ 84 ENET_IOCTL_FDB_BASE | \ 85 ENET_IOCTL_PER_CPSW | \ 89 #define CPSW_ALE_NUM_PORTS (9U) 92 #define CPSW_ALE_NUM_MAC_PORTS (CPSW_ALE_NUM_PORTS - 1U) 95 #define CPSW_ALE_MAX_WHITELIST_IP_NXT_HDR (4U) 98 #define CPSW_ALE_ALL_PORTS_MASK ((uint32_t)((1U << CPSW_ALE_NUM_PORTS) - 1U)) 101 #define CPSW_ALE_ALL_MACPORTS_MASK ((uint32_t)(((1U << CPSW_ALE_NUM_PORTS) - 1U) - 1U)) 104 #define CPSW_ALE_HOST_PORT_MASK (ENET_BIT(0)) 107 #define CPSW_ALE_HOST_PORT_NUM (0U) 110 #define CPSW_ALE_MACPORT_BASE (1U) 113 #define CPSW_ALE_MACPORT_TO_ALEPORT(macPortNum) (ENET_MACPORT_NORM(macPortNum) + CPSW_ALE_MACPORT_BASE) 116 #define CPSW_ALE_ALEPORT_TO_MACPORT(alePortNum) (ENET_MACPORT_DENORM(alePortNum - CPSW_ALE_MACPORT_BASE)) 119 #define CPSW_ALE_MACPORT_TO_PORTMASK(macPort) (ENET_BIT(CPSW_ALE_MACPORT_TO_ALEPORT(macPort))) 122 #define CPSW_ALE_MCAST_IGN_BITS_MAX (10U) 125 #define CPSW_ALE_PEAKBITRATE_DISABLE (0U) 128 #define CPSW_ALE_COMMITBITRATE_DISABLE (0U) 131 #define CPSW_ALE_THREADID_INVALID (~0U) 143 #define CPSW_ALE_CFG_MODULE_EN (ENET_BIT(0U)) 146 #define CPSW_ALE_CFG_BYPASS_EN (ENET_BIT(1U)) 149 #define CPSW_ALE_CFG_UNKNOWN_UCAST_FLOOD2HOST (ENET_BIT(2U)) 164 #define CPSW_ALE_POLICER_MATCH_PORT (ENET_BIT(0U)) 167 #define CPSW_ALE_POLICER_MATCH_PRIORITY (ENET_BIT(1U)) 170 #define CPSW_ALE_POLICER_MATCH_OUI (ENET_BIT(2U)) 173 #define CPSW_ALE_POLICER_MATCH_MACDST (ENET_BIT(3U)) 176 #define CPSW_ALE_POLICER_MATCH_MACSRC (ENET_BIT(4U)) 179 #define CPSW_ALE_POLICER_MATCH_OVLAN (ENET_BIT(5U)) 182 #define CPSW_ALE_POLICER_MATCH_IVLAN (ENET_BIT(6U)) 185 #define CPSW_ALE_POLICER_MATCH_ETHERTYPE (ENET_BIT(7U)) 188 #define CPSW_ALE_POLICER_MATCH_IPSRC (ENET_BIT(8U)) 191 #define CPSW_ALE_POLICER_MATCH_IPDST (ENET_BIT(9U)) 207 #define CPSW_ALE_POLICER_TABLEENTRY_DELETE_OUI (CPSW_ALE_POLICER_MATCH_PRIORITY) 210 #define CPSW_ALE_POLICER_TABLEENTRY_DELETE_MACSRC (CPSW_ALE_POLICER_MATCH_MACSRC) 213 #define CPSW_ALE_POLICER_TABLEENTRY_DELETE_MACDST (CPSW_ALE_POLICER_MATCH_MACDST) 216 #define CPSW_ALE_POLICER_TABLEENTRY_DELETE_IVLAN (CPSW_ALE_POLICER_MATCH_IVLAN) 219 #define CPSW_ALE_POLICER_TABLEENTRY_DELETE_OVLAN (CPSW_ALE_POLICER_MATCH_OVLAN) 222 #define CPSW_ALE_POLICER_TABLEENTRY_DELETE_ETHERTYPE (CPSW_ALE_POLICER_MATCH_ETHERTYPE) 225 #define CPSW_ALE_POLICER_TABLEENTRY_DELETE_IPSRC (CPSW_ALE_POLICER_MATCH_IPSRC) 228 #define CPSW_ALE_POLICER_TABLEENTRY_DELETE_IPDST (CPSW_ALE_POLICER_MATCH_IPDST) 231 #define CPSW_ALE_POLICER_TABLEENTRY_DELETE_ALL (CPSW_ALE_POLICER_TABLEENTRY_DELETE_OUI | \ 232 CPSW_ALE_POLICER_TABLEENTRY_DELETE_MACSRC | \ 233 CPSW_ALE_POLICER_TABLEENTRY_DELETE_MACDST | \ 234 CPSW_ALE_POLICER_TABLEENTRY_DELETE_IVLAN | \ 235 CPSW_ALE_POLICER_TABLEENTRY_DELETE_OVLAN | \ 236 CPSW_ALE_POLICER_TABLEENTRY_DELETE_ETHERTYPE | \ 237 CPSW_ALE_POLICER_TABLEENTRY_DELETE_IPSRC | \ 238 CPSW_ALE_POLICER_TABLEENTRY_DELETE_IPDST) 249 typedef enum CpswAle_Ioctl_e
796 typedef enum CpswAle_PortState_e
823 typedef enum CpswAle_FwdStateLevel_e
838 typedef enum CpswAle_RxFilter_e
862 typedef struct CpswAle_MacAddrInfo_s
874 typedef struct CpswAle_UcastEntryInfo_s
903 typedef struct CpswAle_SetUcastEntryInArgs_s
915 typedef struct CpswAle_GetUcastEntryOutArgs_s
931 typedef struct CpswAle_McastEntryInfo_s
951 typedef struct CpswAle_SetMcastEntryInArgs_s
963 typedef struct CpswAle_GetMcastEntryInArgs_s
975 typedef struct CpswAle_GetMcastEntryOutArgs_s
987 typedef struct CpswAle_VlanIdInfo_s
999 typedef struct CpswAle_VlanEntryInfo_s
1041 typedef struct CpswAle_GetVlanEntryOutArgs_s
1074 typedef struct CpswAle_OuiEntryInfo_s
1083 typedef struct CpswAle_IPv4EntryInfo_s
1095 typedef struct CpswAle_IPv6EntryInfo_s
1107 typedef struct CpswAle_SetPortStateInArgs_s
1119 typedef struct CpswAle_GetPortMacAddrInArgs_s
1134 typedef struct CpswAle_GetPortMacAddrOutArgs_s
1152 typedef struct CpswAle_DefaultThreadCfg_s
1174 typedef enum CpswAle_TableEntryType_s
1199 typedef struct CpswAle_MacAddrClassifierInfo_s
1211 typedef struct CpswAle_MirrorMatchParams_s
1244 typedef struct CpswAle_PortMirroringCfg_s
1279 typedef struct CpswAle_TrunkCfg_s
1328 typedef struct CpswAle_PortBcastMcastRateLimitParams_s
1352 typedef struct CpswAle_SetBcastMcastRateLimitInArgs_s
1368 typedef struct CpswAle_GetBcastMcastRateLimitOutArgs_s
1387 typedef enum CpswAle_IpAddrClassifierType_e
1399 typedef struct CpswAle_IpAddrClassifierInfo_s
1414 typedef struct CpswAle_PolicerMatchParams_s
1477 typedef struct CpswAle_SetPolicerEntryInArgs_s
1498 typedef struct CpswAle_SetPolicerEntryOutArgs_s
1550 typedef struct CpswAle_PolicerEntryOutArgs_s
1653 typedef struct CpswAle_DelPolicerEntryInArgs_s
1667 typedef struct CpswAle_GetPolicerStatsInArgs_s
1679 typedef struct CpswAle_GetPolicerStatsOutArgs_s
1702 typedef struct CpswAle_SetPolicerThreadCfgInArgs_s
1720 typedef enum CpswAle_PolicerYellowThresh_e
1753 typedef enum CpswAle_PolicerNoMatchMode_e
1771 typedef struct CpswAle_UnregulatedTrafficPolicer_s
1783 typedef struct CpswAle_PolicerGlobalCfg_s
1814 typedef struct CpswAle_SetInterVlanCfgInArgs_s
1840 typedef struct CpswAle_AgingCfg_s
1852 typedef struct CpswAle_InitVlanCfg_s
1882 typedef struct CpswAle_MalformedPktSecurityCfg_s
1896 typedef struct CpswAle_IPPktSecurityCfg_s
1916 typedef struct CpswAle_MacAuthCfg_s
1931 typedef struct CpswAle_NetworkSecurityCfg_s
1959 typedef struct CpswAle_PortLearningSecurityCfg_s
1972 typedef struct CpswAle_PortVlanSecurityCfg_s
1993 typedef struct CpswAle_PortMacModeCfg_s
2023 typedef struct CpswAle_PortCfg_s
2044 typedef struct CpswAle_Cfg_s
bool dropDoubleVlan
Definition: cpsw_ale.h:1987
Delete entry info for given OUI address.
Definition: cpsw_ale.h:403
Definition: cpsw_ale.h:844
Output args for CPSW_ALE_IOCTL_GET_POLICER_STATS command.
Definition: cpsw_ale.h:1679
CpswAle_PortState portState
Definition: cpsw_ale.h:1113
uint32_t ivlanAleEntryIdx
Definition: cpsw_ale.h:1518
CpswAle_MacAddrClassifierInfo dstMacAddrInfo
Definition: cpsw_ale.h:1218
uint32_t agingPeriodInMs
Definition: cpsw_ale.h:1846
uint32_t portNum
Definition: cpsw_ale.h:1423
Set host port RX filter.
Definition: cpsw_ale.h:482
CpswAle_MacAuthCfg macAuthCfg
Definition: cpsw_ale.h:1953
bool limitIPNxtHdr
Definition: cpsw_ale.h:1062
Definition: cpsw_ale.h:802
CpswAle_NetworkSecurityCfg nwSecCfg
Definition: cpsw_ale.h:2059
Enable promiscuous mode on a MAC port.
Definition: cpsw_ale.h:776
CpswAle_VlanIdInfo vlanIdInfo
Definition: cpsw_ale.h:1222
uint32_t portNum
Definition: cpsw_ale.h:1205
uint32_t noLearnMask
Definition: cpsw_ale.h:1056
Input args for CPSW_ALE_IOCTL_SET_DEFAULT_THREADCFG command and out args for CPSW_ALE_IOCTL_GET_DEFAU...
Definition: cpsw_ale.h:1152
Unicast entry type info apart from MAC address that can be set.
Definition: cpsw_ale.h:874
Output args for CPSW_ALE_IOCTL_SET_DEFAULT_THREADCFG command.
Definition: cpsw_ale.h:1814
Input args for CPSW_ALE_IOCTL_SET_BCAST_MCAST_LIMIT command.
Definition: cpsw_ale.h:1352
Add unicast address entry.
Definition: cpsw_ale.h:273
uint32_t portMask
Definition: cpsw_ale.h:941
bool autoAgingEn
Definition: cpsw_ale.h:1843
uint32_t ovlanAleEntryIdx
Definition: cpsw_ale.h:1523
Definition: cpsw_ale.h:1726
Disable promiscuous mode on a MAC port.
Definition: cpsw_ale.h:790
bool macOnlyCafEn
Definition: cpsw_ale.h:2001
Definition: cpsw_ale.h:841
Delete entry info for given VLAN id.
Definition: cpsw_ale.h:392
CpswAle_IPv6EntryInfo ipv6Info
Definition: cpsw_ale.h:1230
uint32_t forceUntaggedEgressMask
Definition: cpsw_ale.h:1053
uint32_t forceUntaggedEgressMask
Definition: cpsw_ale.h:1017
CpswAle_PolicerYellowThresh
Yellow threshold value.
Definition: cpsw_ale.h:1720
bool rateLimitAtTxPort
Definition: cpsw_ale.h:1355
CpswAle_FwdStateLevel fwdState
Definition: cpsw_ale.h:938
Delete policer/classifier entry.
Definition: cpsw_ale.h:658
ALE configuration.
Definition: cpsw_ale.h:2044
bool yellowDropEn
Definition: cpsw_ale.h:1791
uint32_t ouiAleEntryIdx
Definition: cpsw_ale.h:1503
Definition: cpsw_ale.h:829
CpswAle_PortLearningSecurityCfg learningCfg
Definition: cpsw_ale.h:2026
ALE aging time configuration.
Definition: cpsw_ale.h:1840
uint32_t peakRateInBitsPerSec
Definition: cpsw_ale.h:1489
Output args for CPSW_ALE_IOCTL_LOOKUP_MCAST command.
Definition: cpsw_ale.h:1041
uint32_t unknownRegMcastFloodMask
Definition: cpsw_ale.h:1870
Output args for CPSW_ALE_IOCTL_GET_BCAST_MCAST_LIMIT IOCTL command.
Definition: cpsw_ale.h:1368
uint32_t numLSBIgnoreBits
Definition: cpsw_ale.h:1101
Definition: cpsw_ale.h:1738
CpswAle_MacAddrInfo * addrs
Definition: cpsw_ale.h:1125
bool trunk
Definition: cpsw_ale.h:897
uint32_t ipNxtHdrWhitelistCnt
Definition: cpsw_ale.h:1907
CpswAle_IPv4EntryInfo ipv4Info
Definition: cpsw_ale.h:1405
uint32_t addrCnt
Definition: cpsw_ale.h:1128
Input args for CPSW_ALE_IOCTL_ADD_MCAST command.
Definition: cpsw_ale.h:951
uint32_t aleEntryIdx
Definition: cpsw_ale.h:925
Disable broadcast/multicast rate limit.
Definition: cpsw_ale.h:625
CpswAle_MacAddrInfo addr
Definition: cpsw_ale.h:954
Definition: cpsw_ale.h:1765
CpswAle_IpAddrClassifierInfo srcIpInfo
Definition: cpsw_ale.h:1466
bool authModeEn
Definition: cpsw_ale.h:1919
CpswAle_OuiEntryInfo ouiInfo
Definition: cpsw_ale.h:1234
uint32_t dstMacAleEntryIdx
Definition: cpsw_ale.h:1513
Definition: cpsw_ale.h:1741
Definition: cpsw_ale.h:856
bool dropUntagged
Definition: cpsw_ale.h:1978
bool rateLimitAtTxPort
Definition: cpsw_ale.h:1374
CpswAle_MacAddrInfo addr
Definition: cpsw_ale.h:966
uint32_t trunkId
Definition: cpsw_ale.h:1282
CpswAle_IpAddrClassifierType ipAddrType
Definition: cpsw_ale.h:1402
uint32_t noLearnMask
Definition: cpsw_ale.h:1023
Add IPv6 address.
Definition: cpsw_ale.h:327
Definition: cpsw_ale.h:1756
uint32_t vlanId
Definition: cpsw_ale.h:990
bool autoLearnWithVlan
Definition: cpsw_ale.h:1861
uint32_t toPortNum
Definition: cpsw_ale.h:1265
bool ttlCheckEn
Definition: cpsw_ale.h:1820
bool srcIPEn
Definition: cpsw_ale.h:1301
uint32_t egressOpcode
Definition: cpsw_ale.h:1635
uint32_t srcMacAleEntryIdx
Definition: cpsw_ale.h:1508
uint32_t unregMcastFloodMask
Definition: cpsw_ale.h:1009
Add IPv4 address.
Definition: cpsw_ale.h:316
uint32_t ivlanAleEntryIdx
Definition: cpsw_ale.h:1589
CpswAle_PortMacModeCfg macModeCfg
Definition: cpsw_ale.h:2032
Get policer/classifier entry info.
Definition: cpsw_ale.h:647
uint32_t dstPortMask
Definition: cpsw_ale.h:1823
CpswAle_IPv4EntryInfo ipv4Info
Definition: cpsw_ale.h:1226
Unregulated traffic (no classifier hit) policing params.
Definition: cpsw_ale.h:1771
CpswAle_MacAddrInfo addr
Definition: cpsw_ale.h:1202
uint32_t vlanMemberList
Definition: cpsw_ale.h:1005
uint32_t portNum
Definition: cpsw_ale.h:878
uint32_t threadId
Definition: cpsw_ale.h:1711
uint32_t priority
Definition: cpsw_ale.h:1431
Definition: cpsw_ale.h:850
Delete all learned entries for a given port.
Definition: cpsw_ale.h:449
uint16_t etherType
Definition: cpsw_ale.h:1461
uint32_t peakRateInBitsPerSec
Definition: cpsw_ale.h:1774
CpswAle_PolicerNoMatchMode policerNoMatchMode
Definition: cpsw_ale.h:1800
Definition: cpsw_ale.h:832
bool dstEnEn
Definition: cpsw_ale.h:1322
VLAN id info.
Definition: cpsw_ale.h:987
#define ENET_MAC_ADDR_LEN
MAC address length in bytes/octets.
Definition: enet_types.h:153
bool disallowIPFrag
Definition: cpsw_ale.h:1035
CpswAle_PolicerMatchParams policerInfo
Definition: cpsw_ale.h:1670
Definition: cpsw_ale.h:1723
bool rateLimitEn
Definition: cpsw_ale.h:1371
CpswAle_PolicerMatchParams policerMatch
Definition: cpsw_ale.h:1705
Definition: cpsw_ale.h:809
uint32_t portNum
Definition: cpsw_ale.h:1122
bool mcastRateLimitForPortEn
Definition: cpsw_ale.h:1340
Enet_VlanTagType tagType
Definition: cpsw_ale.h:993
Definition: cpsw_ale.h:799
bool secure
Definition: cpsw_ale.h:887
CpswAle_IPPktSecurityCfg ipPktCfg
Definition: cpsw_ale.h:1950
ALE init time port specific configuration params.
Definition: cpsw_ale.h:2023
Definition: cpsw_ale.h:806
Definition: cpsw_ale.h:1390
Definition: cpsw_ale.h:1180
bool threadIdEn
Definition: cpsw_ale.h:1708
#define CPSW_ALE_MAX_WHITELIST_IP_NXT_HDR
Maximum IP next header whitelist.
Definition: cpsw_ale.h:95
Policer global configuration parameters.
Definition: cpsw_ale.h:1783
CpswAle_FwdStateLevel
Forward state level.
Definition: cpsw_ale.h:823
CpswAle_UnregulatedTrafficPolicer noMatchPolicer
Definition: cpsw_ale.h:1805
bool portIsTrunk
Definition: cpsw_ale.h:1426
CpswAle_TableEntryType
Defines ALE table entry type.
Definition: cpsw_ale.h:1174
uint32_t srcIpAleEntryIdx
Definition: cpsw_ale.h:1533
CpswAle_Ioctl
ALE IOCTL commands.
Definition: cpsw_ale.h:249
uint32_t regMcastFloodMask
Definition: cpsw_ale.h:1013
uint32_t srcMacAleEntryIdx
Definition: cpsw_ale.h:1579
bool dropDualVlan
Definition: cpsw_ale.h:1982
bool bcastRateLimitForPortEn
Definition: cpsw_ale.h:1336
uint32_t numLSBIgnoreBits
Definition: cpsw_ale.h:1089
bool super
Definition: cpsw_ale.h:935
uint32_t ivlanId
Definition: cpsw_ale.h:1451
bool egressOpEn
Definition: cpsw_ale.h:1628
uint32_t dstMacAleEntryIdx
Definition: cpsw_ale.h:1584
uint32_t routeIdx
Definition: cpsw_ale.h:1827
Definition: cpsw_ale.h:1762
Input args for CPSW_ALE_IOCTL_ADD_UCAST command.
Definition: cpsw_ale.h:903
Get MAC addresses reachable on given port.
Definition: cpsw_ale.h:525
uint32_t ouiAleEntryIdx
Definition: cpsw_ale.h:1574
Definition: cpsw_ale.h:1393
IPv6 entry info.
Definition: cpsw_ale.h:1095
CpswAle_PortState
ALE port state.
Definition: cpsw_ale.h:796
bool hostOuiNoMatchDeny
Definition: cpsw_ale.h:1939
Port specific auto learning security configuration.
Definition: cpsw_ale.h:1959
Input args for CPSW_ALE_IOCTL_GET_POLICER_STATS command.
Definition: cpsw_ale.h:1667
uint32_t unknownVlanMemberListMask
Definition: cpsw_ale.h:1876
Delete all policer entries and associated ALE entry with the given thread id.
Definition: cpsw_ale.h:726
Multicast entry type info apart from MAC address.
Definition: cpsw_ale.h:931
Definition: cpsw_ale.h:1732
Definition: cpsw_ale.h:1177
bool macPortDfltThreadDis
Definition: cpsw_ale.h:1168
Return entry info for given VLAN id.
Definition: cpsw_ale.h:370
#define CPSW_ALE_PUBLIC_IOCTL(x)
Helper macro to create IOCTL commands for ALE module.
Definition: cpsw_ale.h:83
bool aleVlanAwareMode
Definition: cpsw_ale.h:1855
Disable port mirror (match mirror, destination port mirror and source port mirror).
Definition: cpsw_ale.h:570
uint32_t numIgnBits
Definition: cpsw_ale.h:969
CpswAle_PolicerMatchParams policerMatch
Definition: cpsw_ale.h:1817
uint32_t aleEntryIdx
Definition: cpsw_ale.h:1068
ALE IP address classifier info.
Definition: cpsw_ale.h:1399
Set policer/classifier entry.
Definition: cpsw_ale.h:636
Get port state.
Definition: cpsw_ale.h:514
CpswAle_UcastEntryInfo info
Definition: cpsw_ale.h:918
IPv4 entry info.
Definition: cpsw_ale.h:1083
uint32_t totalAddrCnt
Definition: cpsw_ale.h:1145
CpswAle_IPv6EntryInfo ipv6Info
Definition: cpsw_ale.h:1408
Output args for CPSW_ALE_IOCTL_GET_PORT_MACADDR command.
Definition: cpsw_ale.h:1134
CpswAle_TableEntryType entryType
Definition: cpsw_ale.h:1214
Get configured broadcast/multicast rate limit configuration.
Definition: cpsw_ale.h:614
bool srcEn
Definition: cpsw_ale.h:1249
Output args for CPSW_ALE_IOCTL_LOOKUP_UCAST command.
Definition: cpsw_ale.h:915
CpswAle_VlanEntryInfo CpswAle_PortVlanCfg
Port default VLAN configuration.
Definition: cpsw_ale.h:2018
bool vidIngressCheck
Definition: cpsw_ale.h:1059
Input args for CPSW_ALE_IOCTL_DEL_POLICER IOCTL command.
Definition: cpsw_ale.h:1653
#define CPSW_ALE_NUM_PORTS
Number of switch ports in the subsystem.
Definition: cpsw_ale.h:89
CpswAle_PortVlanCfg pvidCfg
Definition: cpsw_ale.h:2035
Return entry info for given multicast address.
Definition: cpsw_ale.h:359
IP packet security configuration.
Definition: cpsw_ale.h:1896
bool srcEn
Definition: cpsw_ale.h:1317
bool unknownVlanNoLearn
Definition: cpsw_ale.h:1864
Set broadcast/multicast rate limit configuration.
Definition: cpsw_ale.h:603
uint32_t commitRateInBitsPerSec
Definition: cpsw_ale.h:1777
Input args for CPSW_ALE_IOCTL_GET_PORT_MACADDR command.
Definition: cpsw_ale.h:1119
Enable OAM loopback for ports in the given port mask.
Definition: cpsw_ale.h:592
uint32_t portNum
Definition: cpsw_ale.h:1110
uint32_t ovlanAleEntryIdx
Definition: cpsw_ale.h:1594
bool dfltThreadEn
Definition: cpsw_ale.h:1159
Dump ALE table entries.
Definition: cpsw_ale.h:262
MAC address and VLAN Id.
Definition: cpsw_ale.h:862
This file contains the type definitions and helper macros for the Enet Forwarding Database (FDB) modu...
Configure policer global settings.
Definition: cpsw_ale.h:714
CpswAle_IpAddrClassifierInfo dstIpInfo
Definition: cpsw_ale.h:1471
uint32_t srcIpAleEntryIdx
Definition: cpsw_ale.h:1604
uint32_t srcPortNumMask
Definition: cpsw_ale.h:1273
Age all entries now.
Definition: cpsw_ale.h:471
OUI entry info.
Definition: cpsw_ale.h:1074
CpswAle_RxFilter
Packet filtering type (cumulative).
Definition: cpsw_ale.h:838
uint64_t addr
Definition: csl_udmap_tr.h:214
bool policerHit
Definition: cpsw_ale.h:1684
CpswAle_PolicerGlobalCfg policerGlobalCfg
Definition: cpsw_ale.h:2050
bool vidIngressCheck
Definition: cpsw_ale.h:1975
bool cpswVlanAwareMode
Definition: cpsw_ale.h:1858
Init time VLAN configuration.
Definition: cpsw_ale.h:1852
uint32_t unknownForceUntaggedEgressMask
Definition: cpsw_ale.h:1867
#define ENET_OUI_ADDR_LEN
Organization Unique Id (OUI) address length in bytes/octets.
Definition: enet_types.h:156
bool portIsTrunk
Definition: cpsw_ale.h:1564
Definition: cpsw_ale.h:847
bool dstEnEn
Definition: cpsw_ale.h:1254
ALE classifier/policer match parameters for source or destination MAC address.
Definition: cpsw_ale.h:1199
bool policerYellowHit
Definition: cpsw_ale.h:1694
uint32_t dstIpAleEntryIdx
Definition: cpsw_ale.h:1538
bool vidIngressCheck
Definition: cpsw_ale.h:1027
CpswAle_MacAddrClassifierInfo dstMacAddrInfo
Definition: cpsw_ale.h:1446
Get ALE policer statistics.
Definition: cpsw_ale.h:682
uint32_t mcastLimitNumPktsPerSec
Definition: cpsw_ale.h:1346
CpswAle_VlanIdInfo vlanIdInfo
Definition: cpsw_ale.h:1002
Get current host port Rx filter.
Definition: cpsw_ale.h:493
uint32_t commitRateInBitsPerSec
Definition: cpsw_ale.h:1622
bool super
Definition: cpsw_ale.h:891
VLAN entry type info.
Definition: cpsw_ale.h:999
Return entry info for given unicast address.
Definition: cpsw_ale.h:348
Add multicast address entry.
Definition: cpsw_ale.h:284
uint32_t etherTypeAleEntryIdx
Definition: cpsw_ale.h:1599
uint32_t dstPortMask
Definition: cpsw_ale.h:1647
MAC authentication configuration.
Definition: cpsw_ale.h:1916
Get InterVLAN routing configuration.
Definition: cpsw_ale.h:762
uint32_t priority
Definition: cpsw_ale.h:1569
uint32_t macAuthDisMask
Definition: cpsw_ale.h:1925
bool macOnlyEn
Definition: cpsw_ale.h:2012
Definition: cpsw_ale.h:1735
bool priorityOrEn
Definition: cpsw_ale.h:1165
bool vid0ModeEn
Definition: cpsw_ale.h:1944
Delete entry info for given EtherType.
Definition: cpsw_ale.h:436
Get default thread configuration.
Definition: cpsw_ale.h:547
CpswAle_MacAddrInfo * addrs
Definition: cpsw_ale.h:1138
uint32_t dstIpAleEntryIdx
Definition: cpsw_ale.h:1609
bool threadIdEn
Definition: cpsw_ale.h:1612
uint32_t numIgnBits
Definition: cpsw_ale.h:945
Add EtherType entry.
Definition: cpsw_ale.h:338
uint32_t egressTrunkIdx
Definition: cpsw_ale.h:1643
Definition: cpsw_ale.h:1186
uint32_t portNum
Definition: cpsw_ale.h:1332
bool clearStats
Definition: cpsw_ale.h:1673
uint32_t policerEntryIdx
Definition: cpsw_ale.h:1625
Input args for CPSW_ALE_IOCTL_SET_TRUNK_CFG command.
Definition: cpsw_ale.h:1279
Output args for CPSW_ALE_IOCTL_GET_POLICER, CPSW_ALE_IOCTL_SET_POLICER_THREADCFG, CPSW_ALE_IOCTL_BLOC...
Definition: cpsw_ale.h:1550
bool threadIdEn
Definition: cpsw_ale.h:1483
CpswAle_McastEntryInfo info
Definition: cpsw_ale.h:978
bool ageable
Definition: cpsw_ale.h:894
uint32_t policerEntryIdx
Definition: cpsw_ale.h:1541
bool disallowIPFrag
Definition: cpsw_ale.h:1065
CpswAle_PolicerYellowThresh yellowThresh
Definition: cpsw_ale.h:1797
ALE port mirroring configuration for mirroring based on packet match.
Definition: cpsw_ale.h:1211
bool noLearn
Definition: cpsw_ale.h:1962
bool enablePri
Definition: cpsw_ale.h:1312
uint32_t addrCnt
Definition: cpsw_ale.h:1142
CpswAle_PortVlanSecurityCfg vlanCfg
Definition: cpsw_ale.h:2029
bool touched
Definition: cpsw_ale.h:922
Set InterVLAN routing configuration.
Definition: cpsw_ale.h:751
#define ENET_IPv4_ADDR_LEN
IPv4 address length in bytes/octets.
Definition: enet_types.h:159
bool innerVlanEn
Definition: cpsw_ale.h:1307
CpswAle_MalformedPktSecurityCfg malformedPktCfg
Definition: cpsw_ale.h:1947
uint32_t aleEntryMask
Definition: cpsw_ale.h:1661
CpswAle_MacAddrInfo addr
Definition: cpsw_ale.h:906
uint32_t commitRateInBitsPerSec
Definition: cpsw_ale.h:1492
bool dstIPEn
Definition: cpsw_ale.h:1296
Broadcast/multicast bandwidth limit configuration parameters.
Definition: cpsw_ale.h:1328
Port MAC mode configuration.
Definition: cpsw_ale.h:1993
uint32_t threadId
Definition: cpsw_ale.h:1616
Set port mirroring configuration.
Definition: cpsw_ale.h:558
Input args for CPSW_ALE_IOCTL_SET_PORT_MIRROR_CFG command.
Definition: cpsw_ale.h:1244
Dump ALE policer entries.
Definition: cpsw_ale.h:671
Set default thread configuration.
Definition: cpsw_ale.h:536
uint32_t policerMatchEnMask
Definition: cpsw_ale.h:1418
CpswAle_PolicerNoMatchMode
Policing Match Mode.
Definition: cpsw_ale.h:1753
Definition: cpsw_ale.h:826
Configure policer global settings. IOCTL params:
Definition: cpsw_ale.h:703
Input args for CPSW_ALE_IOCTL_SET_POLICER_THREADCFG command.
Definition: cpsw_ale.h:1702
Definition: cpsw_ale.h:1183
bool dfltNoFragEn
Definition: cpsw_ale.h:1899
uint32_t trunkHashBase
Definition: cpsw_ale.h:1291
Definition: cpsw_ale.h:1744
uint32_t numPorts
Definition: cpsw_ale.h:1359
Input args for CPSW_ALE_IOCTL_SET_POLICER command.
Definition: cpsw_ale.h:1498
uint32_t threadId
Definition: cpsw_ale.h:1162
CpswAle_AgingCfg agingCfg
Definition: cpsw_ale.h:2053
uint32_t port
Definition: cpsw_ale.h:1559
Input args for CPSW_ALE_IOCTL_LOOKUP_MCAST command.
Definition: cpsw_ale.h:963
Delete all entries.
Definition: cpsw_ale.h:460
uint32_t threadId
Definition: cpsw_ale.h:1486
Output args for CPSW_ALE_IOCTL_LOOKUP_MCAST command.
Definition: cpsw_ale.h:975
uint32_t numPorts
Definition: cpsw_ale.h:1285
Input args for CPSW_ALE_IOCTL_SET_POLICER command.
Definition: cpsw_ale.h:1477
Definition: cpsw_ale.h:1729
Add inner/outer VLAN entry.
Definition: cpsw_ale.h:295
Set thread id for given classifier/policer.
Definition: cpsw_ale.h:693
Definition: cpsw_ale.h:1189
ALE classifier/policer match parameters.
Definition: cpsw_ale.h:1414
bool ttlCheckEn
Definition: cpsw_ale.h:1639
bool redDropEn
Definition: cpsw_ale.h:1794
uint32_t unregMcastFloodMask
Definition: cpsw_ale.h:1047
uint32_t etherTypeAleEntryIdx
Definition: cpsw_ale.h:1528
Add OUI address entry. IOCTL params:
Definition: cpsw_ale.h:305
bool policerRedHit
Definition: cpsw_ale.h:1689
Delete entry info for given IPv6 address.
Definition: cpsw_ale.h:425
bool dfltNxtHdrWhitelistEn
Definition: cpsw_ale.h:1903
Definition: cpsw_ale.h:1192
uint32_t aleEntryIdx
Definition: cpsw_ale.h:981
uint32_t egressTrunkIdx
Definition: cpsw_ale.h:1834
bool noSaUpdateEn
Definition: cpsw_ale.h:1966
uint32_t dstPortNum
Definition: cpsw_ale.h:1262
Enet_VlanTagType
Double tagging VLAN type.
Definition: enet_types.h:369
Set port state.
Definition: cpsw_ale.h:503
bool matchEn
Definition: cpsw_ale.h:1259
uint32_t regMcastFloodMask
Definition: cpsw_ale.h:1050
Definition: cpsw_ale.h:1759
CpswAle_MirrorMatchParams matchParams
Definition: cpsw_ale.h:1270
Set port trunking configuration.
Definition: cpsw_ale.h:581
uint32_t vlanMemberList
Definition: cpsw_ale.h:1044
CpswAle_OuiEntryInfo ouiInfo
Definition: cpsw_ale.h:1436
bool policingEn
Definition: cpsw_ale.h:1787
uint32_t policerMatchEnMask
Definition: cpsw_ale.h:1554
uint32_t modeFlags
Definition: cpsw_ale.h:2047
uint32_t bcastLimitNumPktsPerSec
Definition: cpsw_ale.h:1343
CpswAle_UcastEntryInfo info
Definition: cpsw_ale.h:909
bool blocked
Definition: cpsw_ale.h:882
uint32_t vlanId
Definition: cpsw_ale.h:868
CpswAle_InitVlanCfg vlanCfg
Definition: cpsw_ale.h:2056
Input args for CPSW_ALE_IOCTL_SET_PORT_STATE command.
Definition: cpsw_ale.h:1107
CpswAle_MacAddrClassifierInfo srcMacAddrInfo
Definition: cpsw_ale.h:1441
Delete entry info for given unicast/multicast address.
Definition: cpsw_ale.h:381
uint32_t ovlanId
Definition: cpsw_ale.h:1456
Delete entry info for given IPv4 address.
Definition: cpsw_ale.h:414
Blacklist classifier to host port.
Definition: cpsw_ale.h:740
High level structure with ALE network security configuration.
Definition: cpsw_ale.h:1931
uint32_t unknownUnregMcastFloodMask
Definition: cpsw_ale.h:1873
CpswAle_PolicerMatchParams policerMatch
Definition: cpsw_ale.h:1480
CpswAle_PolicerMatchParams policerMatch
Definition: cpsw_ale.h:1656
uint32_t peakRateInBitsPerSec
Definition: cpsw_ale.h:1619
CpswAle_IpAddrClassifierType
IP address classifier type.
Definition: cpsw_ale.h:1387
uint32_t numPorts
Definition: cpsw_ale.h:1378
Port specific VLAN security configuration.
Definition: cpsw_ale.h:1972
uint16_t etherType
Definition: cpsw_ale.h:1238
#define ENET_IPv6_ADDR_LEN
IPv6 address length in bytes/octets.
Definition: enet_types.h:162
Definition: cpsw_ale.h:853
void CpswAle_initCfg(CpswAle_Cfg *aleCfg)
Initialize CPSW ALE configuration parameters.
bool limitIPNxtHdr
Definition: cpsw_ale.h:1031
CpswAle_McastEntryInfo info
Definition: cpsw_ale.h:957