![]() |
PDK API Guide for J721E
|
Init time VLAN configuration.
Data Fields | |
bool | aleVlanAwareMode |
bool | cpswVlanAwareMode |
bool | autoLearnWithVlan |
bool | unknownVlanNoLearn |
uint32_t | unknownForceUntaggedEgressMask |
uint32_t | unknownRegMcastFloodMask |
uint32_t | unknownUnregMcastFloodMask |
uint32_t | unknownVlanMemberListMask |
bool CpswAle_InitVlanCfg::aleVlanAwareMode |
Configure ALE to operate in VLAN aware mode
bool CpswAle_InitVlanCfg::cpswVlanAwareMode |
Flag indicating if CPSW is in VLAN aware mode
bool CpswAle_InitVlanCfg::autoLearnWithVlan |
Learn VLAN with address when autolearning addresses
bool CpswAle_InitVlanCfg::unknownVlanNoLearn |
Do not learn addresses with unknown VLAN
uint32_t CpswAle_InitVlanCfg::unknownForceUntaggedEgressMask |
Unknown VLAN Force Untagged Egress
uint32_t CpswAle_InitVlanCfg::unknownRegMcastFloodMask |
Unknown VLAN Registered Multicast Flood Mask
uint32_t CpswAle_InitVlanCfg::unknownUnregMcastFloodMask |
Unknown VLAN Multicast Flood Mask
uint32_t CpswAle_InitVlanCfg::unknownVlanMemberListMask |
Unknown VLAN Member List