MCUSW
|
This file contains interface header for CAN MCAL driver.
Go to the source code of this file.
Data Structures | |
struct | Can_MaskType |
Structure defining the filter mask to be used. More... | |
struct | Can_HwFilterType |
Structure defining the HW filter to be used. More... | |
struct | Can_FdBaudConfigType |
Structure defining the CAN FD data phase baud rate configuration. More... | |
struct | Can_BaudConfigType |
Structure defining the CAN baud rate configuration. More... | |
struct | Can_ControllerType |
Can Controller Configuration definition. More... | |
struct | Can_ControllerType_PC |
Can Controller Pre Compile Configuration definition. More... | |
struct | Can_MailboxType |
Can mailox configuration definition. More... | |
struct | Can_MailboxType_PC |
Can mailox Pre compile configuration definition. More... | |
struct | Can_DmaPrms |
Dummy structure will be used if DMA support is required. More... | |
struct | Can_ConfigType |
Can MCAL root configuration structure. More... | |
struct | Can_RegisterReadbackType |
Register Readback Structure. More... | |
Macros | |
#define | CAN_SW_PATCH_VERSION (2U) |
Driver Implementation Patch Version. More... | |
#define | CAN_AR_RELEASE_REVISION_VERSION (1U) |
AUTOSAR Patch version specification implemented by CanDriver. More... | |
Can Driver Module SW Version Info | |
Defines for CAN Driver version used for compatibility checks | |
#define | CAN_SW_MAJOR_VERSION (1U) |
Driver Implementation Major Version.Used for version compatibiltiy check. More... | |
#define | CAN_SW_MINOR_VERSION (3U) |
Driver Implementation Minor Version.Used for version compatibiltiy check. More... | |
Can Driver Module AUTOSAR Version Info | |
Defines for CAN Driver AUTOSAR version used for compatibility checks | |
#define | CAN_AR_RELEASE_MAJOR_VERSION (4U) |
AUTOSAR Major version specification implemented by CanDriver. More... | |
#define | CAN_AR_RELEASE_MINOR_VERSION (3U) |
AUTOSAR Minor version specification implemented by CanDriver. More... | |
Can Driver ID Info | |
#define | CAN_VENDOR_ID (44U) |
Texas Instruments Vendor ID. More... | |
#define | CAN_MODULE_ID (80U) |
Can Driver Module ID. More... | |
#define | CAN_INSTANCE_ID (0U) |
CAN Driver Instance ID. More... | |
CAN Driver states. | |
#define | CAN_UNINIT ((uint8)0U) |
CAN Driver is NOT initialized. More... | |
#define | CAN_READY ((uint8)1U) |
CAN Driver is initialized. More... | |
Can Driver Service Id | |
The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error | |
#define | CAN_INIT_ID (0x00U) |
Can_Init() More... | |
#define | CAN_MAINFCT_WRITE_ID (0x01U) |
Can_MainFunction_Write() More... | |
#define | CAN_SETCTR_ID (0x03U) |
Can_SetControllerMode() More... | |
#define | CAN_DIINT_ID (0x04U) |
Can_DisableControllerInterrupts() More... | |
#define | CAN_ENINT_ID (0x05U) |
Can_EnableControllerInterrupts() More... | |
#define | CAN_WRITE_ID (0x06U) |
Can_Write() More... | |
#define | CAN_VERSION_ID (0x07U) |
Can_GetVersionInfo() More... | |
#define | CAN_MAINFCT_READ_ID (0x08U) |
Can_MainFunction_Read() More... | |
#define | CAN_MAINFCT_BO_ID (0x09U) |
Can_MainFunction_BusOff() More... | |
#define | CAN_MAINFCT_WU_ID (0x0AU) |
Can_MainFunction_Wakeup() More... | |
#define | CAN_CKWAKEUP_ID (0x0BU) |
Can_CheckWakeup() More... | |
#define | CAN_MAINFCT_MODE_ID (0x0CU) |
Can_MainFunction_Mode() More... | |
#define | CAN_SETBAUDRATE_ID (0x0FU) |
Can_SetBaudrate() More... | |
#define | CAN_DEINIT_ID (0x10U) |
Can_DeInit() More... | |
#define | CAN_GETCTRERRST_ID (0x11U) |
Can_GetControllerErrorState() More... | |
#define | CAN_GETCTRMODE_ID (0x12U) |
Can_GetControllerMode() More... | |
#define | CAN_LOOPBACK_ID (0x20U) |
Can_TestLoopBackModeEnable() More... | |
#define | CAN_RXPROCESS_ID (0x21U) |
Can_RxProcess() More... | |
Can Error Codes | |
Error codes returned by Can functions | |
#define | CAN_E_PARAM_POINTER (0x01U) |
#define | CAN_E_PARAM_HANDLE (0x02U) |
ERROR:NULL_PTR passed as parameter. More... | |
#define | CAN_E_PARAM_DLC (0x03U) |
ERROR:Invalid Controller Handle. More... | |
#define | CAN_E_PARAM_CONTROLLER (0x04U) |
ERROR:Invalid length of msg. More... | |
#define | CAN_E_UNINIT (0x05U) |
ERROR:Invalid controller id. More... | |
#define | CAN_E_TRANSITION (0x06U) |
ERROR:Eror due to API invoked without performing Can_Init() More... | |
#define | CAN_E_DATALOST (0x07U) |
ERROR:Eror during Controller state transition. More... | |
#define | CAN_E_PARAM_BAUDRATE (0x08U) |
ERROR:Data lost/dropped. More... | |
#define | CAN_E_ICOM_CONFIG_INVALID (0x09U) |
ERROR:Timeout occured. More... | |
#define | CAN_E_INIT_FAILED (0x0AU) |
ERROR:Invalid Baudrate configuration. More... | |
CAN Config Ids | |
ERROR:Invalid configuration set selection The Config Ids used for different CAN Configuration builds | |
#define | CAN_CFG_ID_0 (0x01U) |
Config 0 (All configurations ON) More... | |
#define | CAN_CFG_ID_1 (0x02U) |
Config 1 (All configurations OFF). CAN_CFG_ID_1 is used only for compile check. More... | |
#define | CAN_CFG_ID_2 (0x04U) |
Config 2 (All configurations ON except DET OFF) More... | |
#define | CAN_CFG_ID_3 (0x08U) |
Config 3 (Configurator auto generated file) More... | |
#define | CAN_CFG_ID_4 (0x10U) |
Config 4 (Configurator auto generated file MCAN instead of DCAN2 with pre-compile variant ON) More... | |
#define | CAN_CFG_ID_5 (0x20U) |
Config 5 (All configurations ON but used only for testing WakeUp by external HW event and Performance tests) More... | |
#define | CAN_CFG_ID_6 (0x40U) |
Config 6 (Used for MCAN Testing) More... | |
Typedefs | |
typedef uint8 | CanControllerState_Type |
Can Controller State enum type. More... | |
typedef uint32 | Can_InterruptMask_Type |
Can Interrupt Mask type. More... | |
Functions | |
void | Can_GetVersionInfo (Std_VersionInfoType *VersionInfo) |
Function returns the version information of this module. More... | |
void | Can_Init (const Can_ConfigType *CfgPtr) |
This function initializes the module. More... | |
Std_ReturnType | Can_SetControllerMode (uint8 Controller, Can_ControllerStateType Transition) |
This function performs software triggered state transitions of the CAN controller State machine. More... | |
Std_ReturnType | Can_Write (Can_HwHandleType Hth, const Can_PduType *PduInfo) |
This function is called by CanIf to pass a CAN message to CanDrv for transmission. More... | |
void | Can_DisableControllerInterrupts (uint8 Controller) |
This function disables all interrupts for this CAN controller. More... | |
void | Can_EnableControllerInterrupts (uint8 Controller) |
This function enables all allowed interrupts. More... | |
void | Can_MainFunction_Write (void) |
This function performs the polling of TX confirmation when CAN_TX_PROCESSING is set to POLLING. More... | |
void | Can_MainFunction_BusOff (void) |
This function performs the polling of bus-off events that are configured statically as 'to be polled'. More... | |
void | Can_MainFunction_Read (void) |
This function performs the polling of RX indications when CAN_RX_PROCESSING is set to POLLING. More... | |
void | Can_MainFunction_Wakeup (void) |
This function performs the polling of wake-up events that are configured statically as 'to be polled'. More... | |
void | Can_MainFunction_Mode (void) |
This function performs the polling of CAN controller mode transitions. More... | |
Std_ReturnType | Can_SetBaudrate (uint8 Controller, uint16 BaudRateConfigID) |
This service shall set the baud rate configuration of the CAN controller. Depending on necessary baud rate modifications the controller might have to reset. More... | |
Std_ReturnType | Can_TestLoopBackModeEnable (uint8 Controller, uint8 Mode) |
This service will enable CAN loopback mode. More... | |
Std_ReturnType | Can_TestLoopBackModeDisable (uint8 Controller, uint8 Mode) |
This service will disable CAN loopback mode. More... | |
Std_ReturnType | Can_RegisterReadback (VAR(uint8,) Controller, Can_RegisterReadbackType *RegRbPtr) |
This service will readback CAN registers. More... | |
void | Can_DeInit (void) |
This function de-initializes the module. More... | |
Std_ReturnType | Can_GetControllerMode (uint8 Controller, Can_ControllerStateType *ControllerModePtr) |
This service reports about the current status of the requested CAN controller. More... | |
Std_ReturnType | Can_GetControllerErrorState (uint8 ControllerId, Can_ErrorStateType *ErrorStatePtr) |
This service obtains the error state of the CAN controller. More... | |