PDK API Guide for J721E
|
Response to get device request.
hdr | TISCI header. |
context_loss_count | Indicates how many times the device has lost context. A driver can use this monotonic counter to determine if the device has lost context since the last time this message was exchanged. |
resets | Programmed state of the reset lines. |
programmed_state | The state as programmed by set_device. |
current_state | The actual state of the hardware. |
Data Fields | |
struct tisci_header | hdr |
uint32_t | context_loss_count |
uint32_t | resets |
uint8_t | programmed_state |
uint8_t | current_state |
struct tisci_header tisci_msg_get_device_resp::hdr |
uint32_t tisci_msg_get_device_resp::context_loss_count |
uint32_t tisci_msg_get_device_resp::resets |
uint8_t tisci_msg_get_device_resp::programmed_state |
uint8_t tisci_msg_get_device_resp::current_state |