![]() |
PDK API Guide for J721E
|
Header that prefixes all TISCI messages.
ROM messaging: Header for loading firmware. This is the same as the firmware header.
type | Type of message identified by a TISCI_MSG_* ID |
host | Host of the message. |
seq | Message identifier indicating a transfer sequence. |
flags | TISCI_MSG_FLAG_* for the message. |
payload | Placeholder pointer that can be used to access the raw message body. |
Data Fields | |
uint16_t | type |
uint8_t | host |
uint8_t | seq |
uint32_t | flags |
uint8_t | payload [] |
uint16_t Sciclient_RomFirmwareLoadHdr_t::type |
uint8_t Sciclient_RomFirmwareLoadHdr_t::host |
uint8_t Sciclient_RomFirmwareLoadHdr_t::seq |
uint32_t Sciclient_RomFirmwareLoadHdr_t::flags |
uint8_t Sciclient_RomFirmwareLoadHdr_t::payload[] |