PDK API Guide for J721E
CSL_CPSW_ALE_VLANMCASTADDR_ENTRY Struct Reference

Detailed Description

Holds the ALE VLAN/Multicast Address Table entry configuration.

Data Fields

Uint8 macAddress [6]
 
Uint32 vlanId
 
Uint32 mcastFwdState
 
Uint32 superEnable
 
Uint32 portMask
 
Uint32 ignMBits
 

Field Documentation

Uint8 CSL_CPSW_ALE_VLANMCASTADDR_ENTRY::macAddress[6]

Multicast address

Uint32 CSL_CPSW_ALE_VLANMCASTADDR_ENTRY::vlanId

VLAN Id

Uint32 CSL_CPSW_ALE_VLANMCASTADDR_ENTRY::mcastFwdState

Multicast forward state

Uint32 CSL_CPSW_ALE_VLANMCASTADDR_ENTRY::superEnable

Supervisory bit enable?

Uint32 CSL_CPSW_ALE_VLANMCASTADDR_ENTRY::portMask

Port Mask.

Uint32 CSL_CPSW_ALE_VLANMCASTADDR_ENTRY::ignMBits

Enable multicast address mask