PDK API Guide for J721E
|
DMSC controls the power management, security and resource management of the device.
Variables | |
enum tisci_msg_value_rm_share_type | __attribute__ |
Enumerations | |
enum | tisci_msg_value_rm_share_type { TISCI_MSG_VALUE_RM_SHARE_EXCLUSIVE = 0u, TISCI_MSG_VALUE_RM_SHARE_OPEN = 1u, TISCI_MSG_VALUE_RM_SHARE_LIMITED = 2u } |
Resource sharing types. More... | |
Macros | |
#define | TISCI_MSG_VALUE_RM_SECONDARY_HOST_VALID ((uint32_t) 1u << 31u) |
This file contains: More... | |
#define | TISCI_MSG_VALUE_RM_UNUSED_SECONDARY_HOST (0xFFu) |
#define TISCI_MSG_VALUE_RM_SECONDARY_HOST_VALID ((uint32_t) 1u << 31u) |
This file contains:
WARNING!!: Autogenerated file from SYSFW. DO NOT MODIFY!! System Firmware TISCI RM Messaging Core
Common TISCI Protocol Definitions for RM messages The secondary_host parameter is valid for any RM TISCI message utilizing the seconday host mechanic.
#define TISCI_MSG_VALUE_RM_UNUSED_SECONDARY_HOST (0xFFu) |
Value specified for the secondary_host element within TISCI RM messages to signify the secondary_host value is not used and the source host of the message is specified in the TISCI message header tisci_header::host field.
Resource sharing types.
Enumerates the sharing options allowed to be programmed for any TISCI RM messages supporting the share parameter.