DMSC controls the power management of the device, hence is responsible for bringing the device out of reset, enforce clock and reset rules. DMSC power management functions are critical to bring device to low power modes, for example DeepSleep, and sense wake-up events to bring device back online to active state.
|
file | sciclient_procboot.h |
| This file contains the definition of all the message IDs, message formats to be able to interact with the System Controller firmware for processor boot and control. APIs are divided into the following two sets:
|
|
|
int32_t | Sciclient_procBootRequestProcessor (uint8_t processorId, uint32_t timeout) |
| Message to request a processor Provides a means for either the “recovery master” host or another host in the permitted access list to request for a physical processor control. More...
|
|
int32_t | Sciclient_procBootReleaseProcessor (uint8_t processorId, uint32_t reqFlag, uint32_t timeout) |
| Message to release a processor Provides a means for the host with current control to relinquish a physical processor control. More...
|
|
int32_t | Sciclient_procBootHandoverProcessor (uint8_t processorId, uint8_t hostId, uint32_t timeout) |
| Message to handover a processor Provides a means for the host with current control to relinquish a physical processor control to another host in the permitted list. More...
|
|
int32_t | Sciclient_procBootSetProcessorCfg (const struct tisci_msg_proc_set_config_req *configReq, uint32_t timeout) |
| Message to set the processor configuration Provides a means for the host with current control to do the base configuration of the processor. More...
|
|
int32_t | Sciclient_procBootSetSequenceCtrl (uint8_t processorId, uint32_t control_flags_1_set, uint32_t control_flags_1_clear, uint32_t reqFlag, uint32_t timeout) |
| Message to setup the processor sequence control. Provides a means for the host with current control to setup limited control flags in specific cases. More...
|
|
int32_t | Sciclient_procBootAuthAndStart (const struct tisci_msg_proc_auth_boot_req *authBootCfg, uint32_t timeout) |
| Message to Authorize and Start Processor Boot: Provides a means for the host with current control to do the following: More...
|
|
int32_t | Sciclient_procBootGetProcessorState (uint8_t processorId, struct tisci_msg_proc_get_status_resp *procStatus, uint32_t timeout) |
| Message to Get Processor Status Provides a means for hosts in the permitted list to get the status of a physical processor. This is required for the hosts to sequence events in the correct order. More...
|
|
int32_t | Sciclient_procBootWaitProcessorState (uint8_t processorId, uint8_t num_match_iterations, uint8_t delay_per_iteration_us, uint32_t status_flags_1_set_all_wait, uint32_t status_flags_1_set_any_wait, uint32_t status_flags_1_clr_all_wait, uint32_t status_flags_1_clr_any_wait, uint32_t reqFlag, uint32_t timeout) |
| Message to Wait for Processor Status Provides a means for hosts to request the SYSFW to wait till a a processor status matches a user defined value. More...
|
|
int32_t Sciclient_procBootRequestProcessor |
( |
uint8_t |
processorId, |
|
|
uint32_t |
timeout |
|
) |
| |
int32_t Sciclient_procBootReleaseProcessor |
( |
uint8_t |
processorId, |
|
|
uint32_t |
reqFlag, |
|
|
uint32_t |
timeout |
|
) |
| |
int32_t Sciclient_procBootHandoverProcessor |
( |
uint8_t |
processorId, |
|
|
uint8_t |
hostId, |
|
|
uint32_t |
timeout |
|
) |
| |
int32_t Sciclient_procBootSetSequenceCtrl |
( |
uint8_t |
processorId, |
|
|
uint32_t |
control_flags_1_set, |
|
|
uint32_t |
control_flags_1_clear, |
|
|
uint32_t |
reqFlag, |
|
|
uint32_t |
timeout |
|
) |
| |
Message to setup the processor sequence control. Provides a means for the host with current control to setup limited control flags in specific cases.
Message: TISCI_MSG_PROC_SET_CONTROL
Request: tisci_msg_proc_set_control_req
Response: tisci_msg_proc_set_control_resp
- Parameters
-
processorId | Index of the processor Refer Sciclient_ProcessorIds. |
control_flags_1_set | Optional Processor specific Control Flags to set. Setting a bit here implies required bit has to be set to 1. |
control_flags_1_clear | Optional Processor specific Control Flags to clear. Setting a bit here implies required bit has to be cleared to 0. |
reqFlag | Can be TISCI_MSG_FLAG_AOR/TISCI_MSG_FLAG_AOP ORRed with additional flag that can be set to alter the device state. |
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
- Returns
- CSL_PASS on success, else failure
Message to Authorize and Start Processor Boot: Provides a means for the host with current control to do the following:
- Authenticate and load a binary using the certificate provided information
- Use certificate information also to setup critical processor specific flags
Message: TISCI_MSG_PROC_AUTH_BOOT
Request: tisci_msg_proc_auth_boot_req
Response: tisci_msg_proc_auth_boot_resp
- Parameters
-
authBootCfg | Configuration Structure for the Authentication and boot |
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
- Returns
- CSL_PASS on success, else failure
int32_t Sciclient_procBootWaitProcessorState |
( |
uint8_t |
processorId, |
|
|
uint8_t |
num_match_iterations, |
|
|
uint8_t |
delay_per_iteration_us, |
|
|
uint32_t |
status_flags_1_set_all_wait, |
|
|
uint32_t |
status_flags_1_set_any_wait, |
|
|
uint32_t |
status_flags_1_clr_all_wait, |
|
|
uint32_t |
status_flags_1_clr_any_wait, |
|
|
uint32_t |
reqFlag, |
|
|
uint32_t |
timeout |
|
) |
| |
Message to Wait for Processor Status Provides a means for hosts to request the SYSFW to wait till a a processor status matches a user defined value.
Message: TISCI_MSG_PROC_WAIT_STATUS
Request: tisci_msg_proc_status_wait_req
Response: tisci_msg_proc_status_wait_resp
- Parameters
-
processorId | Index of the processor Refer Sciclient_ProcessorIds. |
num_match_iterations | Must be between 1 - 255. Specifies number of interations the status bit must be stable, before it is used by API. This is to account for glitches. For eg. specifying a value of 10 would mean that the bit must be stable for 10 iterations before the SYSFW API would report to the host that the bit has changed. |
delay_per_iteration_us | Must be between 0 - 255.Specifies how long to wait (in micro seconds) between each status check. |
status_flags_1_set_all_wait | Optional Processor specific status Flags to wait on. Setting a bit implies that the SYFW will wait until all bits of the status matching this field become '1'. |
status_flags_1_set_any_wait | Optional Processor specific status Flags to wait on. Setting a bit implies that the SYFW will wait until any bit of the status matching this field becomes '1'. |
status_flags_1_clr_all_wait | Optional Processor specific status Flags to wait on. Setting a bit implies that the SYFW will wait until all bits of the status matching this field become '0'. |
status_flags_1_clr_any_wait | Optional Processor specific status Flags to wait on. Setting a bit implies that the SYFW will wait until any bit of the status matching this field becomes '0'. |
timeout | Gives a sense of how long to wait for the operation. Refer Sciclient_ServiceOperationTimeout. |
reqFlag | Can be TISCI_MSG_FLAG_AOR/TISCI_MSG_FLAG_AOP |
- Returns
- CSL_PASS on success, else failure