PDK API Guide for J721E
UDMA Driver Proxy API

Introduction

This is UDMA driver proxy related configuration parameters and API

Files

file  udma_proxy.h
 UDMA proxy related parameters and API.
 

Data Structures

struct  Udma_ProxyCfg
 This structure contains configuration parameters for each proxy thread. More...
 
struct  Udma_ProxyHandle
 UDMA proxy object. More...
 

Functions

int32_t Udma_proxyAlloc (Udma_DrvHandle drvHandle, Udma_ProxyHandle proxyHandle, uint16_t proxyNum)
 UDMA proxy allocation API. More...
 
int32_t Udma_proxyFree (Udma_ProxyHandle proxyHandle)
 UDMA free proxy. More...
 
int32_t Udma_proxyConfig (Udma_ProxyHandle proxyHandle, const Udma_ProxyCfg *proxyCfg)
 UDMA proxy config API. More...
 
static void Udma_proxyQueue (Udma_ProxyHandle proxyHandle, uint64_t phyDescMem)
 UDMA queue descriptor to a proxy which is pre-configured to queue to a ring. More...
 
static void Udma_proxyDequeue (Udma_ProxyHandle proxyHandle, uint64_t *phyDescMem)
 UDMA dequeue descriptor from a proxy which is pre-configured to dequeue from a ring. More...
 
static void Udma_proxyWrite64 (uintptr_t proxyAddr, uint64_t data)
 API to write 64-bit data to proxy. More...
 
static void Udma_proxyRead64 (uintptr_t proxyAddr, uint64_t *data)
 API to read 64-bit data from proxy. More...
 

Macros

#define UDMA_PROXY_INVALID   ((uint16_t) 0xFFFFU)
 Macro used to specify that proxy ID is invalid. More...
 
#define UDMA_PROXY_ANY   ((uint16_t) 0xFFFEU)
 Macro used to specify any available free proxy while requesting one. Used in the API Udma_proxyAlloc. More...
 

Macro Definition Documentation

#define UDMA_PROXY_INVALID   ((uint16_t) 0xFFFFU)

Macro used to specify that proxy ID is invalid.

#define UDMA_PROXY_ANY   ((uint16_t) 0xFFFEU)

Macro used to specify any available free proxy while requesting one. Used in the API Udma_proxyAlloc.

Function Documentation

int32_t Udma_proxyAlloc ( Udma_DrvHandle  drvHandle,
Udma_ProxyHandle  proxyHandle,
uint16_t  proxyNum 
)

UDMA proxy allocation API.

Note: In case of devices like AM64x where there is no proxy, this API is not supported and will return error.

Requirement: DOX_REQ_TAG(PDK-4156)

Parameters
drvHandle[IN] UDMA driver handle pointer passed during Udma_init
proxyHandle[IN/OUT] UDMA proxy handle. The caller need to allocate memory for this object and pass this pointer to all further APIs. The caller should not change any parameters as this is owned and maintained by the driver.
proxyNum[IN] Proxy number. If set to UDMA_PROXY_ANY, will allocate from free proxy pool. Else will try to allocate the mentioned proxy itself.
Returns
Udma_ErrorCodes
int32_t Udma_proxyFree ( Udma_ProxyHandle  proxyHandle)

UDMA free proxy.

Freeup the proxy resources.

Note: In case of devices like AM64x where there is no proxy, this API is not supported and will return error.

Requirement: DOX_REQ_TAG(PDK-4156)

Parameters
proxyHandle[IN] UDMA proxy handle. This parameter can't be NULL.
Returns
Udma_ErrorCodes
int32_t Udma_proxyConfig ( Udma_ProxyHandle  proxyHandle,
const Udma_ProxyCfg proxyCfg 
)

UDMA proxy config API.

This API should be called before performing any proxy operation. This same API can be used to reconfigure the proxy if the ring number changes or the ring (queue/dequeue) operation changes. If there is no change, the proxy queue/dequeue API can be called without the need to reconfigure the proxy (Thus saving CPU cycles)

Note: In case of devices like AM64x where there is no proxy, this API is not supported and will return error.

Requirement: DOX_REQ_TAG(PDK-4156)

Parameters
proxyHandle[IN] UDMA proxy handle. This parameter can't be NULL.
proxyCfg[IN] UDMA proxy configuration. This parameter can't be NULL. For queue operation the mode parameter should be set to CSL_PROXY_QUEUE_ACCESS_MODE_TAIL For dequeue operation the mode parameter should be set to CSL_PROXY_QUEUE_ACCESS_MODE_HEAD
Returns
Udma_ErrorCodes
static void Udma_proxyQueue ( Udma_ProxyHandle  proxyHandle,
uint64_t  phyDescMem 
)
inlinestatic

UDMA queue descriptor to a proxy which is pre-configured to queue to a ring.

Caution: This API doesn't do any error check for performance reasons The user should ensure that the proxy is configured to perform a dequeue or queue operation to a ring. Caution: User should also ensure that the corresponding ring is not full. Performing a proxy queue operation to an already full ring will result in ring error (overflow).

Requirement: DOX_REQ_TAG(PDK-4156)

Parameters
proxyHandle[IN] UDMA proxy handle. This parameter can't be NULL.
phyDescMem[IN] Descriptor memory physical pointer to push to the ring.
static void Udma_proxyDequeue ( Udma_ProxyHandle  proxyHandle,
uint64_t *  phyDescMem 
)
inlinestatic

UDMA dequeue descriptor from a proxy which is pre-configured to dequeue from a ring.

Caution: This API doesn't do any error check for performance reasons The user should ensure that the proxy is configured to perform a dequeue or queue operation to a ring. Caution: User should also ensure that the corresponding ring is not empty. Performing a proxy dequeue operation to an empty ring will result in ring error (underflow).

Requirement: DOX_REQ_TAG(PDK-4156)

Parameters
proxyHandle[IN] UDMA proxy handle. This parameter can't be NULL.
phyDescMem[OUT] Descriptor memory physical pointer read from the ring. This will be NULL if there is nothing to pop from the ring.
static void Udma_proxyWrite64 ( uintptr_t  proxyAddr,
uint64_t  data 
)
inlinestatic

API to write 64-bit data to proxy.

Requirement: DOX_REQ_TAG(PDK-4156)

Parameters
proxyAddr[IN] Proxy data address (pre-calculated for a 64-bit write).
data[IN] 64-bit data to write.
static void Udma_proxyRead64 ( uintptr_t  proxyAddr,
uint64_t *  data 
)
inlinestatic

API to read 64-bit data from proxy.

Requirement: DOX_REQ_TAG(PDK-4156)

Parameters
proxyAddr[IN] Proxy data address (pre-calculated for a 64-bit read).
data[OUT] Pointer to 64-bit word where the data is read to.