This is VISS GLBCE Configuration file
|
file | glbce_cfg.h |
| Interface file for GLBCE module, Defines the structures / control operations that could be used to configure / control GLBCE module in VISS GLBCE is independent module, between RAW FE and FCFA. This is why a separate interface file is used for controlling GLBCE.
|
|
|
struct | Glbce_Config |
| GLBCE configuration structure Used to configure common GLBCE configuration which is used for contrast brightness enhancement. More...
|
|
struct | Glbce_PerceptConfig |
| Control structure for Perceptual Module. Used for both forward & reverse. Used to enable/disable module and to set Perceptual Lut. More...
|
|
struct | Glbce_WdrConfig |
| Control structure for WDR Module. Used to enable/disable module and to set WDR Lut. More...
|
|
struct | Glbce_StatsInfo |
| GLBCE Stats memory information Used to get the address and size of the GLBCE statistics memory for the context save and restore purpose. More...
|
|
struct | Glbce_Control |
| GLBCE control structure, passed as an argument to IOCTL_GLBCE_SET_CONFIG. More...
|
|
|
Control Commands for GLBCE module in VISS
|
#define | IOCTL_GLBCE_SET_CONFIG |
| Used for setting individual GLBCE sub-module's configuration. Single ioctl for configuring all sub-module's configuration, by selecting module id and setting appropriate pointer in Glbce_Control. More...
|
|
#define | IOCTL_GLBCE_GET_CONFIG |
| Used for getting individual GLBCE sub-module's configuration. Single ioctl for configuring all sub-module's configuration, by selecting module id and setting appropriate pointer in Glbce_Control. More...
|
|
#define IOCTL_GLBCE_SET_CONFIG |
Value: 1U)
#define VHWA_IOCTL_GLBCE_IOCTL_BASE
Definition: vhwa_common.h:158
Used for setting individual GLBCE sub-module's configuration. Single ioctl for configuring all sub-module's configuration, by selecting module id and setting appropriate pointer in Glbce_Control.
- Returns
- FVID2_SOK on success, else error code.
#define IOCTL_GLBCE_GET_CONFIG |
Value: 2U)
#define VHWA_IOCTL_GLBCE_IOCTL_BASE
Definition: vhwa_common.h:158
Used for getting individual GLBCE sub-module's configuration. Single ioctl for configuring all sub-module's configuration, by selecting module id and setting appropriate pointer in Glbce_Control.
Currently this is supported only Statistics information.
- Returns
- FVID2_SOK on success, else error code.
#define GLBCE_ASYMMETRY_LUT_SIZE (33U) |
Size of the asymmentry LUT.
#define GLBCE_PERCEPT_LUT_SIZE (65U) |
#define GLBCE_WDR_LUT_SIZE (257U) |
#define GLBCE_ASYMMETRY_LUT_SECOND_POLE (255U) |
Value of the second pole, used in generating assymetry lut.
#define GLBCE_NO_DITHER (0x0U) |
< No Dithering One least significant bit of the output is dithered
#define GLBCE_DITHER_ONE_BIT (0x1U) |
Two least significant bit of the output are dithered
#define GLBCE_DITHER_TWO_BIT (0x2U) |
Three least significant bit of the output are dithered
#define GLBCE_DITHER_THREE_BIT (0x3U) |
Four least significant bit of the output are dithered
#define GLBCE_DITHER_FOUR_BIT (0x4U) |
Max Dither, used for error checking
#define GLBCE_DITHER_MAX (0x5U) |
#define GLBCE_MODULE_GLBCE (0x0U) |
< Configure GLBCE common Settings Configure Forward Perceptual Settings
#define GLBCE_MODULE_FWD_PERCEPT (0x1U) |
Configure Forward Perceptual Settings
#define GLBCE_MODULE_REV_PERCEPT (0x2U) |
Command to get the GLBCE Stats Information
#define GLBCE_MODULE_GET_STATS_INFO (0x3U) |
Command to get/set WDR module configuration
#define GLBCE_MODULE_WDR (0x4U) |