This is CSI2 Tx's top level include for applications.
|
file | csitx.h |
| CSITX Driver API/interface file.
|
|
#define CSITX_TX_DRV_ID (FVID2_CSITX_DRV_BASE + 0x00000000U) |
Application API calling sequence:
- Csitx_init()
- to initialize CSITX Driver
- Csitx_initParamsInit()
- to initialize initialization parameters
- Csitx_createParamsInit()
- to initialize create time parameters
- Csitx_instStatusInit()
- not mandatory
- to initialize driver instance status parameters
- Fvid2_create()
- to create CSITX driver instance
- Fvid2_control(FVID2_REGISTER_TIMESTAMP_FXN)
- to register time-stamping function
- Fvid2_control(IOCTL_CSITX_REGISTER_EVENT)
- mandatory for error handling
- to enable event handling in CSITX driver
- Fvid2_start()
- to start CSITX driver instance
- Fvid2_queue() and Fvid2_dequeue()
- Fvid2_stop()
- to stop CSITX driver instance
- Fvid2_delete()
- to delete CSITX driver instance
- Csitx_deInit()
- to un-initialize CSITX DriverCSITX transmit driver ID used at the time of FVID2 create.
#define IOCTL_CSITX_GET_INST_STATUS (FVID2_CSITX_DRV_IOCTL_BASE + 0x0000U) |
Get transmit status IOCTL.
This IOCTL can be used to get the transmit status like number of frames queued/dequeued. Note: These counters will be reset either at the time of driver create or while starting the transmit operation. See respective counter comments for details.
- Parameters
-
- Returns
- FVID2_SOK on success, else failure
#define IOCTL_CSITX_PRINT_DEBUG_LOGS (FVID2_CSITX_DRV_IOCTL_BASE + 0x0100U) |
Print transmit debug logs.
This IOCTL can be used to print the transmit debug logs if enabled through CSITX_DRV_ENABLE_DEBUG. Note: These logs will be reset at the time of driver create.
- Parameters
-
cmdArgs | [OUT] NULL |
cmdArgsStatus | [OUT] NULL |
- Returns
- FVID2_SOK on success, else failure