PDK API Guide for J721E
|
Capture status structure used to get the current status.
Data Fields | |
uint32_t | queueCount [CSITX_NUM_CH] |
uint32_t | dequeueCount [CSITX_NUM_CH] |
uint32_t | frmRepeatCount [CSITX_NUM_CH] |
uint32_t | overflowCount |
uint32_t Csitx_InstStatus::queueCount[CSITX_NUM_CH] |
Counter to keep track of how many requests are queued to the driver. Note: This counter will be reset at the time of driver init.
uint32_t Csitx_InstStatus::dequeueCount[CSITX_NUM_CH] |
Counter to keep track of how many requests are dequeued from the driver. Note: This counter will be reset at the time of driver init.
uint32_t Csitx_InstStatus::frmRepeatCount[CSITX_NUM_CH] |
Counter to keep track of how many frames are repeated from the driver when no buffers are queued by the application. Note: This counter will be reset at the time of driver init.
uint32_t Csitx_InstStatus::overflowCount |
Counter to keep track of the occurrence of overflow error. Note: This counter will be reset at the time of driver create and during driver start.