81 #ifndef DSPLIB_QRD_INVERSE_IXX_IXX_OXX_H_
82 #define DSPLIB_QRD_INVERSE_IXX_IXX_OXX_H_
84 #include "../common/DSPLIB_types.h"
215 void *restrict pInvA,
216 void *restrict pInvAScratch,
217 void *restrict pScratch);
261 void *restrict pInvA,
262 void *restrict pInvAScratch,
263 void *restrict pScratch);
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
DSPLIB_STATUS DSPLIB_qrd_inverse_init_checkParams(DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsQ, DSPLIB_bufParams2D_t *bufParamsR, DSPLIB_bufParams2D_t *bufParamsInvA, DSPLIB_bufParams2D_t *bufParamsInvAFinal, const DSPLIB_qrdInvInitArgs *pKerInitArgs)
This function checks the validity of the parameters passed to DSPLIB_qrd_inverse_init function....
DSPLIB_STATUS DSPLIB_qrd_inverse_exec_checkParams(DSPLIB_kernelHandle handle, void *restrict pQ, void *restrict pR, void *restrict pInvA, void *restrict pInvAScratch, void *restrict pScratch)
This function checks the validity of the parameters passed to DSPLIB_qrd_inverse_exec function....
DSPLIB_STATUS DSPLIB_qrd_inverse_exec(DSPLIB_kernelHandle handle, void *restrict pQ, void *restrict pR, void *restrict pInvA, void *restrict pInvAScratch, void *restrict pScratch)
This function is the main kernel compute function.
DSPLIB_STATUS DSPLIB_qrd_inverse_init(DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsQ, DSPLIB_bufParams2D_t *bufParamsR, DSPLIB_bufParams2D_t *bufParamsInvA, DSPLIB_bufParams2D_t *bufParamsInvAFinal, const DSPLIB_qrdInvInitArgs *pKerInitArgs)
This function should be called before the DSPLIB_qrd_inverse_exec function is called....
int32_t DSPLIB_qrd_inverse_getHandleSize(DSPLIB_qrdInvInitArgs *pKerInitArgs)
This is a query function to calculate the size of internal handle.
A structure for a 2 dimensional buffer descriptor.
Structure containing the parameters to initialize the kernel.
uint32_t dimX
Size of input data.
uint32_t dimY
Size of input data.
int8_t funcStyle
Variant of the function refer to DSPLIB_FUNCTION_STYLE