Go to the source code of this file.
|
| int32_t | DSPLIB_qrd_inverse_getHandleSize (DSPLIB_qrdInvInitArgs *pKerInitArgs) |
| | This is a query function to calculate the size of internal handle. More...
|
| |
| DSPLIB_STATUS | DSPLIB_qrd_inverse_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsQ, DSPLIB_bufParams2D_t *bufParamsR, DSPLIB_bufParams2D_t *bufParamsInvA, DSPLIB_bufParams2D_t *bufParamsInvAFinal, const DSPLIB_qrdInvInitArgs *pKerInitArgs) |
| | This function should be called before the DSPLIB_qrd_inverse_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the streaming engine and streaming address generator. The results of these operations are stored in the handle. More...
|
| |
| DSPLIB_STATUS | DSPLIB_qrd_inverse_init_checkParams (DSPLIB_kernelHandle handle, DSPLIB_bufParams2D_t *bufParamsQ, DSPLIB_bufParams2D_t *bufParamsR, DSPLIB_bufParams2D_t *bufParamsInvA, DSPLIB_bufParams2D_t *bufParamsInvAFinal, const DSPLIB_qrdInvInitArgs *pKerInitArgs) |
| | This function checks the validity of the parameters passed to DSPLIB_qrd_inverse_init function. This function is called with the same parameters as the DSPLIB_qrd_inverse_init, and this function must be called before the DSPLIB_qrd_inverse_init is called. More...
|
| |
| DSPLIB_STATUS | DSPLIB_qrd_inverse_exec_checkParams (DSPLIB_kernelHandle handle, void *restrict pQ, void *restrict pR, void *restrict pInvA, void *restrict pInvAScratch, void *restrict pScratch) |
| | This function checks the validity of the parameters passed to DSPLIB_qrd_inverse_exec function. This function is called with the same parameters as the DSPLIB_qrd_inverse_exec, and this function must be called before the DSPLIB_qrd_inverse_exec is called. More...
|
| |
| DSPLIB_STATUS | DSPLIB_qrd_inverse_exec (DSPLIB_kernelHandle handle, void *restrict pQ, void *restrict pR, void *restrict pInvA, void *restrict pInvAScratch, void *restrict pScratch) |
| | This function is the main kernel compute function. More...
|
| |