21 #ifndef DSPLIB_CHOLESKY_IXX_IXX_OXX_PRIV_H_
22 #define DSPLIB_CHOLESKY_IXX_IXX_OXX_PRIV_H_
24 #include "../common/DSPLIB_inlines.h"
25 #include "../common/DSPLIB_utility.h"
40 #define DSPLIB_cholesky_IXX_IXX_OXX_PBLOCK_SIZE (7 * SE_PARAM_SIZE)
50 void *restrict multiplierPtr);
76 template <
typename dataType>
104 template <
typename dataType>
107 void *restrict pOutU,
108 void *restrict multiplierPtr);
124 template <
typename dataType>
127 void *restrict pOutU,
128 void *restrict multiplierPtr);
DSPLIB_STATUS DSPLIB_cholesky_exec_ci(DSPLIB_kernelHandle handle, void *restrict pInA, void *restrict pOutU, void *restrict multiplierPtr)
This function is the main execution function for the C7x implementation of the kernel....
DSPLIB_STATUS(* pFxnDSPLIB_cholesky_exec)(DSPLIB_kernelHandle handle, void *restrict pInA, void *restrict pOutU, void *restrict multiplierPtr)
This is a function pointer type that conforms to the declaration of DSPLIB_cholesky_exec_ci and DSPLI...
#define DSPLIB_cholesky_IXX_IXX_OXX_PBLOCK_SIZE
Macro to define the size of bufPblock array of DSPLIB_cholesky_PrivArgs structure.
DSPLIB_STATUS DSPLIB_cholesky_init_ci(DSPLIB_kernelHandle handle, const DSPLIB_bufParams2D_t *bufParamsIn, const DSPLIB_bufParams2D_t *bufParamsOut, const DSPLIB_cholesky_InitArgs *pKerInitArgs)
This function is the initialization function for the C7x implementation of the kernel....
DSPLIB_STATUS DSPLIB_cholesky_exec_cn(DSPLIB_kernelHandle handle, void *restrict pInA, void *restrict pOutU, void *restrict multiplierPtr)
This function is the main execution function for the natural C implementation of the kernel....
DSPLIB_STATUS_NAME DSPLIB_STATUS
Return value for DSPLIB functions.
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
A structure for a 2 dimensional buffer descriptor.
Structure containing the parameters to initialize the kernel.
Structure that is reserved for internal use by the kernel.
int32_t order
Order of input buffer for different batches DSPLIB_cholesky_init that will be retrieved and used by D...
pFxnDSPLIB_cholesky_exec execute
Function pointer to point to the right execution variant between DSPLIB_cholesky_exec_cn and DSPLIB_c...
int32_t shiftForVecLenDiv