![]() |
DSPLIB User Guide
|
Go to the source code of this file.
Macros | |
| #define | SE_PARAM_BASE (0x0000) |
| #define | SE_SE0_PARAM_OFFSET (SE_PARAM_BASE) |
| #define | SE_SE1_PARAM_OFFSET (SE_SE0_PARAM_OFFSET + SE_PARAM_SIZE) |
| #define | SE_SE2_PARAM_OFFSET (SE_SE1_PARAM_OFFSET + SE_PARAM_SIZE) |
| #define | SE_SE3_PARAM_OFFSET (SE_SE2_PARAM_OFFSET + SE_PARAM_SIZE) |
| #define | SA_SA0_PARAM_OFFSET (SE_SE3_PARAM_OFFSET + SE_PARAM_SIZE) |
| #define | SA_SA1_PARAM_OFFSET (SA_SA0_PARAM_OFFSET + SA_PARAM_SIZE) |
| #define | SA_SA2_PARAM_OFFSET (SA_SA1_PARAM_OFFSET + SA_PARAM_SIZE) |
Functions | |
| template<typename dataType > | |
| DSPLIB_STATUS | DSPLIB_cholesky_inplace_isPosDefinite_init (int32_t order, int32_t colStride, uint8_t *pBlock) |
| template<typename dataType > | |
| dataType | DSPLIB_cholesky_inplace_isPosDefinite (dataType *A, const int32_t order, const int32_t eleCount, uint8_t *pBlock) |
| #define SE_PARAM_BASE (0x0000) |
Definition at line 97 of file DSPLIB_cholesky_common.h.
| #define SE_SE0_PARAM_OFFSET (SE_PARAM_BASE) |
Definition at line 98 of file DSPLIB_cholesky_common.h.
| #define SE_SE1_PARAM_OFFSET (SE_SE0_PARAM_OFFSET + SE_PARAM_SIZE) |
Definition at line 99 of file DSPLIB_cholesky_common.h.
| #define SE_SE2_PARAM_OFFSET (SE_SE1_PARAM_OFFSET + SE_PARAM_SIZE) |
Definition at line 100 of file DSPLIB_cholesky_common.h.
| #define SE_SE3_PARAM_OFFSET (SE_SE2_PARAM_OFFSET + SE_PARAM_SIZE) |
Definition at line 101 of file DSPLIB_cholesky_common.h.
| #define SA_SA0_PARAM_OFFSET (SE_SE3_PARAM_OFFSET + SE_PARAM_SIZE) |
Definition at line 102 of file DSPLIB_cholesky_common.h.
| #define SA_SA1_PARAM_OFFSET (SA_SA0_PARAM_OFFSET + SA_PARAM_SIZE) |
Definition at line 103 of file DSPLIB_cholesky_common.h.
| #define SA_SA2_PARAM_OFFSET (SA_SA1_PARAM_OFFSET + SA_PARAM_SIZE) |
Definition at line 104 of file DSPLIB_cholesky_common.h.
| DSPLIB_STATUS DSPLIB_cholesky_inplace_isPosDefinite_init | ( | int32_t | order, |
| int32_t | colStride, | ||
| uint8_t * | pBlock | ||
| ) |
Definition at line 37 of file DSPLIB_cholesky_common.cpp.
| dataType DSPLIB_cholesky_inplace_isPosDefinite | ( | dataType * | A, |
| const int32_t | order, | ||
| const int32_t | eleCount, | ||
| uint8_t * | pBlock | ||
| ) |
Definition at line 97 of file DSPLIB_cholesky_common.cpp.