75 if ((pIn == NULL) || (pOut == NULL)) {
191 status = pKerPrivArgs->
execute(handle, pIn, pOut);
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< int64_t, DSPLIB_UINT64 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< int16_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< uint16_t, DSPLIB_UINT16 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< uint32_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< double, DSPLIB_UINT64 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< uint16_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< double >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< uint64_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< int32_t, DSPLIB_UINT32 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< uint32_t, DSPLIB_UINT32 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< int16_t, DSPLIB_UINT16 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< int32_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< float, DSPLIB_UINT32 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< float >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< uint64_t, DSPLIB_UINT64 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< int64_t >(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_cn< float, DSPLIB_UINT32 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
DSPLIB_STATUS DSPLIB_blk_eswap_init_cn(DSPLIB_kernelHandle handle, DSPLIB_bufParams1D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
This function is the initialization function for the natural C implementation of the kernel....
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_cn< int32_t, DSPLIB_UINT32 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_cn< uint32_t, DSPLIB_UINT32 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_cn< uint16_t, DSPLIB_UINT16 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_cn< uint64_t, DSPLIB_UINT64 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_cn< int64_t, DSPLIB_UINT64 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_cn< int16_t, DSPLIB_UINT16 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_cn< double, DSPLIB_UINT64 >(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
Header file for kernel's internal use. For the kernel's interface, please see DSPLIB_blk_eswap.
#define DSPLIB_DEBUGPRINTFN(N, fmt,...)
DSPLIB_STATUS_NAME
The enumeration of all status codes.
void * DSPLIB_kernelHandle
Handle type for DSPLIB operations.
@ DSPLIB_ERR_NULL_POINTER
@ DSPLIB_ERR_INVALID_TYPE
DSPLIB_STATUS DSPLIB_blk_eswap_exec_checkParams(DSPLIB_kernelHandle handle, const void *restrict pIn, const void *restrict pOut)
This function checks the validity of the parameters passed to DSPLIB_blk_eswap_exec function....
DSPLIB_STATUS DSPLIB_blk_eswap_init(DSPLIB_kernelHandle handle, DSPLIB_bufParams1D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
This function should be called before the DSPLIB_blk_eswap_exec function is called....
DSPLIB_STATUS DSPLIB_blk_eswap_exec(DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
This function is the main kernel swapping function.
int32_t DSPLIB_blk_eswap_getHandleSize(DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
This is a query function to calculate the size of internal handle.
DSPLIB_STATUS DSPLIB_blk_eswap_init_checkParams(DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
This function checks the validity of the parameters passed to DSPLIB_blk_eswap_init function....
Structure containing the parameters to initialize the kernel.
int8_t funcStyle
Variant of the function refer to DSPLIB_FUNCTION_STYLE
uint32_t dataSize
Size of input data
Structure that is reserved for internal use by the kernel.
pFxnDSPLIB_blk_eswap_exec execute
Function pointer to point to the right execution variant between DSPLIB_blk_eswap_exec_cn and DSPLIB_...
int32_t blockSize
Size of input buffer for different batches DSPLIB_blk_eswap_init that will be retrieved and used by D...
A structure for a 1 dimensional buffer descriptor.
uint32_t data_type
Values are of type DSPLIB_data_type_e.