DSPLIB User Guide
DSPLIB_blk_eswap_ci.cpp File Reference

Go to the source code of this file.

Functions

template<uint32_t maskType>
c7x::uchar_vec blk_eswap_mask ()
 
template<>
c7x::uchar_vec blk_eswap_mask< DSPLIB_UINT16 > ()
 
template<>
c7x::uchar_vec blk_eswap_mask< DSPLIB_UINT32 > ()
 
template<>
c7x::uchar_vec blk_eswap_mask< DSPLIB_UINT64 > ()
 
template<typename dataType >
DSPLIB_STATUS DSPLIB_blk_eswap_init_ci (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
 This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_blk_eswap_init. More...
 
template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< uint16_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
 
template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< uint32_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
 
template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< uint64_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
 
template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< int16_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
 
template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< int32_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
 
template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< int64_t > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
 
template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< float > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
 
template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< double > (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_blk_eswap_InitArgs *pKerInitArgs)
 
template<typename dataType , uint32_t maskType>
DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_blk_eswap_exec. More...
 
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< uint16_t, DSPLIB_UINT16 > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< uint32_t, DSPLIB_UINT32 > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< uint64_t, DSPLIB_UINT64 > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< int16_t, DSPLIB_UINT16 > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< int32_t, DSPLIB_UINT32 > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< int64_t, DSPLIB_UINT64 > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< float, DSPLIB_UINT32 > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 
template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< double, DSPLIB_UINT64 > (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 

Function Documentation

◆ blk_eswap_mask()

template<uint32_t maskType>
c7x::uchar_vec blk_eswap_mask ( )
inline

◆ blk_eswap_mask< DSPLIB_UINT16 >()

template<>
c7x::uchar_vec blk_eswap_mask< DSPLIB_UINT16 > ( )
inline

Definition at line 344 of file DSPLIB_blk_eswap_ci.cpp.

◆ blk_eswap_mask< DSPLIB_UINT32 >()

template<>
c7x::uchar_vec blk_eswap_mask< DSPLIB_UINT32 > ( )
inline

Definition at line 346 of file DSPLIB_blk_eswap_ci.cpp.

◆ blk_eswap_mask< DSPLIB_UINT64 >()

template<>
c7x::uchar_vec blk_eswap_mask< DSPLIB_UINT64 > ( )
inline

Definition at line 348 of file DSPLIB_blk_eswap_ci.cpp.

◆ DSPLIB_blk_eswap_init_ci()

template<typename dataType >
DSPLIB_STATUS DSPLIB_blk_eswap_init_ci ( DSPLIB_kernelHandle  handle,
const DSPLIB_bufParams1D_t bufParamsIn,
const DSPLIB_bufParams1D_t bufParamsOut,
const DSPLIB_blk_eswap_InitArgs pKerInitArgs 
)

This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_blk_eswap_init.

This function determines the configuration for the streaming engine resources based on the function call parameters, and the configuration is saved in bufPBlock array. In the kernel call sequence, DSPLIB_blk_eswap_exec_ci would be called later independently by the application. When DSPLIB_blk_eswap_exec_ci runs, it merely retrieves the configuration from the bufPBlock and uses it to set up the hardware resources. This arrangement is so that DSPLIB_blk_eswap_exec_ci does not lose cycles to determine the hardware configuration.

Parameters
[in]handle: Active handle to the kernel
[in]bufParamsIn: Pointer to the structure containing dimensional information of input buffer
[out]bufParamsOut: Pointer to the structure containing dimensional information of ouput buffer
[in]pKerInitArgs: Pointer to the structure holding init parameters
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.

Definition at line 351 of file DSPLIB_blk_eswap_ci.cpp.

◆ DSPLIB_blk_eswap_init_ci< uint16_t >()

template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< uint16_t > ( DSPLIB_kernelHandle  handle,
const DSPLIB_bufParams1D_t bufParamsIn,
const DSPLIB_bufParams1D_t bufParamsOut,
const DSPLIB_blk_eswap_InitArgs pKerInitArgs 
)

◆ DSPLIB_blk_eswap_init_ci< uint32_t >()

template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< uint32_t > ( DSPLIB_kernelHandle  handle,
const DSPLIB_bufParams1D_t bufParamsIn,
const DSPLIB_bufParams1D_t bufParamsOut,
const DSPLIB_blk_eswap_InitArgs pKerInitArgs 
)

◆ DSPLIB_blk_eswap_init_ci< uint64_t >()

template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< uint64_t > ( DSPLIB_kernelHandle  handle,
const DSPLIB_bufParams1D_t bufParamsIn,
const DSPLIB_bufParams1D_t bufParamsOut,
const DSPLIB_blk_eswap_InitArgs pKerInitArgs 
)

◆ DSPLIB_blk_eswap_init_ci< int16_t >()

template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< int16_t > ( DSPLIB_kernelHandle  handle,
const DSPLIB_bufParams1D_t bufParamsIn,
const DSPLIB_bufParams1D_t bufParamsOut,
const DSPLIB_blk_eswap_InitArgs pKerInitArgs 
)

◆ DSPLIB_blk_eswap_init_ci< int32_t >()

template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< int32_t > ( DSPLIB_kernelHandle  handle,
const DSPLIB_bufParams1D_t bufParamsIn,
const DSPLIB_bufParams1D_t bufParamsOut,
const DSPLIB_blk_eswap_InitArgs pKerInitArgs 
)

◆ DSPLIB_blk_eswap_init_ci< int64_t >()

template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< int64_t > ( DSPLIB_kernelHandle  handle,
const DSPLIB_bufParams1D_t bufParamsIn,
const DSPLIB_bufParams1D_t bufParamsOut,
const DSPLIB_blk_eswap_InitArgs pKerInitArgs 
)

◆ DSPLIB_blk_eswap_init_ci< float >()

template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< float > ( DSPLIB_kernelHandle  handle,
const DSPLIB_bufParams1D_t bufParamsIn,
const DSPLIB_bufParams1D_t bufParamsOut,
const DSPLIB_blk_eswap_InitArgs pKerInitArgs 
)

◆ DSPLIB_blk_eswap_init_ci< double >()

template DSPLIB_STATUS DSPLIB_blk_eswap_init_ci< double > ( DSPLIB_kernelHandle  handle,
const DSPLIB_bufParams1D_t bufParamsIn,
const DSPLIB_bufParams1D_t bufParamsOut,
const DSPLIB_blk_eswap_InitArgs pKerInitArgs 
)

◆ DSPLIB_blk_eswap_exec_ci()

template<typename dataType , uint32_t maskType>
DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_blk_eswap_exec.

The function uses one streaming engine to load the input data then endian swap operation is performed. The result is then stored using streaming address generator.

Parameters
[in]handle: Active handle to the kernel
[in]pIn: Pointer to buffer holding the input data
[out]pOut: Pointer to buffer holding the output data
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.
Performance Considerations:
For best performance,
  • the input and output data buffers are expected to be in L2 memory
  • the buffer pointers are assumed to be 64-byte aligned

Definition at line 427 of file DSPLIB_blk_eswap_ci.cpp.

◆ DSPLIB_blk_eswap_exec_ci< uint16_t, DSPLIB_UINT16 >()

template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< uint16_t, DSPLIB_UINT16 > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

◆ DSPLIB_blk_eswap_exec_ci< uint32_t, DSPLIB_UINT32 >()

template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< uint32_t, DSPLIB_UINT32 > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

◆ DSPLIB_blk_eswap_exec_ci< uint64_t, DSPLIB_UINT64 >()

template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< uint64_t, DSPLIB_UINT64 > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

◆ DSPLIB_blk_eswap_exec_ci< int16_t, DSPLIB_UINT16 >()

template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< int16_t, DSPLIB_UINT16 > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

◆ DSPLIB_blk_eswap_exec_ci< int32_t, DSPLIB_UINT32 >()

template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< int32_t, DSPLIB_UINT32 > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

◆ DSPLIB_blk_eswap_exec_ci< int64_t, DSPLIB_UINT64 >()

template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< int64_t, DSPLIB_UINT64 > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

◆ DSPLIB_blk_eswap_exec_ci< float, DSPLIB_UINT32 >()

template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< float, DSPLIB_UINT32 > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

◆ DSPLIB_blk_eswap_exec_ci< double, DSPLIB_UINT64 >()

template DSPLIB_STATUS DSPLIB_blk_eswap_exec_ci< double, DSPLIB_UINT64 > ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)