DSPLIB User Guide
DSPLIB_w_vec_priv.h File Reference

Introduction

Header file for kernel's internal use. For the kernel's interface, please see DSPLIB_w_vec.

Definition in file DSPLIB_w_vec_priv.h.

Go to the source code of this file.

Data Structures

struct  DSPLIB_w_vec_PrivArgs
 Structure that is reserved for internal use by the kernel. More...
 

Macros

#define DSPLIB_W_VEC_IXX_IXX_OXX_PBLOCK_SIZE   (2 * SE_PARAM_SIZE + 1 * DSPLIB_PARAM_SIZE + 2 * sizeof(int32_t))
 Macro to define the size of bufPblock array of DSPLIB_w_vec_PrivArgs structure. More...
 

Typedefs

typedef DSPLIB_STATUS(* pFxnDSPLIB_w_vec_exec) (DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pM, void *restrict pOut)
 This is a function pointer type that conforms to the declaration of DSPLIB_w_vec_s_exec_ci, DSPLIB_w_vec_v_exec_ci and DSPLIB_w_vec_s_exec_cn, DSPLIB_w_vec_v_exec_cn. More...
 

Functions

template<typename dataType >
DSPLIB_STATUS DSPLIB_w_vec_init_ci (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_w_vec_InitArgs *pKerInitArgs)
 This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_w_vec_init. More...
 
template<typename dataType >
DSPLIB_STATUS DSPLIB_w_vec_exec_ci (DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pM, void *restrict pOut)
 This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_w_vec_exec. More...
 
template<typename dataType >
DSPLIB_STATUS DSPLIB_w_vec_exec_cn (DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pM, void *restrict pOut)
 This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_w_vec_exec. More...
 

Macro Definition Documentation

◆ DSPLIB_W_VEC_IXX_IXX_OXX_PBLOCK_SIZE

#define DSPLIB_W_VEC_IXX_IXX_OXX_PBLOCK_SIZE   (2 * SE_PARAM_SIZE + 1 * DSPLIB_PARAM_SIZE + 2 * sizeof(int32_t))

Macro to define the size of bufPblock array of DSPLIB_w_vec_PrivArgs structure.

Definition at line 39 of file DSPLIB_w_vec_priv.h.

Typedef Documentation

◆ pFxnDSPLIB_w_vec_exec

typedef DSPLIB_STATUS(* pFxnDSPLIB_w_vec_exec) (DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pM, void *restrict pOut)

This is a function pointer type that conforms to the declaration of DSPLIB_w_vec_s_exec_ci, DSPLIB_w_vec_v_exec_ci and DSPLIB_w_vec_s_exec_cn, DSPLIB_w_vec_v_exec_cn.

Definition at line 46 of file DSPLIB_w_vec_priv.h.

Function Documentation

◆ DSPLIB_w_vec_init_ci()

template<typename dataType >
DSPLIB_STATUS DSPLIB_w_vec_init_ci ( DSPLIB_kernelHandle  handle,
const DSPLIB_bufParams1D_t bufParamsIn,
const DSPLIB_bufParams1D_t bufParamsOut,
const DSPLIB_w_vec_InitArgs pKerInitArgs 
)

This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_w_vec_init.

This function determines the configuration for the streaming engine and MMA hardware resources based on the function call parameters, and the configuration is saved in bufPBlock array. In the kernel call sequence, DSPLIB_w_vec_v_exec_ci or DSPLIB_w_vec_s_exec_ci would be called later independently by the application. When DSPLIB_w_vec_v_exec_ci/ DSPLIB_w_vec_s_exec_ci runs, it merely retrieves the configuration from the bufPBlock and uses it to set up the hardware resources. This arrangement is so that the exec functions do not lose cycles to determine the hardware configuration.

Parameters
[in]handle: Active handle to the kernel
[in]bufParamsIn: Pointer to the structure containing dimensional information of input buffer
[out]bufParamsOut: Pointer to the structure containing dimensional information of ouput buffer
[in]pKerInitArgs: Pointer to the structure holding init parameters
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.

Definition at line 59 of file DSPLIB_w_vec_ci.cpp.

◆ DSPLIB_w_vec_exec_ci()

template<typename dataType >
DSPLIB_STATUS DSPLIB_w_vec_exec_ci ( DSPLIB_kernelHandle  handle,
void *restrict  pIn1,
void *restrict  pIn2,
void *restrict  pM,
void *restrict  pOut 
)

This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_w_vec_exec.

TBD

Parameters
[in]handle: Active handle to the kernel
[in]pIn1: Pointer to buffer holding the input data 1
[in]pIn2: Pointer to buffer holding input data 2
[in]pM: Pointer to buffer holding weight factor
[out]pOut: Pointer to buffer holding the output data
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.
Performance Considerations:
For best performance,
  • the input and output data buffers are expected to be in L2 memory
  • the buffer pointers are assumed to be 64-byte aligned

Definition at line 211 of file DSPLIB_w_vec_ci.cpp.

◆ DSPLIB_w_vec_exec_cn()

template<typename dataType >
DSPLIB_STATUS DSPLIB_w_vec_exec_cn ( DSPLIB_kernelHandle  handle,
void *restrict  pIn1,
void *restrict  pIn2,
void *restrict  pM,
void *restrict  pOut 
)

This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_w_vec_exec.

TBD

Parameters
[in]handle: Active handle to the kernel
[in]pIn1: Pointer to buffer holding the input data 1
[in]pIn2: Pointer to buffer holding the input data 2 data
[in]pM: Pointer to buffer holding weight factor data
[out]pOut: Pointer to buffer holding the output data
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.

Definition at line 32 of file DSPLIB_w_vec_cn.cpp.