![]() |
DSPLIB User Guide
|
Kernel for weighted addition of two input vector data.
Data Structures | |
| struct | DSPLIB_w_vec_InitArgs |
| Structure containing the parameters to initialize the kernel. More... | |
Functions | |
| int32_t | DSPLIB_w_vec_getHandleSize (DSPLIB_w_vec_InitArgs *pKerInitArgs) |
| This is a query function to calculate the size of internal handle. More... | |
| DSPLIB_STATUS | DSPLIB_w_vec_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams1D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_w_vec_InitArgs *pKerInitArgs) |
| This function should be called before the DSPLIB_w_vec_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the MMA accelerator and the streaming engine. The results of these operations are stored in the handle. More... | |
| DSPLIB_STATUS | DSPLIB_w_vec_init_checkParams (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_w_vec_InitArgs *pKerInitArgs) |
| This function checks the validity of the parameters passed to DSPLIB_w_vec_init function. This function is called with the same parameters as the DSPLIB_w_vec_init, and this function must be called before the DSPLIB_w_vec_init is called. More... | |
| DSPLIB_STATUS | DSPLIB_w_vec_exec_checkParams (DSPLIB_kernelHandle handle, const void *restrict pIn1, const void *restrict pIn2, const void *restrict pM, const void *restrict pOut) |
| This function checks the validity of the parameters passed to DSPLIB_w_vec_exec function. This function is called with the same parameters as the DSPLIB_w_vec_init, and this function must be called before the DSPLIB_w_vec_init is called. More... | |
| DSPLIB_STATUS | DSPLIB_w_vec_exec (DSPLIB_kernelHandle handle, void *restrict pIn1, void *restrict pIn2, void *restrict pM, void *restrict pOut) |
| This function is the main kernel compute function. More... | |
Enumerations | |
| enum | DSPLIB_w_vec_weightStyle { DSPLIB_SCALAR = 0 , DSPLIB_VECTOR = 1 } |
| Enumeration for w_vec flag pertaining to scalar or vector input weight. More... | |
Enumeration for w_vec flag pertaining to scalar or vector input weight.
| Enumerator | |
|---|---|
| DSPLIB_SCALAR | Input Weight is a Scalar. |
| DSPLIB_VECTOR | Input Weight is a Vector. |
Definition at line 107 of file DSPLIB_w_vec.h.
| int32_t DSPLIB_w_vec_getHandleSize | ( | DSPLIB_w_vec_InitArgs * | pKerInitArgs | ) |
This is a query function to calculate the size of internal handle.
| [in] | pKerInitArgs | : Pointer to structure holding init parameters |
Definition at line 25 of file DSPLIB_w_vec.cpp.
| DSPLIB_STATUS DSPLIB_w_vec_init | ( | DSPLIB_kernelHandle | handle, |
| DSPLIB_bufParams1D_t * | bufParamsIn, | ||
| DSPLIB_bufParams1D_t * | bufParamsOut, | ||
| const DSPLIB_w_vec_InitArgs * | pKerInitArgs | ||
| ) |
This function should be called before the DSPLIB_w_vec_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the MMA accelerator and the streaming engine. The results of these operations are stored in the handle.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffers |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of ouput buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 83 of file DSPLIB_w_vec.cpp.
| DSPLIB_STATUS DSPLIB_w_vec_init_checkParams | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams1D_t * | bufParamsIn, | ||
| const DSPLIB_bufParams1D_t * | bufParamsOut, | ||
| const DSPLIB_w_vec_InitArgs * | pKerInitArgs | ||
| ) |
This function checks the validity of the parameters passed to DSPLIB_w_vec_init function. This function is called with the same parameters as the DSPLIB_w_vec_init, and this function must be called before the DSPLIB_w_vec_init is called.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffers |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of output buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 32 of file DSPLIB_w_vec.cpp.
| DSPLIB_STATUS DSPLIB_w_vec_exec_checkParams | ( | DSPLIB_kernelHandle | handle, |
| const void *restrict | pIn1, | ||
| const void *restrict | pIn2, | ||
| const void *restrict | pM, | ||
| const void *restrict | pOut | ||
| ) |
This function checks the validity of the parameters passed to DSPLIB_w_vec_exec function. This function is called with the same parameters as the DSPLIB_w_vec_init, and this function must be called before the DSPLIB_w_vec_init is called.
| [in] | handle | : Active handle to the kernel |
| [in] | pIn1 | : Pointer to the structure input buffer 1 |
| [in] | pIn2 | : Pointer to the structure input buffer 2 |
| [in] | pM | : Pointer to structure weight factor |
| [out] | pOut | : Pointer to the output buffer |
Definition at line 62 of file DSPLIB_w_vec.cpp.
| DSPLIB_STATUS DSPLIB_w_vec_exec | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn1, | ||
| void *restrict | pIn2, | ||
| void *restrict | pM, | ||
| void *restrict | pOut | ||
| ) |
This function is the main kernel compute function.
Please refer to details under DSPLIB_w_vec_exec
| [in] | handle | : Active handle to the kernel |
| [in] | pIn1 | : Pointer to buffer holding the input data 1 |
| [in] | pIn2 | : Pointer to buffer holding the input data 2 |
| [in] | pM | : Pointer to buffer holding weight factor |
| [out] | pOut | : Pointer to buffer holding the output data |
Definition at line 191 of file DSPLIB_w_vec.cpp.