![]() |
DSPLIB User Guide
|
Header file for kernel's internal use. For the kernel's interface, please see DSPLIB_maxIndex.
Definition in file DSPLIB_maxIndex_priv.h.
Go to the source code of this file.
Data Structures | |
| struct | DSPLIB_maxIndex_PrivArgs |
| Structure that is reserved for internal use by the kernel. More... | |
| struct | metadata< T, TIndex > |
Macros | |
| #define | SE_PARAM_BASE (0x0000) |
| #define | SE_SE0_PARAM_OFFSET (SE_PARAM_BASE) |
| #define | SE_SE1_PARAM_OFFSET (SE_SE0_PARAM_OFFSET + SE_PARAM_SIZE) |
| #define | DSPLIB_MAXINDEX_IXX_IXX_OXX_PBLOCK_SIZE (1 * SE_PARAM_SIZE + 1 * DSPLIB_PARAM_SIZE + 2 * sizeof(int32_t)) |
| Macro to define the size of bufPblock array of DSPLIB_maxIndex_PrivArgs structure. More... | |
Typedefs | |
| typedef DSPLIB_STATUS(* | pFxnDSPLIB_maxIndex_exec) (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| This is a function pointer type that conforms to the declaration of DSPLIB_maxIndex_exec_ci and DSPLIB_maxIndex_exec_cn. More... | |
Functions | |
| template<typename dataType > | |
| DSPLIB_STATUS | DSPLIB_maxIndex_init_ci (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_maxIndex_InitArgs *pKerInitArgs) |
| This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_maxIndex_init. More... | |
| template<typename T , typename TIndex > | |
| DSPLIB_STATUS | DSPLIB_maxIndex_exec_ci (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_maxIndex_exec. More... | |
| template<typename dataType > | |
| DSPLIB_STATUS | DSPLIB_maxIndex_exec_cn (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_maxIndex_exec. More... | |
| template<typename T , typename TIndex > | |
| metadata< T, TIndex > | DSPLIB_maxIndex_loopLogic (size_t length, void *pSrc) |
| This function is the kernel loop helper function for the optimized implementation of the kernel. The function is called within DSPLIB_maxIndex_exec_c and this method performs the loops needed to calculate the vector containing all of the maxIndeximum values. More... | |
| #define SE_PARAM_BASE (0x0000) |
Definition at line 37 of file DSPLIB_maxIndex_priv.h.
| #define SE_SE0_PARAM_OFFSET (SE_PARAM_BASE) |
Definition at line 38 of file DSPLIB_maxIndex_priv.h.
| #define SE_SE1_PARAM_OFFSET (SE_SE0_PARAM_OFFSET + SE_PARAM_SIZE) |
Definition at line 39 of file DSPLIB_maxIndex_priv.h.
| #define DSPLIB_MAXINDEX_IXX_IXX_OXX_PBLOCK_SIZE (1 * SE_PARAM_SIZE + 1 * DSPLIB_PARAM_SIZE + 2 * sizeof(int32_t)) |
Macro to define the size of bufPblock array of DSPLIB_maxIndex_PrivArgs structure.
Definition at line 46 of file DSPLIB_maxIndex_priv.h.
| typedef DSPLIB_STATUS(* pFxnDSPLIB_maxIndex_exec) (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
This is a function pointer type that conforms to the declaration of DSPLIB_maxIndex_exec_ci and DSPLIB_maxIndex_exec_cn.
Definition at line 53 of file DSPLIB_maxIndex_priv.h.
| DSPLIB_STATUS DSPLIB_maxIndex_init_ci | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams1D_t * | bufParamsIn, | ||
| const DSPLIB_bufParams1D_t * | bufParamsOut, | ||
| const DSPLIB_maxIndex_InitArgs * | pKerInitArgs | ||
| ) |
This function is the initialization function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_maxIndex_init.
This function determines the configuration for the streaming engine and MMA hardware resources based on the function call parameters, and the configuration is saved in bufPBlock array. In the kernel call sequence, DSPLIB_maxIndex_exec_ci would be called later independently by the application. When DSPLIB_maxIndex_exec_ci runs, it merely retrieves the configuration from the bufPBlock and uses it to set up the hardware resources. This arrangement is so that DSPLIB_maxIndex_exec_ci does not lose cycles to determine the hardware configuration.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of ouput buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 76 of file DSPLIB_maxIndex_ci.cpp.
| DSPLIB_STATUS DSPLIB_maxIndex_exec_ci | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn, | ||
| void *restrict | pOut | ||
| ) |
This function is the main execution function for the C7x implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_maxIndex_exec.
The function uses MMA hardware accelerator to perform the convolution computation. Filter data is loaded into B panel of the MMA from memory using one streaming engine, while the input data is loaded into A vectors of the MMA using the other streaming engine. Result of the compute from MMA C panel is stored into memory using a stream minress generator.
| [in] | handle | : Active handle to the kernel |
| [in] | pIn | : Pointer to buffer holding the input data |
| [out] | pOut | : Pointer to buffer holding the output data |
Definition at line 215 of file DSPLIB_maxIndex_ci.cpp.
| DSPLIB_STATUS DSPLIB_maxIndex_exec_cn | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn, | ||
| void *restrict | pOut | ||
| ) |
This function is the main execution function for the natural C implementation of the kernel. The function declaration conforms to the declaration of DSPLIB_maxIndex_exec.
| [in] | handle | : Active handle to the kernel |
| [in] | pIn | : Pointer to buffer holding the input data |
| [out] | pOut | : Pointer to buffer holding the output data |
Definition at line 32 of file DSPLIB_maxIndex_cn.cpp.
| metadata<T, TIndex> DSPLIB_maxIndex_loopLogic | ( | size_t | length, |
| void * | pSrc | ||
| ) |
This function is the kernel loop helper function for the optimized implementation of the kernel. The function is called within DSPLIB_maxIndex_exec_c and this method performs the loops needed to calculate the vector containing all of the maxIndeximum values.
| [in] | length | : length of the input buffer |
| [in] | width | : width of one SIMD buffer |
| [out] | pSrc | : Pointer to buffer holding the input buffer |
Definition at line 349 of file DSPLIB_maxIndex_ci.cpp.