DSPLIB User Guide
DSPLIB_maxIndex

Introduction

Kernel to find the index of the first instance of the maximum value in an input vector.

Data Structures

struct  DSPLIB_maxIndex_InitArgs
 Structure containing the parameters to initialize the kernel. More...
 

Functions

int32_t DSPLIB_maxIndex_getHandleSize (DSPLIB_maxIndex_InitArgs *pKerInitArgs)
 This is a query function to calculate the size of internal handle. More...
 
DSPLIB_STATUS DSPLIB_maxIndex_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams1D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_maxIndex_InitArgs *pKerInitArgs)
 This function should be called before the DSPLIB_maxIndex_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the MMA accelerator and the streaming engine. The results of these operations are stored in the handle. More...
 
DSPLIB_STATUS DSPLIB_maxIndex_init_checkParams (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_maxIndex_InitArgs *pKerInitArgs)
 This function checks the validity of the parameters passed to DSPLIB_maxIndex_init function. This function is called with the same parameters as the DSPLIB_maxIndex_init, and this function must be called before the DSPLIB_maxIndex_init is called. More...
 
DSPLIB_STATUS DSPLIB_maxIndex_exec_checkParams (DSPLIB_kernelHandle handle, const void *restrict pIn, const void *restrict pOut)
 This function checks the validity of the parameters passed to DSPLIB_maxIndex_exec function. This function is called with the same parameters as the DSPLIB_maxIndex_init, and this function must be called before the DSPLIB_maxIndex_init is called. More...
 
DSPLIB_STATUS DSPLIB_maxIndex_exec (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut)
 This function is the main kernel compute function. More...
 

Function Documentation

◆ DSPLIB_maxIndex_getHandleSize()

int32_t DSPLIB_maxIndex_getHandleSize ( DSPLIB_maxIndex_InitArgs pKerInitArgs)

This is a query function to calculate the size of internal handle.

Parameters
[in]pKerInitArgs: Pointer to structure holding init parameters
Returns
Size of the buffer in bytes
Remarks
Application is expected to allocate buffer of the requested size and provide it as input to other functions requiring it.

Definition at line 25 of file DSPLIB_maxIndex.cpp.

◆ DSPLIB_maxIndex_init()

DSPLIB_STATUS DSPLIB_maxIndex_init ( DSPLIB_kernelHandle  handle,
DSPLIB_bufParams1D_t bufParamsIn,
DSPLIB_bufParams1D_t bufParamsOut,
const DSPLIB_maxIndex_InitArgs pKerInitArgs 
)

This function should be called before the DSPLIB_maxIndex_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the MMA accelerator and the streaming engine. The results of these operations are stored in the handle.

Parameters
[in]handle: Active handle to the kernel
[in]bufParamsIn: Pointer to the structure containing dimensional information of input buffer
[out]bufParamsOut: Pointer to the structure containing dimensional information of ouput buffer
[in]pKerInitArgs: Pointer to the structure holding init parameters
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.
Remarks
Application is expected to provide a valid handle.

Definition at line 79 of file DSPLIB_maxIndex.cpp.

◆ DSPLIB_maxIndex_init_checkParams()

DSPLIB_STATUS DSPLIB_maxIndex_init_checkParams ( DSPLIB_kernelHandle  handle,
const DSPLIB_bufParams1D_t bufParamsIn,
const DSPLIB_bufParams1D_t bufParamsOut,
const DSPLIB_maxIndex_InitArgs pKerInitArgs 
)

This function checks the validity of the parameters passed to DSPLIB_maxIndex_init function. This function is called with the same parameters as the DSPLIB_maxIndex_init, and this function must be called before the DSPLIB_maxIndex_init is called.

Parameters
[in]handle: Active handle to the kernel
[in]bufParamsIn: Pointer to the structure containing dimensional information of input buffer
[out]bufParamsOut: Pointer to the structure containing dimensional information of output buffer
[in]pKerInitArgs: Pointer to the structure holding init parameters
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.
Remarks
None

Definition at line 31 of file DSPLIB_maxIndex.cpp.

◆ DSPLIB_maxIndex_exec_checkParams()

DSPLIB_STATUS DSPLIB_maxIndex_exec_checkParams ( DSPLIB_kernelHandle  handle,
const void *restrict  pIn,
const void *restrict  pOut 
)

This function checks the validity of the parameters passed to DSPLIB_maxIndex_exec function. This function is called with the same parameters as the DSPLIB_maxIndex_init, and this function must be called before the DSPLIB_maxIndex_init is called.

Parameters
[in]handle: Active handle to the kernel
[in]pIn: Pointer to the structure input buffer
[out]pout: Pointer to the output buffer
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.
Remarks
None

Definition at line 62 of file DSPLIB_maxIndex.cpp.

◆ DSPLIB_maxIndex_exec()

DSPLIB_STATUS DSPLIB_maxIndex_exec ( DSPLIB_kernelHandle  handle,
void *restrict  pIn,
void *restrict  pOut 
)

This function is the main kernel compute function.

Please refer to details under DSPLIB_maxIndex_exec

Parameters
[in]handle: Active handle to the kernel
[in]pIn: Pointer to the structure input buffer
[out]pout: Pointer to the output buffer
Returns
Status value indicating success or failure. Refer to DSPLIB_STATUS.
Assumptions:
  • None
Performance Considerations:
For best performance,
  • the input and output data buffers are expected to be in L2 memory
  • the buffer pointers are assumed to be 64-byte aligned
Remarks
Before calling this function, application is expected to call DSPLIB_maxIndex_init and DSPLIB_maxIndex_exec_checkParams functions. This ensures resource configuration and error checks are done only once for several invocations of this function.

Definition at line 176 of file DSPLIB_maxIndex.cpp.