This section contains APIs for HW accelerator configuration, in particular to configure the frequency of the VPAC and DMPAC from the A-core.
◆ APP_HWA_CONFIGURE_FREQ_VPAC_720_DMPAC_480
| #define APP_HWA_CONFIGURE_FREQ_VPAC_720_DMPAC_480 (0x0001) |
Configure VPAC to 720 MHz and DMPAC to 480 MHz
◆ APP_HWA_CONFIGURE_FREQ_VPAC_650_DMPAC_520
| #define APP_HWA_CONFIGURE_FREQ_VPAC_650_DMPAC_520 (0x0002) |
Configure VPAC to 650 MHz and DMPAC to 520 MHz
◆ appVhwaConfigureFreq()
| int32_t appVhwaConfigureFreq |
( |
uint32_t |
freq_config | ) |
|
Configures frequency based on input.