Utility and infrastructure APIs used to create applications and kernels.
Sub Modules | |
| (ISP Tuning Tool Server) APIs | |
| This section contains APIs for ISP Tuning Tool Server. | |
| Application Initialization APIs | |
| This section contains APIs for application initialization and de-initialization. | |
| Application RTOS OSAL/DPL APIs | |
| This section contains APIs for providing abstraction between PDK OSAL and MCU+SDK DPL. | |
| Codec Wrapper APIs | |
| This section contains APIs to use CODEC Pipelines within demos. | |
| Display controller remote service APIs (RTOS only) | |
| This section contains APIs for display controller remote service. | |
| Display subsystem initialization APIs (RTOS only) | |
| This section contains APIs for display initialization. | |
| Font and 2D Drawing API | |
| This module has the interface for drawing fonts and 2D primitives like lines. | |
| GStreamer Wrapper APIs | |
| This section contains APIs to use GStreamer CODEC Pipelines within demos. | |
| Graphics overlay utility APIs | |
| This section contains APIs to create and draw graphics overlays for demos. | |
| HW accelerator initialization APIs (HLOS only) | |
| This section contains APIs for HW accelerator configuration, in particular to configure the frequency of the VPAC and DMPAC from the A-core. | |
| HW accelerator initialization APIs (RTOS only) | |
| This section contains APIs for HW accelerator initialization. | |
| ISS | |
| This section contains APIs for ISS. | |
| Inter-processor communication (IPC) APIs | |
| This section contains APIs for Inter-processor communication (IPC) | |
| Logging APIs | |
| This section contains APIs for logging from remote cores to a central host core which prints all the logs to a common console. | |
| Memory allocation APIs | |
| This section contains APIs for memory allocation. | |
| Miscellaneous utility APIs (RTOS only) | |
| This section contains miscellaneous utility APIs. | |
| NetworkCtrl Implementation | |
| OpenGL APIs | |
| This section contains APIs to use OpenGL within Apps. | |
| OpenMAX Codec Wrapper APIs | |
| This section contains APIs to use OpenMAX CODEC Pipelines within demos. | |
| Performance statistics reporting APIs | |
| These APIs allows user to get performance information of RTOS based remote cores. | |
| Remote Service APIs (RTOS only) | |
| These APIs allows user to invoke functions or services on remote cores by abstracting the low level IPC details. | |
| SCICLIENT initialization APIs (RTOS only) | |
| This section contains APIs for SCICLIENT initialization. | |
| SCISERVER initialization APIs (RTOS only) | |
| This section contains APIs for SCISERVER initialization. | |
| Sensor Initialization API (RTOS only) | |
| This section contains APIs for Sensor initialization. | |
| UDMA initialization APIs (RTOS only) | |
| This section contains APIs for UDMA initialization. | |