TIOVX User Guide

Super Node object descriptor. More...

#include <tivx_obj_desc_priv.h>

Data Fields

tivx_obj_desc_t base
 base object descriptor
 
uint16_t num_nodes
 number of nodes in super node
 
uint16_t node_obj_desc_id [TIVX_SUPER_NODE_MAX_NODES]
 topologically sorted list of nodes obj desc's in super node
 
uint16_t num_edges
 number of edges in super node sub graph
 
tivx_obj_desc_super_node_edge_t edge_list [TIVX_SUPER_NODE_MAX_EDGES]
 super node edge list
 

Detailed Description

Super Node object descriptor.

Definition at line 383 of file tivx_obj_desc_priv.h.


The documentation for this struct was generated from the following file: