Internal APIs for node operations.
|
| vx_status | ownSetNodeImmTarget (vx_node node) |
| | Set the target for node based on immediate mode target set in context. More...
|
| |
| vx_status | ownSetNodeAttributeValidRectReset (vx_node node, vx_bool is_reset) |
| | Set the attribute VX_NODE_VALID_RECT_RESET in node. More...
|
| |
|
vx_status | ownNodeKernelValidate (vx_node node, vx_meta_format meta[]) |
| | Validate user kernel or target kernel associated with this node.
|
| |
|
vx_status | ownNodeKernelInit (vx_node node) |
| | Init user kernel or target kernel associated with this node.
|
| |
|
vx_status | ownNodeKernelInitKernelName (vx_node node) |
| | Init user kernel or target kernel name associated with this node.
|
| |
|
vx_status | ownNodeKernelDeinitKernelName (vx_node node) |
| | Deinit user kernel or target kernel name associated with this node.
|
| |
|
vx_status | ownNodeKernelSchedule (vx_node node, uint32_t pipeline_id) |
| | Schedule user kernel or target kernel associated with this node for execution.
|
| |
|
vx_status | ownNodeKernelDeinit (vx_node node) |
| | DeInit user kernel or target kernel associated with this node.
|
| |
|
vx_status | ownResetNodePerf (vx_node node) |
| | Reset node performance statistics.
|
| |
|
vx_status | ownUpdateNodePerf (vx_node node, uint32_t pipeline_id) |
| | Called by graph each time after node execution.
|
| |
|
uint32_t | ownNodeGetNumParameters (vx_node node) |
| | Return number of node parameters.
|
| |
|
vx_enum | ownNodeGetParameterDir (vx_node node, uint32_t prm_index) |
| | Get direction of a parameter.
|
| |
|
vx_reference | ownNodeGetParameterRef (vx_node node, uint32_t prm_index) |
| | Get reference associated with a parameters of a parameter.
|
| |
|
vx_status | ownNodeAddOutNode (vx_node node, vx_node out_node) |
| | Associate a output node with a given node.
|
| |
|
vx_status | ownNodeReplaceOutNode (vx_node node, vx_node old_out_node, vx_node new_out_node) |
| | Replace an output node for a given node with a new output node.
|
| |
|
vx_status | ownNodeAddInNode (vx_node node, vx_node out_node) |
| | Associate a input node with a given node.
|
| |
|
vx_status | ownNodeReplaceInNode (vx_node node, vx_node old_in_node, vx_node new_in_node) |
| | Replace an input node for a given node with a new input node.
|
| |
|
uint32_t | ownNodeGetNumInNodes (vx_node node) |
| | Get number of input nodes associated with this node.
|
| |
|
uint32_t | ownNodeGetNumOutNodes (vx_node node) |
| | Get number of output nodes associated with this node.
|
| |
|
vx_status | ownNodeCreateUserCallbackCommand (vx_node node, uint32_t pipeline_id) |
| | Create resources required to call a user callback If user callback is assigned then nothing is done.
|
| |
|
vx_action | ownNodeExecuteUserCallback (vx_node node) |
| | Call user specified callback.
|
| |
|
void | ownNodeClearExecuteState (vx_node node, uint32_t pipeline_id) |
| | clears execute status of the node
|
| |
|
vx_status | ownNodeUserKernelExecute (vx_node node, vx_reference prm_ref[]) |
| | Execute user kernel.
|
| |
|
vx_bool | ownNodeIsPrmReplicated (vx_node node, uint32_t prm_idx) |
| | Is prm_idx of node replicated.
|
| |
|
vx_status | ownNodeSetParameter (vx_node node, vx_uint32 idx, vx_reference value) |
| | Set parameter at node.
|
| |
|
vx_node | ownNodeGetNextNode (vx_node node, vx_uint32 idx) |
| | Get next node at given output index.
|
| |
|
vx_node | ownNodeGetNextInNode (vx_node node, vx_uint32 idx) |
| | Get next node at given input index.
|
| |
|
vx_status | ownNodeRegisterEvent (vx_node node, vx_enum event_type, vx_uint32 app_value, enum tivx_queue_type_e queue_type) |
| | Register node completion event.
|
| |
|
void | ownNodeCheckAndSendCompletionEvent (const tivx_obj_desc_node_t *node_obj_desc, uint64_t timestamp) |
| | Send node completion event if enabled.
|
| |
|
void | ownNodeCheckAndSendErrorEvent (const tivx_obj_desc_node_t *node_obj_desc, uint64_t timestamp, vx_status status) |
| | Send node error event if node failed.
|
| |
|
vx_status | ownNodeAllocObjDescForPipeline (vx_node node, uint32_t pipeline_depth) |
| | Alloc additional node obj desc's for pipelining.
|
| |
|
void | ownNodeSetObjDescParamDirection (vx_node node) |
| | Set param direction for 0th node obj desc.
|
| |
|
void | ownNodeLinkObjDescForPipeline (vx_node node) |
| | Update in node id and out node id for node pipeline obj desc's.
|
| |
|
void | ownNodeLinkDataRefQueue (vx_node node, uint32_t prm_id, tivx_data_ref_queue data_ref_q) |
| | Link data ref q to node at parameter index 'prm_id'.
|
| |
|
void | ownNodeLinkArrayElement (vx_node node, uint32_t prm_id) |
| | Link array element to node at parameter index 'prm_id'.
|
| |
| uint32_t | ownNodeGetParameterNumBuf (vx_node node, vx_uint32 idx) |
| | Return number of buffers to allocate at a node,index. More...
|
| |