TIOVX User Guide
tivx_data_ref_queue.h File Reference

Implementation of Data Reference Queue Object APIs. More...

Go to the source code of this file.

Data Structures

struct  tivx_data_ref_queue_t
 Data Ref Queue internal state. More...
 
struct  tivx_data_ref_queue_create_params_t
 Parameters used to create a data ref queue. More...
 

Typedefs

typedef struct _tivx_data_ref_queue * tivx_data_ref_queue
 Data Ref Queue Object.
 

Functions

tivx_data_ref_queue tivxDataRefQueueCreate (vx_graph graph, const tivx_data_ref_queue_create_params_t *prms)
 Create data reference queue.
 
vx_status ownDataRefQueueRelease (tivx_data_ref_queue *ref)
 Release data reference queue.
 
uint16_t ownDataRefQueueGetObjDescId (tivx_data_ref_queue ref, uint32_t pipeline_id)
 return object descriptor ID of specific pipeline ID
 
vx_status ownDataRefQueueWaitDoneRef (tivx_data_ref_queue data_ref_q, vx_uint32 timeout)
 Wait for 'DONE' queue to be non-empty. More...
 
vx_status ownDataRefQueueGetDoneQueueCount (tivx_data_ref_queue data_ref_q, vx_uint32 *count)
 Return number of elements in 'DONE' queue.
 
vx_status ownDataRefQueueGetReadyQueueCount (tivx_data_ref_queue data_ref_q, vx_uint32 *count)
 Return number of elements in 'READY' queue.
 
vx_status ownDataRefQueueSendRefConsumedEvent (tivx_data_ref_queue ref, uint64_t timestamp)
 Send 'ref consumed event' if event send is enabled.
 
vx_status ownDataRefQueueLinkDelayDataRefQueues (tivx_data_ref_queue delay_data_ref_q_list[], vx_bool auto_age_delay_slot[], uint32_t delay_slots)
 Link data ref queues that participate in a delay in a circular manner.
 

Detailed Description

Implementation of Data Reference Queue Object APIs.

Definition in file tivx_data_ref_queue.h.

Function Documentation

◆ ownDataRefQueueWaitDoneRef()

vx_status ownDataRefQueueWaitDoneRef ( tivx_data_ref_queue  data_ref_q,
vx_uint32  timeout 
)

Wait for 'DONE' queue to be non-empty.

if 'timeout' units of time elapses then VX_FAILURE is returned

NOTE, this is a blocking API and block for 'timeout' units of time