![]() |
MATHLIB User Guide
|
Go to the source code of this file.
Functions | |
| template<typename T > | |
| MATHLIB_STATUS | MATHLIB_acosh (size_t length, T *pSrc, T *pDst) |
| Performs the elementwise inverse hyperbolic cosine of an input vector. Function can be overloaded with float pointers, and the appropriate precision is employed to compute elementwise inverse hyperbolic cosine of the input vector. More... | |
| MATHLIB_STATUS | MATHLIB_acosh_sp (size_t length, float *pSrc, float *pDst) |
| This function is the C interface for MATHLIB_acosh. Function accepts float pointers. More... | |