MATHLIB User Guide
MATHLIB_acosh

Introduction

Kernel for elementwise inverse hyperbolic cosine of an input vector. Supports float datatype.

Functions

template<typename T >
MATHLIB_STATUS MATHLIB_acosh (size_t length, T *pSrc, T *pDst)
 Performs the elementwise inverse hyperbolic cosine of an input vector. Function can be overloaded with float pointers, and the appropriate precision is employed to compute elementwise inverse hyperbolic cosine of the input vector. More...
 
MATHLIB_STATUS MATHLIB_acosh_sp (size_t length, float *pSrc, float *pDst)
 This function is the C interface for MATHLIB_acosh. Function accepts float pointers. More...
 

Function Documentation

◆ MATHLIB_acosh()

template<typename T >
MATHLIB_STATUS MATHLIB_acosh ( size_t  length,
T *  pSrc,
T *  pDst 
)

Performs the elementwise inverse hyperbolic cosine of an input vector. Function can be overloaded with float pointers, and the appropriate precision is employed to compute elementwise inverse hyperbolic cosine of the input vector.

Template Parameters
T: implementation datatype
Parameters
[in]length: length of input vector
[in]pSrc: pointer to buffer holding input vector
[out]pDst: pointer to buffer holding result vector
Returns
Status of success.
Remarks
None

◆ MATHLIB_acosh_sp()

MATHLIB_STATUS MATHLIB_acosh_sp ( size_t  length,
float *  pSrc,
float *  pDst 
)

This function is the C interface for MATHLIB_acosh. Function accepts float pointers.

Template Parameters
T: implementation datatype
Parameters
[in]length: length of input vector
[in]pSrc: pointer to buffer holding input vector
[out]pDst: pointer to buffer holding result vector
Returns
Status of success.
Remarks
None

Definition at line 375 of file MATHLIB_acosh.cpp.