![]() |
DSPLIB User Guide
|
Structure that is reserved for internal use by the kernel.
Definition at line 58 of file DSPLIB_fltoq15_priv.h.
Data Fields | |
| pFxnDSPLIB_fltoq15_exec | execute |
| Function pointer to point to the right execution variant between DSPLIB_fltoq15_exec_cn and DSPLIB_fltoq15_exec_ci. More... | |
| int32_t | blockSize |
| Size of input buffer for different batches DSPLIB_fltoq15_init that will be retrieved and used by DSPLIB_fltoq15_exec More... | |
| bool | isSEReadEnabled |
| Flag indicating if SE reads and stores are enabled, set by DSPLIB_fltoq15_init_ci that will be retrieved and used by DSPLIB_bexp_exec More... | |
| uint8_t | bufPblock [DSPLIB_FLTOQ15_IXX_IXX_OXX_PBLOCK_SIZE] |
| pFxnDSPLIB_fltoq15_exec DSPLIB_fltoq15_PrivArgs::execute |
Function pointer to point to the right execution variant between DSPLIB_fltoq15_exec_cn and DSPLIB_fltoq15_exec_ci.
Definition at line 62 of file DSPLIB_fltoq15_priv.h.
| int32_t DSPLIB_fltoq15_PrivArgs::blockSize |
Size of input buffer for different batches DSPLIB_fltoq15_init that will be retrieved and used by DSPLIB_fltoq15_exec
Definition at line 66 of file DSPLIB_fltoq15_priv.h.
| bool DSPLIB_fltoq15_PrivArgs::isSEReadEnabled |
Flag indicating if SE reads and stores are enabled, set by DSPLIB_fltoq15_init_ci that will be retrieved and used by DSPLIB_bexp_exec
Definition at line 70 of file DSPLIB_fltoq15_priv.h.
| uint8_t DSPLIB_fltoq15_PrivArgs::bufPblock[DSPLIB_FLTOQ15_IXX_IXX_OXX_PBLOCK_SIZE] |
Definition at line 72 of file DSPLIB_fltoq15_priv.h.