![]() |
DSPLIB User Guide
|
This Kernel converts the IEEE floating point numbers stored in vector pIn into Q.15 format numbers and stores in vector pOut.
Data Structures | |
| struct | DSPLIB_fltoq15_InitArgs |
| Structure containing the parameters to initialize the kernel. More... | |
Functions | |
| int32_t | DSPLIB_fltoq15_getHandleSize (DSPLIB_fltoq15_InitArgs *pKerInitArgs) |
| This is a query function to calculate the size of internal handle. More... | |
| DSPLIB_STATUS | DSPLIB_fltoq15_init_checkParams (DSPLIB_kernelHandle handle, const DSPLIB_bufParams1D_t *bufParamsIn, const DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_fltoq15_InitArgs *pKerInitArgs) |
| This function checks the validity of the parameters passed to DSPLIB_fltoq15_init function. This function is called with the same parameters as the DSPLIB_fltoq15_init, and this function must be called before the DSPLIB_fltoq15_init is called. More... | |
| DSPLIB_STATUS | DSPLIB_fltoq15_init (DSPLIB_kernelHandle handle, DSPLIB_bufParams1D_t *bufParamsIn, DSPLIB_bufParams1D_t *bufParamsOut, const DSPLIB_fltoq15_InitArgs *pKerInitArgs) |
| This function should be called before the DSPLIB_fltoq15_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the the streaming engine and streaming address generator. The results of these operations are stored in the handle. More... | |
| DSPLIB_STATUS | DSPLIB_fltoq15_exec_checkParams (DSPLIB_kernelHandle handle, const void *restrict pIn, const void *restrict pOut) |
| This function checks the validity of the parameters passed to DSPLIB_fltoq15_exec function. This function is called with the same parameters as the DSPLIB_fltoq15_init, and this function must be called before the DSPLIB_fltoq15_init is called. More... | |
| DSPLIB_STATUS | DSPLIB_fltoq15_exec (DSPLIB_kernelHandle handle, void *restrict pIn, void *restrict pOut) |
| This function is the main kernel compute function. More... | |
| int32_t DSPLIB_fltoq15_getHandleSize | ( | DSPLIB_fltoq15_InitArgs * | pKerInitArgs | ) |
This is a query function to calculate the size of internal handle.
| [in] | pKerInitArgs | : Pointer to structure holding init parameters |
Definition at line 25 of file DSPLIB_fltoq15.cpp.
| DSPLIB_STATUS DSPLIB_fltoq15_init_checkParams | ( | DSPLIB_kernelHandle | handle, |
| const DSPLIB_bufParams1D_t * | bufParamsIn, | ||
| const DSPLIB_bufParams1D_t * | bufParamsOut, | ||
| const DSPLIB_fltoq15_InitArgs * | pKerInitArgs | ||
| ) |
This function checks the validity of the parameters passed to DSPLIB_fltoq15_init function. This function is called with the same parameters as the DSPLIB_fltoq15_init, and this function must be called before the DSPLIB_fltoq15_init is called.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of output buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 34 of file DSPLIB_fltoq15.cpp.
| DSPLIB_STATUS DSPLIB_fltoq15_init | ( | DSPLIB_kernelHandle | handle, |
| DSPLIB_bufParams1D_t * | bufParamsIn, | ||
| DSPLIB_bufParams1D_t * | bufParamsOut, | ||
| const DSPLIB_fltoq15_InitArgs * | pKerInitArgs | ||
| ) |
This function should be called before the DSPLIB_fltoq15_exec function is called. This function takes care of any one-time operations such as setting up the configuration of required hardware resources such as the the streaming engine and streaming address generator. The results of these operations are stored in the handle.
| [in] | handle | : Active handle to the kernel |
| [in] | bufParamsIn | : Pointer to the structure containing dimensional information of input buffer |
| [out] | bufParamsOut | : Pointer to the structure containing dimensional information of ouput buffer |
| [in] | pKerInitArgs | : Pointer to the structure holding init parameters |
Definition at line 82 of file DSPLIB_fltoq15.cpp.
| DSPLIB_STATUS DSPLIB_fltoq15_exec_checkParams | ( | DSPLIB_kernelHandle | handle, |
| const void *restrict | pIn, | ||
| const void *restrict | pOut | ||
| ) |
This function checks the validity of the parameters passed to DSPLIB_fltoq15_exec function. This function is called with the same parameters as the DSPLIB_fltoq15_init, and this function must be called before the DSPLIB_fltoq15_init is called.
| [in] | handle | : Active handle to the kernel |
| [in] | pIn | : Pointer to the structure input buffer |
| [out] | pout | : Pointer to the output buffer |
Definition at line 65 of file DSPLIB_fltoq15.cpp.
| DSPLIB_STATUS DSPLIB_fltoq15_exec | ( | DSPLIB_kernelHandle | handle, |
| void *restrict | pIn, | ||
| void *restrict | pOut | ||
| ) |
This function is the main kernel compute function.
Please refer to details under DSPLIB_fltoq15_exec
| [in] | handle | : Active handle to the kernel |
| [in] | pIn | : Pointer to buffer holding the input data |
| [out] | pOut | : Pointer to buffer holding the output data |
Definition at line 128 of file DSPLIB_fltoq15.cpp.