![]() |
SDL API Guide for J721S2
|
MPU Data configuration.
This structure defines the elements of the MPU Data configuration Please refer to ARM R5 Technical Reference Manual for details on MPU The self test code assumes a free memory region ID to be provided which configures the test memory location sub region to trigger the intended
Data Fields | |
uint32_t * | pMemLocation |
SDL_MPU_memAccessType | memAccessType |
uint32_t | mpuRegionId |
uint32_t* SDL_MPU_memConfig_t::pMemLocation |
Pointer to 16 byte aligned 32 byte memory block for self test example location as 0x41C7EFE0
SDL_MPU_memAccessType SDL_MPU_memConfig_t::memAccessType |
Memory access type to be used to generate exception
uint32_t SDL_MPU_memConfig_t::mpuRegionId |
MPU Region ID to be used for MPU Self Test