SDL API Guide for J721S2
|
Sub Modules | |
Built-In Test (PBIST) | |
CPU Compare Module(CCM) | |
Dual Clock Comparator(DCC) | |
Error Correction Code(ECC) | |
Error Signaling Module (ESM) | |
Logical Built-In Test (LBIST) | |
MSMC API | |
Master Timeout Gasket(MTOG) | |
Memory Cyclic Redundancy check(MCRC) | |
This file contains the prototypes of the APIs present in the device abstraction layer file of MCRC. This also contains some related macros. | |
Power OK(POK) | |
RAT API | |
ROM_CHECKSUM API | |
Real Time Interrupt(RTI) | |
SDL MPU API | |
Timeout Gasket(TOG) | |
Voltage and Thermal Monitor(VTM) | |